<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>topic Re: Debugger Cable in S32K</title>
    <link>https://community.nxp.com/t5/S32K/Debugger-Cable/m-p/2093485#M48572</link>
    <description>&lt;P&gt;Hi&lt;/P&gt;
&lt;P&gt;&lt;A href="https://www.segger.com/products/debug-probes/j-link/accessories/adapters/19-pin-cortex-m-adapter/" target="_blank"&gt;https://www.segger.com/products/debug-probes/j-link/accessories/adapters/19-pin-cortex-m-adapter/&lt;/A&gt;&lt;/P&gt;
&lt;P&gt;This can be used to debug S32K148.&lt;/P&gt;
&lt;P&gt;Best Regards,&lt;BR /&gt;Robin&lt;BR /&gt;-------------------------------------------------------------------------------&lt;BR /&gt;Note:&lt;BR /&gt;- If this post answers your question, please click the "ACCEPT AS SOLUTION" button. Thank you!&lt;/P&gt;
&lt;P&gt;- We are following threads for 7 weeks after the last post, later replies are ignored&lt;BR /&gt;Please open a new thread and refer to the closed one, if you have a related question at a later point in time.&lt;BR /&gt;-------------------------------------------------------------------------------&lt;/P&gt;</description>
    <pubDate>Thu, 08 May 2025 08:42:50 GMT</pubDate>
    <dc:creator>Robin_Shen</dc:creator>
    <dc:date>2025-05-08T08:42:50Z</dc:date>
    <item>
      <title>Debugger Cable</title>
      <link>https://community.nxp.com/t5/S32K/Debugger-Cable/m-p/2093311#M48554</link>
      <description>&lt;P&gt;I want to connect the segger 20-pin J-Link pro debugger to S32K148EVB JTAG header. The pitch size of the S32K148EVB JTAG header is 1.27mm(0.05") whereas the size of the J-Link pro is 2.54mm(0.1"). Can I use the " J-Link 19-pin Cortex-M Adapter: Adapts from 20&lt;BR /&gt;pin, 0.1' Standard connector to 19-pin, 0.05' Cortex&lt;BR /&gt;M connector incl. 19 pin cable" to connect the J-Link pro debugger to the JTAG header in S32K148EVB?&lt;/P&gt;</description>
      <pubDate>Thu, 08 May 2025 05:42:31 GMT</pubDate>
      <guid>https://community.nxp.com/t5/S32K/Debugger-Cable/m-p/2093311#M48554</guid>
      <dc:creator>Prajwal123</dc:creator>
      <dc:date>2025-05-08T05:42:31Z</dc:date>
    </item>
    <item>
      <title>Re: Debugger Cable</title>
      <link>https://community.nxp.com/t5/S32K/Debugger-Cable/m-p/2093313#M48555</link>
      <description>&lt;P&gt;For debugging&lt;/P&gt;</description>
      <pubDate>Thu, 08 May 2025 05:43:14 GMT</pubDate>
      <guid>https://community.nxp.com/t5/S32K/Debugger-Cable/m-p/2093313#M48555</guid>
      <dc:creator>Prajwal123</dc:creator>
      <dc:date>2025-05-08T05:43:14Z</dc:date>
    </item>
    <item>
      <title>Re: Debugger Cable</title>
      <link>https://community.nxp.com/t5/S32K/Debugger-Cable/m-p/2093485#M48572</link>
      <description>&lt;P&gt;Hi&lt;/P&gt;
&lt;P&gt;&lt;A href="https://www.segger.com/products/debug-probes/j-link/accessories/adapters/19-pin-cortex-m-adapter/" target="_blank"&gt;https://www.segger.com/products/debug-probes/j-link/accessories/adapters/19-pin-cortex-m-adapter/&lt;/A&gt;&lt;/P&gt;
&lt;P&gt;This can be used to debug S32K148.&lt;/P&gt;
&lt;P&gt;Best Regards,&lt;BR /&gt;Robin&lt;BR /&gt;-------------------------------------------------------------------------------&lt;BR /&gt;Note:&lt;BR /&gt;- If this post answers your question, please click the "ACCEPT AS SOLUTION" button. Thank you!&lt;/P&gt;
&lt;P&gt;- We are following threads for 7 weeks after the last post, later replies are ignored&lt;BR /&gt;Please open a new thread and refer to the closed one, if you have a related question at a later point in time.&lt;BR /&gt;-------------------------------------------------------------------------------&lt;/P&gt;</description>
      <pubDate>Thu, 08 May 2025 08:42:50 GMT</pubDate>
      <guid>https://community.nxp.com/t5/S32K/Debugger-Cable/m-p/2093485#M48572</guid>
      <dc:creator>Robin_Shen</dc:creator>
      <dc:date>2025-05-08T08:42:50Z</dc:date>
    </item>
  </channel>
</rss>