<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>S32KのトピックRe: FS26 Not Entering Standby &amp;amp;amp; Initialization Fails – FS_STATE</title>
    <link>https://community.nxp.com/t5/S32K/FS26-Not-Entering-Standby-amp-amp-Initialization-Fails-FS-STATE/m-p/2091275#M48420</link>
    <description>&lt;P class=""&gt;Thank you for your response. I checked the suggested solution, but it was still showing the same issue. On further debugging, I found that the system was entering the INVALID_FS state and was not updating any configurations from the peripherals. I reviewed the default register values and identified the SBC_FS26_FS_GRL_FLAGS_ADDR register, which indicated an overvoltage fault. Upon checking the SBC_FS26_FS_OVUV_REG_STATUS_ADDR register, I saw that it was a VMON_EXT overvoltage condition. After adjusting the circuit connection and changing the resistance values, the issue was resolved. The system now transitions properly into the FS_Init state, and other operations are working as expected. Thanks again for your support.&lt;/P&gt;</description>
    <pubDate>Mon, 05 May 2025 07:42:22 GMT</pubDate>
    <dc:creator>GaneshBhagwat</dc:creator>
    <dc:date>2025-05-05T07:42:22Z</dc:date>
    <item>
      <title>FS26 Not Entering Standby &amp;amp; Initialization Fails – FS_STATE</title>
      <link>https://community.nxp.com/t5/S32K/FS26-Not-Entering-Standby-amp-amp-Initialization-Fails-FS-STATE/m-p/2089503#M48306</link>
      <description>&lt;P&gt;Hello NXP Support,&lt;/P&gt;&lt;P&gt;I’m working with the following example from your knowledge base:&lt;BR /&gt;&lt;A href="https://community.nxp.com/t5/S32K-Knowledge-Base/RTD-Example-FS26-WKUP-with-PGOOD-and-EXTWAKE-using-a-S32K3X8EVB/ta-p/1973656" target="_blank" rel="noopener"&gt;RTD Example: FS26 WKUP with PGOOD and EXTWAKE using a S32K3X8EVB&lt;/A&gt;&lt;/P&gt;&lt;P&gt;My goal is to put both the FS26 and the S32K3X8 controller into &lt;STRONG&gt;standby mode&lt;/STRONG&gt;. While the controller successfully transitions to standby, the FS26 remains in the same state and does not follow.&lt;/P&gt;&lt;P&gt;Additionally, the function call:&lt;/P&gt;&lt;PRE&gt;eReturnValue |= Sbc_fs26_InitDevice();&lt;/PRE&gt;&lt;P&gt;returns not_ok, and the initialization process fails. Upon debugging, I found that Sbc_fs26_GetDeviceState() is returning 0x14 as the FS_STATE value.&lt;/P&gt;&lt;P&gt;According to the FS26 datasheet, I couldn't find any documentation clearly explaining the meaning of this value, particularly &lt;STRONG&gt;bit 4&lt;/STRONG&gt; (i.e., 0x14 = 0b10100). Could you please clarify what bit 4 represents in the FS_STATE register? It's not mentioned in the register description section of the datasheet.&lt;/P&gt;&lt;P&gt;I also came across this related post that seems to touch on a similar issue, but there is no clear resolution provided:&lt;BR /&gt;&lt;A href="https://community.nxp.com/t5/Other-NXP-Products/FS26-FS-STATES-amp-SPI-Communication/m-p/2019073" target="_blank" rel="noopener"&gt;FS26 FS_STATES &amp;amp; SPI Communication&lt;/A&gt;&lt;/P&gt;&lt;P&gt;Could you please assist with the following:&lt;/P&gt;&lt;OL&gt;&lt;LI&gt;&lt;P&gt;Why is the FS26 not transitioning to standby mode alongside the S32K3X8?&lt;/P&gt;&lt;/LI&gt;&lt;LI&gt;&lt;P&gt;What does the FS_STATE value 0x14 indicate, specifically the significance of bit 4?&lt;/P&gt;&lt;/LI&gt;&lt;LI&gt;&lt;P&gt;What are the possible reasons for Sbc_fs26_InitDevice() returning not_ok?&lt;/P&gt;&lt;/LI&gt;&lt;/OL&gt;&lt;P&gt;Any guidance or clarification would be greatly appreciated, especially regarding the undocumented FS_STATE bits.&lt;/P&gt;&lt;P&gt;&lt;span class="lia-inline-image-display-wrapper lia-image-align-inline" image-alt="GaneshBhagwat_0-1745942345751.png"&gt;&lt;img src="https://community.nxp.com/t5/image/serverpage/image-id/335610i79DE284628DE25AC/image-size/medium?v=v2&amp;amp;px=400" alt="GaneshBhagwat_0-1745942345751.png" title="GaneshBhagwat_0-1745942345751.png" /&gt;&lt;/span&gt;&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;</description>
      <pubDate>Tue, 29 Apr 2025 15:59:52 GMT</pubDate>
      <guid>https://community.nxp.com/t5/S32K/FS26-Not-Entering-Standby-amp-amp-Initialization-Fails-FS-STATE/m-p/2089503#M48306</guid>
      <dc:creator>GaneshBhagwat</dc:creator>
      <dc:date>2025-04-29T15:59:52Z</dc:date>
    </item>
    <item>
      <title>Re: FS26 Not Entering Standby &amp;amp; Initialization Fails – FS_STATE</title>
      <link>https://community.nxp.com/t5/S32K/FS26-Not-Entering-Standby-amp-amp-Initialization-Fails-FS-STATE/m-p/2089511#M48307</link>
      <description>&lt;a href="https://community.nxp.com/t5/user/viewprofilepage/user-id/205468"&gt;@YvanR&lt;/a&gt; Can you please have a look.</description>
      <pubDate>Tue, 29 Apr 2025 16:13:02 GMT</pubDate>
      <guid>https://community.nxp.com/t5/S32K/FS26-Not-Entering-Standby-amp-amp-Initialization-Fails-FS-STATE/m-p/2089511#M48307</guid>
      <dc:creator>GaneshBhagwat</dc:creator>
      <dc:date>2025-04-29T16:13:02Z</dc:date>
    </item>
    <item>
      <title>Re: FS26 Not Entering Standby &amp;amp; Initialization Fails – FS_STATE</title>
      <link>https://community.nxp.com/t5/S32K/FS26-Not-Entering-Standby-amp-amp-Initialization-Fails-FS-STATE/m-p/2089779#M48319</link>
      <description>&lt;P&gt;HI&amp;nbsp;&lt;/P&gt;
&lt;OL&gt;
&lt;LI&gt;
&lt;P&gt;Why is the FS26 not transitioning to standby mode alongside the S32K3X8?[gw]before enter into standby mode,what's the mode of FS26? how did you operate it enter into standby mode?&lt;/P&gt;
&lt;/LI&gt;
&lt;LI&gt;
&lt;P&gt;What does the FS_STATE value 0x14 indicate, specifically the significance of bit 4?&lt;BR /&gt;[gw]If no match the table value in your post picture, there is meaningless for this result.&lt;/P&gt;
&lt;/LI&gt;
&lt;LI&gt;
&lt;P&gt;What are the possible reasons for Sbc_fs26_InitDevice() returning not_ok?[gw]I should know answer in my quesitons1 reply.&lt;/P&gt;
&lt;/LI&gt;
&lt;/OL&gt;</description>
      <pubDate>Wed, 30 Apr 2025 03:27:17 GMT</pubDate>
      <guid>https://community.nxp.com/t5/S32K/FS26-Not-Entering-Standby-amp-amp-Initialization-Fails-FS-STATE/m-p/2089779#M48319</guid>
      <dc:creator>guoweisun</dc:creator>
      <dc:date>2025-04-30T03:27:17Z</dc:date>
    </item>
    <item>
      <title>Re: FS26 Not Entering Standby &amp;amp; Initialization Fails – FS_STATE</title>
      <link>https://community.nxp.com/t5/S32K/FS26-Not-Entering-Standby-amp-amp-Initialization-Fails-FS-STATE/m-p/2090178#M48355</link>
      <description>&lt;P class=""&gt;1. Before entering standby mode, what state is the FS26 in? How are you attempting to transition it into standby mode?&lt;/P&gt;&lt;P class=""&gt;I’m using the S32K358 development board, which includes the FS26 with the default configuration. I’m currently testing the example code provided by NXP[mentioned link in the post]. However, the Sbc_fs26_InitDevice() function is returning NO_OK, indicating the initialization is failing. As a result, the FS26 is not transitioning to the FS_INIT or any other operational state. When I read the FS_STATE register, I’m getting 0x14.&lt;/P&gt;&lt;P class=""&gt;&amp;nbsp;&lt;/P&gt;&lt;P class=""&gt;2.&amp;nbsp;&lt;STRONG&gt;What does the FS_STATE value 0x14 indicate, particularly the significance of bit 4?&lt;/STRONG&gt;&lt;BR /&gt;If this value doesn’t match any entry in the table shown in your screenshot, does it still have any defined meaning?&lt;/P&gt;&lt;P class=""&gt;Also, why does the register use 4 bits when all documented FS states seem to be covered within 3 bits? The table mentions “Actual State of the Fail-Safe State Machine,” so is bit 4 indicating a special fault condition or an undocumented state?&lt;/P&gt;</description>
      <pubDate>Wed, 30 Apr 2025 10:33:49 GMT</pubDate>
      <guid>https://community.nxp.com/t5/S32K/FS26-Not-Entering-Standby-amp-amp-Initialization-Fails-FS-STATE/m-p/2090178#M48355</guid>
      <dc:creator>GaneshBhagwat</dc:creator>
      <dc:date>2025-04-30T10:33:49Z</dc:date>
    </item>
    <item>
      <title>Re: FS26 Not Entering Standby &amp;amp; Initialization Fails – FS_STATE</title>
      <link>https://community.nxp.com/t5/S32K/FS26-Not-Entering-Standby-amp-amp-Initialization-Fails-FS-STATE/m-p/2090519#M48376</link>
      <description>&lt;P&gt;You can try to change green circled as 'no effect on RSTB and FS0B' this in S32DS:&lt;/P&gt;
&lt;P&gt;&lt;span class="lia-inline-image-display-wrapper lia-image-align-inline" image-alt="guoweisun_0-1746063320230.png" style="width: 400px;"&gt;&lt;img src="https://community.nxp.com/t5/image/serverpage/image-id/335928i0748ACFA31823C23/image-size/medium?v=v2&amp;amp;px=400" role="button" title="guoweisun_0-1746063320230.png" alt="guoweisun_0-1746063320230.png" /&gt;&lt;span class="lia-inline-image-caption" onclick="event.preventDefault();"&gt;guoweisun_0-1746063320230.png&lt;/span&gt;&lt;/span&gt;&lt;/P&gt;
&lt;P&gt;disabled watchdog period&lt;/P&gt;
&lt;P&gt;&lt;span class="lia-inline-image-display-wrapper lia-image-align-inline" image-alt="guoweisun_1-1746063442473.png" style="width: 400px;"&gt;&lt;img src="https://community.nxp.com/t5/image/serverpage/image-id/335929i5E5B1B3EEAE2D272/image-size/medium?v=v2&amp;amp;px=400" role="button" title="guoweisun_1-1746063442473.png" alt="guoweisun_1-1746063442473.png" /&gt;&lt;span class="lia-inline-image-caption" onclick="event.preventDefault();"&gt;guoweisun_1-1746063442473.png&lt;/span&gt;&lt;/span&gt;&lt;/P&gt;
&lt;P&gt;No monitoring the FCCU function&lt;/P&gt;
&lt;P&gt;&lt;span class="lia-inline-image-display-wrapper lia-image-align-inline" image-alt="guoweisun_2-1746063504282.png" style="width: 400px;"&gt;&lt;img src="https://community.nxp.com/t5/image/serverpage/image-id/335930iD53F5737E6F0602F/image-size/medium?v=v2&amp;amp;px=400" role="button" title="guoweisun_2-1746063504282.png" alt="guoweisun_2-1746063504282.png" /&gt;&lt;span class="lia-inline-image-caption" onclick="event.preventDefault();"&gt;guoweisun_2-1746063504282.png&lt;/span&gt;&lt;/span&gt;&lt;/P&gt;
&lt;P&gt;&amp;nbsp;&lt;/P&gt;
&lt;P&gt;&amp;nbsp;&lt;/P&gt;
&lt;P&gt;&amp;nbsp;&lt;/P&gt;</description>
      <pubDate>Thu, 01 May 2025 01:38:58 GMT</pubDate>
      <guid>https://community.nxp.com/t5/S32K/FS26-Not-Entering-Standby-amp-amp-Initialization-Fails-FS-STATE/m-p/2090519#M48376</guid>
      <dc:creator>guoweisun</dc:creator>
      <dc:date>2025-05-01T01:38:58Z</dc:date>
    </item>
    <item>
      <title>Re: FS26 Not Entering Standby &amp;amp; Initialization Fails – FS_STATE</title>
      <link>https://community.nxp.com/t5/S32K/FS26-Not-Entering-Standby-amp-amp-Initialization-Fails-FS-STATE/m-p/2091275#M48420</link>
      <description>&lt;P class=""&gt;Thank you for your response. I checked the suggested solution, but it was still showing the same issue. On further debugging, I found that the system was entering the INVALID_FS state and was not updating any configurations from the peripherals. I reviewed the default register values and identified the SBC_FS26_FS_GRL_FLAGS_ADDR register, which indicated an overvoltage fault. Upon checking the SBC_FS26_FS_OVUV_REG_STATUS_ADDR register, I saw that it was a VMON_EXT overvoltage condition. After adjusting the circuit connection and changing the resistance values, the issue was resolved. The system now transitions properly into the FS_Init state, and other operations are working as expected. Thanks again for your support.&lt;/P&gt;</description>
      <pubDate>Mon, 05 May 2025 07:42:22 GMT</pubDate>
      <guid>https://community.nxp.com/t5/S32K/FS26-Not-Entering-Standby-amp-amp-Initialization-Fails-FS-STATE/m-p/2091275#M48420</guid>
      <dc:creator>GaneshBhagwat</dc:creator>
      <dc:date>2025-05-05T07:42:22Z</dc:date>
    </item>
  </channel>
</rss>