<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>topic S32K142 CPU Type in S32K</title>
    <link>https://community.nxp.com/t5/S32K/S32K142-CPU-Type/m-p/924609#M4838</link>
    <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hi,&lt;/P&gt;&lt;P&gt;&amp;nbsp;&amp;nbsp;&amp;nbsp;I'm using S32K142 64-pin package, but I only find S32K142_100 100-pin package in SDK. How can I build a project of S32K142 64-pin package? Thanks!&amp;nbsp;&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
    <pubDate>Tue, 02 Jul 2019 02:33:01 GMT</pubDate>
    <dc:creator>jxl</dc:creator>
    <dc:date>2019-07-02T02:33:01Z</dc:date>
    <item>
      <title>S32K142 CPU Type</title>
      <link>https://community.nxp.com/t5/S32K/S32K142-CPU-Type/m-p/924609#M4838</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hi,&lt;/P&gt;&lt;P&gt;&amp;nbsp;&amp;nbsp;&amp;nbsp;I'm using S32K142 64-pin package, but I only find S32K142_100 100-pin package in SDK. How can I build a project of S32K142 64-pin package? Thanks!&amp;nbsp;&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Tue, 02 Jul 2019 02:33:01 GMT</pubDate>
      <guid>https://community.nxp.com/t5/S32K/S32K142-CPU-Type/m-p/924609#M4838</guid>
      <dc:creator>jxl</dc:creator>
      <dc:date>2019-07-02T02:33:01Z</dc:date>
    </item>
    <item>
      <title>Re: S32K142 CPU Type</title>
      <link>https://community.nxp.com/t5/S32K/S32K142-CPU-Type/m-p/924610#M4839</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hi,&lt;/P&gt;&lt;P&gt;&amp;nbsp;&amp;nbsp;&amp;nbsp;I have solved this problem, but there's another one.&amp;nbsp;&lt;/P&gt;&lt;P&gt;When I was debugging my project, it jumped to DefaultISR after ran the&amp;nbsp; PINS_DRV_Init(NUM_OF_CONFIGURED_PINS, g_pin_mux_InitConfigArr);&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;then I found it jumped to DefaultISR after ran the following assignment when I did single step debugging.&lt;/P&gt;&lt;P&gt;&lt;span class="lia-inline-image-display-wrapper"&gt;&lt;img src="https://community.nxp.com/t5/image/serverpage/image-id/90195iC3352482D451BC4B/image-size/large?v=v2&amp;amp;px=999" title="pastedImage_1.png" alt="pastedImage_1.png" /&gt;&lt;/span&gt;&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;I'm using S32K142 64-pin package for develop. What may cause this problem?&lt;/P&gt;&lt;P&gt;Thanks!&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Wed, 03 Jul 2019 02:08:00 GMT</pubDate>
      <guid>https://community.nxp.com/t5/S32K/S32K142-CPU-Type/m-p/924610#M4839</guid>
      <dc:creator>jxl</dc:creator>
      <dc:date>2019-07-03T02:08:00Z</dc:date>
    </item>
    <item>
      <title>Re: S32K142 CPU Type</title>
      <link>https://community.nxp.com/t5/S32K/S32K142-CPU-Type/m-p/924611#M4840</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hello,&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;What version of the SDK are you using? Could you please try to use the newest version available to see if the problem persists? Regarding on how to change the package on S32DS Processor Expert, please refer the following &lt;A _jive_internal="true" href="https://community.nxp.com/docs/DOC-334936"&gt;community document&lt;/A&gt;.&lt;/P&gt;&lt;P&gt;&lt;BR /&gt;Have a great day,&lt;BR /&gt;TIC&lt;/P&gt;&lt;P&gt;-------------------------------------------------------------------------------&lt;BR /&gt;Note:&lt;BR /&gt;- If this post answers your question, please click the "Mark Correct" button. Thank you!&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;- We are following threads for 7 weeks after the last post, later replies are ignored&lt;BR /&gt; Please open a new thread and refer to the closed one, if you have a related question at a later point in time.&lt;BR /&gt;-------------------------------------------------------------------------------&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Fri, 05 Jul 2019 16:04:55 GMT</pubDate>
      <guid>https://community.nxp.com/t5/S32K/S32K142-CPU-Type/m-p/924611#M4840</guid>
      <dc:creator>victorjimenez</dc:creator>
      <dc:date>2019-07-05T16:04:55Z</dc:date>
    </item>
    <item>
      <title>Re: S32K142 CPU Type</title>
      <link>https://community.nxp.com/t5/S32K/S32K142-CPU-Type/m-p/1185249#M8886</link>
      <description>&lt;P&gt;Please check out the SOSC_CLK setup. Make sure the setting frequency is consistent with the crystal you actually used in the circuit. Further, The SOSC "High-gain Oscillator Select" must be set properly. You can switch the mode and check out whether the&amp;nbsp; "stuck in&amp;nbsp;&lt;SPAN&gt;DefaultISR&lt;/SPAN&gt;" problem exist.&lt;/P&gt;</description>
      <pubDate>Thu, 19 Nov 2020 02:03:44 GMT</pubDate>
      <guid>https://community.nxp.com/t5/S32K/S32K142-CPU-Type/m-p/1185249#M8886</guid>
      <dc:creator>irvinwu</dc:creator>
      <dc:date>2020-11-19T02:03:44Z</dc:date>
    </item>
  </channel>
</rss>