<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>S32KのトピックS32K3 Firmware Update</title>
    <link>https://community.nxp.com/t5/S32K/S32K3-Firmware-Update/m-p/2090573#M48379</link>
    <description>&lt;P&gt;&lt;SPAN&gt;Hello,&lt;/SPAN&gt;&lt;BR /&gt;&lt;BR /&gt;&lt;SPAN&gt;Could you please provide the S32K3XX Firmware Update Application Note, similar to the S32K1XX Firmware Updates Application Note (&lt;A href="https://www.nxp.com/docs/en/application-note/AN12323.pdf?_gl=1*14po2at*_ga*MTYzNTY5MjQ0My4xNzQzNjgyNzQy*_ga_WM5LE0KMSH*MTc0NTk4NTAxNS41Ny4xLjE3NDU5ODU2NTkuMC4wLjA." target="_blank"&gt;AN12323: S32K1xx Firmware updates – Application Note&lt;/A&gt;)?&lt;/SPAN&gt;&lt;BR /&gt;&lt;BR /&gt;&lt;SPAN&gt;It would be greatly appreciated!&lt;/SPAN&gt;&lt;BR /&gt;&lt;BR /&gt;&lt;SPAN&gt;Thanks !.&lt;/SPAN&gt;&lt;/P&gt;</description>
    <pubDate>Thu, 01 May 2025 11:14:13 GMT</pubDate>
    <dc:creator>DiaDev</dc:creator>
    <dc:date>2025-05-01T11:14:13Z</dc:date>
    <item>
      <title>S32K3 Firmware Update</title>
      <link>https://community.nxp.com/t5/S32K/S32K3-Firmware-Update/m-p/2090573#M48379</link>
      <description>&lt;P&gt;&lt;SPAN&gt;Hello,&lt;/SPAN&gt;&lt;BR /&gt;&lt;BR /&gt;&lt;SPAN&gt;Could you please provide the S32K3XX Firmware Update Application Note, similar to the S32K1XX Firmware Updates Application Note (&lt;A href="https://www.nxp.com/docs/en/application-note/AN12323.pdf?_gl=1*14po2at*_ga*MTYzNTY5MjQ0My4xNzQzNjgyNzQy*_ga_WM5LE0KMSH*MTc0NTk4NTAxNS41Ny4xLjE3NDU5ODU2NTkuMC4wLjA." target="_blank"&gt;AN12323: S32K1xx Firmware updates – Application Note&lt;/A&gt;)?&lt;/SPAN&gt;&lt;BR /&gt;&lt;BR /&gt;&lt;SPAN&gt;It would be greatly appreciated!&lt;/SPAN&gt;&lt;BR /&gt;&lt;BR /&gt;&lt;SPAN&gt;Thanks !.&lt;/SPAN&gt;&lt;/P&gt;</description>
      <pubDate>Thu, 01 May 2025 11:14:13 GMT</pubDate>
      <guid>https://community.nxp.com/t5/S32K/S32K3-Firmware-Update/m-p/2090573#M48379</guid>
      <dc:creator>DiaDev</dc:creator>
      <dc:date>2025-05-01T11:14:13Z</dc:date>
    </item>
    <item>
      <title>Re: S32K3 Firmware Update</title>
      <link>https://community.nxp.com/t5/S32K/S32K3-Firmware-Update/m-p/2091018#M48399</link>
      <description>&lt;P&gt;Hi&amp;nbsp;&lt;a href="https://community.nxp.com/t5/user/viewprofilepage/user-id/248971"&gt;@DiaDev&lt;/a&gt;&lt;/P&gt;
&lt;P&gt;There is no direct application note for the S32K3XX devices as with the S32K1XX; However, there are some ANs and examples for FW updates:&lt;/P&gt;
&lt;P&gt;Under the &lt;A href="https://www.nxp.com/webapp/Download?colCode=S32K3_HSE_DemoExamples" target="_self"&gt;S32K3 HSE Demo Examples&lt;/A&gt;, there is the Secure boot &amp;amp; Device configuration examples, which showcase basic/advanced secure boot, HSE installation (FULL_MEM &amp;amp; AB SWAP), along with other functionalities.&lt;/P&gt;
&lt;P&gt;There is also the&amp;nbsp;&lt;SPAN&gt;OTA DEMO application which can be found in S32K3 Reference Software:&amp;nbsp;&lt;/SPAN&gt;&lt;SPAN&gt;&lt;A href="https://www.nxp.com/webapp/swlicensing/sso/downloadSoftware.sp?catid=SW32K3-REFSW-D" target="_blank" rel="nofollow noopener noreferrer"&gt;SW32K3-REFSW-D.&lt;/A&gt;&lt;/SPAN&gt;&lt;/P&gt;
&lt;P&gt;Finally, you can also refer to the&amp;nbsp;&lt;A href="https://community.nxp.com/t5/S32K-Knowledge-Base/Unified-bootloader-Demo/ta-p/1423099" target="_blank"&gt;Unified bootloader Demo&lt;/A&gt;&amp;nbsp;&amp;amp; the&amp;nbsp;&lt;A href="https://community.nxp.com/t5/S32K-Knowledge-Base/Example-S32K312-Bootloader-to-Application-Jump-DS3-5-RTD300/ta-p/1809810" target="_blank"&gt;Example S32K312 Bootloader to Application Jump DS3.5 RTD300&lt;/A&gt; from the community.&lt;/P&gt;
&lt;P&gt;Hope this helps &amp;amp; best regards,&lt;BR /&gt;Julián&lt;/P&gt;
&lt;P&gt;&amp;nbsp;&lt;/P&gt;</description>
      <pubDate>Fri, 02 May 2025 17:27:34 GMT</pubDate>
      <guid>https://community.nxp.com/t5/S32K/S32K3-Firmware-Update/m-p/2091018#M48399</guid>
      <dc:creator>Julián_AragónM</dc:creator>
      <dc:date>2025-05-02T17:27:34Z</dc:date>
    </item>
  </channel>
</rss>