<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>S32KのトピックRe: S32K312 boot with HSE enabled</title>
    <link>https://community.nxp.com/t5/S32K/S32K312-boot-with-HSE-enabled/m-p/2089135#M48275</link>
    <description>&lt;P&gt;I solved the issue by updating my debugger client (PLS UDE) to version 2024.05&lt;/P&gt;</description>
    <pubDate>Tue, 29 Apr 2025 08:17:59 GMT</pubDate>
    <dc:creator>strofald</dc:creator>
    <dc:date>2025-04-29T08:17:59Z</dc:date>
    <item>
      <title>S32K312 boot with HSE enabled</title>
      <link>https://community.nxp.com/t5/S32K/S32K312-boot-with-HSE-enabled/m-p/2085758#M48078</link>
      <description>&lt;P&gt;Hello,&lt;/P&gt;&lt;P&gt;I have flashed HSE FW on my S32K312 microcontroller, and I have enabled the HSE FW Feature flag in UTEST.&lt;BR /&gt;Anyway I experience the following: whenever I flash a new application FW, right after flashing if I step with the debugger (without executing any instruction, just the first one from the startup code), an Hard Fault is triggered. If instead, after flashing, I perform a reset with the debugger, the Hard Fault does not happen.&lt;BR /&gt;How is this possible?&lt;/P&gt;&lt;P&gt;May this be related with the IVT configuration?&lt;BR /&gt;I am using the standard linker and startup files that are provided with the Platform module in RTD v5.0.0, I attached them below (renamed in .s.c due to update policies)&lt;BR /&gt;I also uploaded the .map file of the application.&lt;/P&gt;</description>
      <pubDate>Wed, 23 Apr 2025 18:38:32 GMT</pubDate>
      <guid>https://community.nxp.com/t5/S32K/S32K312-boot-with-HSE-enabled/m-p/2085758#M48078</guid>
      <dc:creator>strofald</dc:creator>
      <dc:date>2025-04-23T18:38:32Z</dc:date>
    </item>
    <item>
      <title>Re: S32K312 boot with HSE enabled</title>
      <link>https://community.nxp.com/t5/S32K/S32K312-boot-with-HSE-enabled/m-p/2086491#M48114</link>
      <description>&lt;P&gt;Hi &lt;a href="https://community.nxp.com/t5/user/viewprofilepage/user-id/229151"&gt;@strofald&lt;/a&gt;&amp;nbsp;&lt;/P&gt;
&lt;P&gt;I have never seen such behavior and I can't see a reason for that. &lt;/P&gt;
&lt;P&gt;What kind of debugger do you use? It sound like problem of debugger...&lt;/P&gt;
&lt;P&gt;Regards,&lt;/P&gt;
&lt;P&gt;Lukas&lt;/P&gt;</description>
      <pubDate>Thu, 24 Apr 2025 09:47:57 GMT</pubDate>
      <guid>https://community.nxp.com/t5/S32K/S32K312-boot-with-HSE-enabled/m-p/2086491#M48114</guid>
      <dc:creator>lukaszadrapa</dc:creator>
      <dc:date>2025-04-24T09:47:57Z</dc:date>
    </item>
    <item>
      <title>Re: S32K312 boot with HSE enabled</title>
      <link>https://community.nxp.com/t5/S32K/S32K312-boot-with-HSE-enabled/m-p/2089135#M48275</link>
      <description>&lt;P&gt;I solved the issue by updating my debugger client (PLS UDE) to version 2024.05&lt;/P&gt;</description>
      <pubDate>Tue, 29 Apr 2025 08:17:59 GMT</pubDate>
      <guid>https://community.nxp.com/t5/S32K/S32K312-boot-with-HSE-enabled/m-p/2089135#M48275</guid>
      <dc:creator>strofald</dc:creator>
      <dc:date>2025-04-29T08:17:59Z</dc:date>
    </item>
  </channel>
</rss>