<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>topic Re: Timeout for FTFC operations in S32K</title>
    <link>https://community.nxp.com/t5/S32K/Timeout-for-FTFC-operations/m-p/922918#M4811</link>
    <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hello, &lt;BR /&gt;This is specified in the S32K1xx Datasheet rev.9.&lt;BR /&gt;Table 23. Flash command timing specifications for S32K14x&lt;BR /&gt;Table 24. Flash command timing specifications for S32K11x&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;BR, Daniel &lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
    <pubDate>Thu, 30 May 2019 08:15:21 GMT</pubDate>
    <dc:creator>danielmartynek</dc:creator>
    <dc:date>2019-05-30T08:15:21Z</dc:date>
    <item>
      <title>Timeout for FTFC operations</title>
      <link>https://community.nxp.com/t5/S32K/Timeout-for-FTFC-operations/m-p/922917#M4810</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hello,&lt;/P&gt;&lt;P&gt;&amp;nbsp;&amp;nbsp;&amp;nbsp;In the sample code, before doing a flash operation (Or any FTFC operation) we are checking the command complete flag.&amp;nbsp;&lt;/P&gt;&lt;P&gt;&amp;nbsp; &amp;nbsp; &amp;nbsp; &amp;nbsp; &amp;nbsp; &amp;nbsp; &amp;nbsp; &amp;nbsp; &amp;nbsp; &amp;nbsp; &amp;nbsp; &amp;nbsp; &lt;EM&gt;while(0 == (FTFx_FSTAT &amp;amp; FTFx_FSTAT_CCIF_MASK));&lt;/EM&gt;&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;But since it is an infinite loop, I would like to add a specific timeout here to make sure that the program flow is &lt;STRONG&gt;not&lt;/STRONG&gt; stuck here for ever. So&amp;nbsp;I would like to know is there any specification for the command execution time for FTFC commands available?&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;My aim is to add a timeout in these places , so that I can do some recovery actions after timeout.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Thanks&lt;/P&gt;&lt;P&gt;Ummer K&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Wed, 29 May 2019 11:48:58 GMT</pubDate>
      <guid>https://community.nxp.com/t5/S32K/Timeout-for-FTFC-operations/m-p/922917#M4810</guid>
      <dc:creator>ummerkunnummalk</dc:creator>
      <dc:date>2019-05-29T11:48:58Z</dc:date>
    </item>
    <item>
      <title>Re: Timeout for FTFC operations</title>
      <link>https://community.nxp.com/t5/S32K/Timeout-for-FTFC-operations/m-p/922918#M4811</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hello, &lt;BR /&gt;This is specified in the S32K1xx Datasheet rev.9.&lt;BR /&gt;Table 23. Flash command timing specifications for S32K14x&lt;BR /&gt;Table 24. Flash command timing specifications for S32K11x&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;BR, Daniel &lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Thu, 30 May 2019 08:15:21 GMT</pubDate>
      <guid>https://community.nxp.com/t5/S32K/Timeout-for-FTFC-operations/m-p/922918#M4811</guid>
      <dc:creator>danielmartynek</dc:creator>
      <dc:date>2019-05-30T08:15:21Z</dc:date>
    </item>
  </channel>
</rss>