<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>S32K中的主题 Re: LIN Communication with Flexio_Lin</title>
    <link>https://community.nxp.com/t5/S32K/LIN-Communication-with-Flexio-Lin/m-p/2085324#M48054</link>
    <description>&lt;P&gt;Can you clarify how to select the Pin &amp;amp; Channel of FlexIO for LIN ?&amp;nbsp;&lt;BR /&gt;&lt;BR /&gt;&lt;/P&gt;&lt;P&gt;&lt;span class="lia-inline-image-display-wrapper lia-image-align-inline" image-alt="ASN7_0-1745399998352.png" style="width: 400px;"&gt;&lt;img src="https://community.nxp.com/t5/image/serverpage/image-id/334461i1D2752B485327E6B/image-size/medium?v=v2&amp;amp;px=400" role="button" title="ASN7_0-1745399998352.png" alt="ASN7_0-1745399998352.png" /&gt;&lt;span class="lia-inline-image-caption" onclick="event.preventDefault();"&gt;ASN7_0-1745399998352.png&lt;/span&gt;&lt;/span&gt;&lt;/P&gt;&lt;P&gt;&lt;BR /&gt;For example I select PTE0 as LIN_RX which is FXIO_D3 and PTE1 as LIN_TX which is FXIO_D2, what are the channel and respective pin numbers for S32K314 ?&amp;nbsp;&lt;BR /&gt;&lt;BR /&gt;I get the issue because I see multiple FXIO_Dx for each FXIO pins.&amp;nbsp;&lt;/P&gt;</description>
    <pubDate>Wed, 23 Apr 2025 09:22:36 GMT</pubDate>
    <dc:creator>ASN7</dc:creator>
    <dc:date>2025-04-23T09:22:36Z</dc:date>
    <item>
      <title>LIN Communication with Flexio_Lin</title>
      <link>https://community.nxp.com/t5/S32K/LIN-Communication-with-Flexio-Lin/m-p/1993660#M43233</link>
      <description>&lt;P&gt;I have custom board of S32K314_172HDQFP with TJA1029 LIN Transceiver. The TX and RX are assigned to PTA8 and PTA9 which correspond to FXIO_D6 and FXIO_D7 respectively.&lt;/P&gt;&lt;P&gt;&lt;span class="lia-inline-image-display-wrapper lia-image-align-inline" image-alt="ASN7_2-1731495546903.png" style="width: 400px;"&gt;&lt;img src="https://community.nxp.com/t5/image/serverpage/image-id/310276iC7281268AFD513AE/image-size/medium?v=v2&amp;amp;px=400" role="button" title="ASN7_2-1731495546903.png" alt="ASN7_2-1731495546903.png" /&gt;&lt;span class="lia-inline-image-caption" onclick="event.preventDefault();"&gt;ASN7_2-1731495546903.png&lt;/span&gt;&lt;/span&gt;&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;Now I add the Flexio_Mcl_Ip and then under Specific Configuration Tab, I select Logic Channel 0 for Tx and select Flexio Pin as PIN_6 and respectively Flexio Logic Channel 1 for Pin_7. Under Flexio_Lin Driver and under the Lin Global Config Tab, I select Lin hardware FLEXIO_IP_0, and then Rx and Tx Channel as shown in the image below.&lt;/P&gt;&lt;P&gt;&lt;span class="lia-inline-image-display-wrapper lia-image-align-inline" image-alt="ASN7_1-1731495505011.png" style="width: 400px;"&gt;&lt;img src="https://community.nxp.com/t5/image/serverpage/image-id/310275iD6F9F5D6827AAF1E/image-size/medium?v=v2&amp;amp;px=400" role="button" title="ASN7_1-1731495505011.png" alt="ASN7_1-1731495505011.png" /&gt;&lt;span class="lia-inline-image-caption" onclick="event.preventDefault();"&gt;ASN7_1-1731495505011.png&lt;/span&gt;&lt;/span&gt;&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;&lt;span class="lia-inline-image-display-wrapper lia-image-align-inline" image-alt="ASN7_0-1731495492754.png" style="width: 400px;"&gt;&lt;img src="https://community.nxp.com/t5/image/serverpage/image-id/310274i9B70C804301A8A6A/image-size/medium?v=v2&amp;amp;px=400" role="button" title="ASN7_0-1731495492754.png" alt="ASN7_0-1731495492754.png" /&gt;&lt;span class="lia-inline-image-caption" onclick="event.preventDefault();"&gt;ASN7_0-1731495492754.png&lt;/span&gt;&lt;/span&gt;&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;Irrespective of the TJA1029, I should be able to see the output from the MCU on my logic analyser right, but I just see one pulse. Is there something that I am missing ?&lt;/P&gt;&lt;P&gt;&lt;span class="lia-inline-image-display-wrapper lia-image-align-inline" image-alt="ASN7_3-1731495788070.png" style="width: 400px;"&gt;&lt;img src="https://community.nxp.com/t5/image/serverpage/image-id/310278iABE4C9779436E82B/image-size/medium?v=v2&amp;amp;px=400" role="button" title="ASN7_3-1731495788070.png" alt="ASN7_3-1731495788070.png" /&gt;&lt;span class="lia-inline-image-caption" onclick="event.preventDefault();"&gt;ASN7_3-1731495788070.png&lt;/span&gt;&lt;/span&gt;&lt;/P&gt;&lt;P&gt;Since I cannot share my complete code, I have attached the part of code related to LIN which I have taken from the example code "Lin_Ip_FrameTransfer_S32K344".&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;</description>
      <pubDate>Wed, 13 Nov 2024 11:04:00 GMT</pubDate>
      <guid>https://community.nxp.com/t5/S32K/LIN-Communication-with-Flexio-Lin/m-p/1993660#M43233</guid>
      <dc:creator>ASN7</dc:creator>
      <dc:date>2024-11-13T11:04:00Z</dc:date>
    </item>
    <item>
      <title>Re: LIN Communication with Flexio_Lin</title>
      <link>https://community.nxp.com/t5/S32K/LIN-Communication-with-Flexio-Lin/m-p/1993662#M43234</link>
      <description>&lt;P&gt;I do not know why the code was not attached. But I have attached it here.&amp;nbsp;&lt;/P&gt;</description>
      <pubDate>Wed, 13 Nov 2024 11:06:38 GMT</pubDate>
      <guid>https://community.nxp.com/t5/S32K/LIN-Communication-with-Flexio-Lin/m-p/1993662#M43234</guid>
      <dc:creator>ASN7</dc:creator>
      <dc:date>2024-11-13T11:06:38Z</dc:date>
    </item>
    <item>
      <title>Re: LIN Communication with Flexio_Lin</title>
      <link>https://community.nxp.com/t5/S32K/LIN-Communication-with-Flexio-Lin/m-p/1995437#M43337</link>
      <description>&lt;P&gt;Hi,&lt;/P&gt;
&lt;P&gt;&lt;SPAN&gt;it looks like driver interrupt is not installed and called so next frame bytes are not processed. Try to check that. Also discussed on&amp;nbsp;&lt;A href="https://community.nxp.com/t5/S32K/S32K324-Lpuart-lin-Master-Continually-Returning-Status-quot/m-p/1843988" target="_blank"&gt;https://community.nxp.com/t5/S32K/S32K324-Lpuart-lin-Master-Continually-Returning-Status-quot/m-p/1843988&lt;/A&gt;&lt;/SPAN&gt;&lt;/P&gt;
&lt;P&gt;&lt;SPAN&gt;Also LIN transceiver must be connected and active. IF testing without transceiver you need to connect TX to RX.&lt;/SPAN&gt;&lt;/P&gt;
&lt;P&gt;&lt;SPAN&gt;BR, Petr&lt;/SPAN&gt;&lt;/P&gt;</description>
      <pubDate>Fri, 15 Nov 2024 11:56:55 GMT</pubDate>
      <guid>https://community.nxp.com/t5/S32K/LIN-Communication-with-Flexio-Lin/m-p/1995437#M43337</guid>
      <dc:creator>PetrS</dc:creator>
      <dc:date>2024-11-15T11:56:55Z</dc:date>
    </item>
    <item>
      <title>Re: LIN Communication with Flexio_Lin</title>
      <link>https://community.nxp.com/t5/S32K/LIN-Communication-with-Flexio-Lin/m-p/2085324#M48054</link>
      <description>&lt;P&gt;Can you clarify how to select the Pin &amp;amp; Channel of FlexIO for LIN ?&amp;nbsp;&lt;BR /&gt;&lt;BR /&gt;&lt;/P&gt;&lt;P&gt;&lt;span class="lia-inline-image-display-wrapper lia-image-align-inline" image-alt="ASN7_0-1745399998352.png" style="width: 400px;"&gt;&lt;img src="https://community.nxp.com/t5/image/serverpage/image-id/334461i1D2752B485327E6B/image-size/medium?v=v2&amp;amp;px=400" role="button" title="ASN7_0-1745399998352.png" alt="ASN7_0-1745399998352.png" /&gt;&lt;span class="lia-inline-image-caption" onclick="event.preventDefault();"&gt;ASN7_0-1745399998352.png&lt;/span&gt;&lt;/span&gt;&lt;/P&gt;&lt;P&gt;&lt;BR /&gt;For example I select PTE0 as LIN_RX which is FXIO_D3 and PTE1 as LIN_TX which is FXIO_D2, what are the channel and respective pin numbers for S32K314 ?&amp;nbsp;&lt;BR /&gt;&lt;BR /&gt;I get the issue because I see multiple FXIO_Dx for each FXIO pins.&amp;nbsp;&lt;/P&gt;</description>
      <pubDate>Wed, 23 Apr 2025 09:22:36 GMT</pubDate>
      <guid>https://community.nxp.com/t5/S32K/LIN-Communication-with-Flexio-Lin/m-p/2085324#M48054</guid>
      <dc:creator>ASN7</dc:creator>
      <dc:date>2025-04-23T09:22:36Z</dc:date>
    </item>
  </channel>
</rss>