<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>S32KのトピックRe: S32k314 Timer</title>
    <link>https://community.nxp.com/t5/S32K/S32k314-Timer/m-p/2085024#M48031</link>
    <description>&lt;P class=""&gt;Thank you for your reply.&lt;/P&gt;&lt;P class=""&gt;&amp;nbsp;&lt;/P&gt;&lt;P class=""&gt;I tested adding the STM1 module, but the S32k314 board doesn’t boot properly when it runs GPT Init.&lt;/P&gt;&lt;P class=""&gt;&lt;BR /&gt;After looking into it, I found out that the S32K314 doesn’t actually have a clock for STM1.&lt;/P&gt;&lt;P class=""&gt;&amp;nbsp;&lt;/P&gt;&lt;P class=""&gt;As a result, after&amp;nbsp;removing STM1,&amp;nbsp; the S32k314 board boot normally,&lt;/P&gt;&lt;P class=""&gt;&lt;BR /&gt;It operation doesn’t match what’s described in the S32k3xx reference manual.&lt;/P&gt;</description>
    <pubDate>Wed, 23 Apr 2025 02:47:54 GMT</pubDate>
    <dc:creator>dpsdprtmvl</dc:creator>
    <dc:date>2025-04-23T02:47:54Z</dc:date>
    <item>
      <title>S32k314 Timer</title>
      <link>https://community.nxp.com/t5/S32K/S32k314-Timer/m-p/2081183#M47799</link>
      <description>&lt;P&gt;Dear All,&lt;/P&gt;&lt;P&gt;Hello, I using S32k314 board (RTD3.0.0), but i have a question about STM in GPT module.&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;According to S32k3xx RM.pdf,&amp;nbsp; I found S32k314 allowed 2 instances of STM, STM_0 and STM_1 .&lt;/P&gt;&lt;P&gt;&lt;span class="lia-inline-image-display-wrapper lia-image-align-inline" image-alt="dpsdprtmvl_0-1742085963865.png" style="width: 400px;"&gt;&lt;img src="https://community.nxp.com/t5/image/serverpage/image-id/333290iB6ADCB408F68C1DA/image-size/medium?v=v2&amp;amp;px=400" role="button" title="dpsdprtmvl_0-1742085963865.png" alt="dpsdprtmvl_0-1742085963865.png" /&gt;&lt;span class="lia-inline-image-caption" onclick="event.preventDefault();"&gt;dpsdprtmvl_0-1742085963865.png&lt;/span&gt;&lt;/span&gt;&lt;/P&gt;&lt;P&gt;But, S32k314 don't have a clock about STM_1 in example code at design studio 3.5 version.&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;I wonder&amp;nbsp;"S32K314 also supports STM_1, but why is there no clock configuration for STM_1 in the example code?"&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;Thanks.&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;</description>
      <pubDate>Wed, 16 Apr 2025 01:19:05 GMT</pubDate>
      <guid>https://community.nxp.com/t5/S32K/S32k314-Timer/m-p/2081183#M47799</guid>
      <dc:creator>dpsdprtmvl</dc:creator>
      <dc:date>2025-04-16T01:19:05Z</dc:date>
    </item>
    <item>
      <title>Re: S32k314 Timer</title>
      <link>https://community.nxp.com/t5/S32K/S32k314-Timer/m-p/2081573#M47819</link>
      <description>&lt;P&gt;Hello,&lt;/P&gt;
&lt;P&gt;Example code usually implement only basic demo features to show the functionality.&lt;/P&gt;
&lt;BLOCKQUOTE&gt;
&lt;P&gt;I wonder "S32K314 also supports STM_1, but why is there no clock configuration for STM_1 in the example code?"&lt;/P&gt;
&lt;/BLOCKQUOTE&gt;
&lt;P&gt;I have just open the example for GPT and simply added STM0 and 1 modules and everything works as expected. Both are supported.&lt;/P&gt;
&lt;P&gt;&lt;span class="lia-inline-image-display-wrapper lia-image-align-inline" image-alt="petervlna_0-1744792924522.png" style="width: 400px;"&gt;&lt;img src="https://community.nxp.com/t5/image/serverpage/image-id/333424i192F147024E4CD45/image-size/medium?v=v2&amp;amp;px=400" role="button" title="petervlna_0-1744792924522.png" alt="petervlna_0-1744792924522.png" /&gt;&lt;span class="lia-inline-image-caption" onclick="event.preventDefault();"&gt;petervlna_0-1744792924522.png&lt;/span&gt;&lt;/span&gt;&lt;/P&gt;
&lt;P&gt;&lt;span class="lia-inline-image-display-wrapper lia-image-align-inline" image-alt="petervlna_1-1744792939153.png" style="width: 400px;"&gt;&lt;img src="https://community.nxp.com/t5/image/serverpage/image-id/333425i3171EF0C9DA0F24F/image-size/medium?v=v2&amp;amp;px=400" role="button" title="petervlna_1-1744792939153.png" alt="petervlna_1-1744792939153.png" /&gt;&lt;span class="lia-inline-image-caption" onclick="event.preventDefault();"&gt;petervlna_1-1744792939153.png&lt;/span&gt;&lt;/span&gt;&lt;/P&gt;
&lt;P&gt;Simply follow the example or screenshot above and add STM1.&lt;/P&gt;
&lt;P&gt;Best regards,&lt;/P&gt;
&lt;P&gt;Peter&lt;/P&gt;</description>
      <pubDate>Wed, 16 Apr 2025 08:43:01 GMT</pubDate>
      <guid>https://community.nxp.com/t5/S32K/S32k314-Timer/m-p/2081573#M47819</guid>
      <dc:creator>petervlna</dc:creator>
      <dc:date>2025-04-16T08:43:01Z</dc:date>
    </item>
    <item>
      <title>Re: S32k314 Timer</title>
      <link>https://community.nxp.com/t5/S32K/S32k314-Timer/m-p/2085024#M48031</link>
      <description>&lt;P class=""&gt;Thank you for your reply.&lt;/P&gt;&lt;P class=""&gt;&amp;nbsp;&lt;/P&gt;&lt;P class=""&gt;I tested adding the STM1 module, but the S32k314 board doesn’t boot properly when it runs GPT Init.&lt;/P&gt;&lt;P class=""&gt;&lt;BR /&gt;After looking into it, I found out that the S32K314 doesn’t actually have a clock for STM1.&lt;/P&gt;&lt;P class=""&gt;&amp;nbsp;&lt;/P&gt;&lt;P class=""&gt;As a result, after&amp;nbsp;removing STM1,&amp;nbsp; the S32k314 board boot normally,&lt;/P&gt;&lt;P class=""&gt;&lt;BR /&gt;It operation doesn’t match what’s described in the S32k3xx reference manual.&lt;/P&gt;</description>
      <pubDate>Wed, 23 Apr 2025 02:47:54 GMT</pubDate>
      <guid>https://community.nxp.com/t5/S32K/S32k314-Timer/m-p/2085024#M48031</guid>
      <dc:creator>dpsdprtmvl</dc:creator>
      <dc:date>2025-04-23T02:47:54Z</dc:date>
    </item>
    <item>
      <title>Re: S32k314 Timer</title>
      <link>https://community.nxp.com/t5/S32K/S32k314-Timer/m-p/2085210#M48046</link>
      <description>&lt;P&gt;Hello,&lt;/P&gt;
&lt;P&gt;Ok, but once you configure clock you also have to enable it to the peripheral.&lt;/P&gt;
&lt;P&gt;Did you enabled it in ME module for STM0 and 1?&lt;/P&gt;
&lt;P&gt;It is in MCU plugin:&lt;/P&gt;
&lt;P&gt;&lt;span class="lia-inline-image-display-wrapper lia-image-align-inline" image-alt="petervlna_0-1745393794182.png" style="width: 738px;"&gt;&lt;img src="https://community.nxp.com/t5/image/serverpage/image-id/334433iBE7AE4DA3F7FC23C/image-dimensions/738x558?v=v2" width="738" height="558" role="button" title="petervlna_0-1745393794182.png" alt="petervlna_0-1745393794182.png" /&gt;&lt;span class="lia-inline-image-caption" onclick="event.preventDefault();"&gt;petervlna_0-1745393794182.png&lt;/span&gt;&lt;/span&gt;&lt;/P&gt;
&lt;P&gt;I have tested it here and everything is running as expected:&lt;/P&gt;
&lt;P&gt;&lt;span class="lia-inline-image-display-wrapper lia-image-align-inline" image-alt="petervlna_1-1745393824869.png" style="width: 676px;"&gt;&lt;img src="https://community.nxp.com/t5/image/serverpage/image-id/334434i0AE08A0B33C18F39/image-dimensions/676x256?v=v2" width="676" height="256" role="button" title="petervlna_1-1745393824869.png" alt="petervlna_1-1745393824869.png" /&gt;&lt;span class="lia-inline-image-caption" onclick="event.preventDefault();"&gt;petervlna_1-1745393824869.png&lt;/span&gt;&lt;/span&gt;&lt;/P&gt;
&lt;P&gt;&amp;nbsp;&lt;/P&gt;
&lt;P&gt;Attached is the example file if you like to test it&lt;/P&gt;
&lt;P&gt;Best regards,&lt;/P&gt;
&lt;P&gt;Peter&lt;/P&gt;</description>
      <pubDate>Wed, 23 Apr 2025 07:38:27 GMT</pubDate>
      <guid>https://community.nxp.com/t5/S32K/S32k314-Timer/m-p/2085210#M48046</guid>
      <dc:creator>petervlna</dc:creator>
      <dc:date>2025-04-23T07:38:27Z</dc:date>
    </item>
  </channel>
</rss>