<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>topic hse_interface.h missing from CRYPTO_43_HSE in S32K</title>
    <link>https://community.nxp.com/t5/S32K/hse-interface-h-missing-from-CRYPTO-43-HSE/m-p/2084508#M47986</link>
    <description>&lt;P&gt;Hello,&lt;/P&gt;&lt;P&gt;I want to try to encrypt some messages using the HSE, I've configured the CRYPTO_43_HSE to use the AES cypher. After updating the code in the peripherals, it says that the hse_interface.h file is missing.&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;My target device is the S32K342, and I'm using RTD's 4.0.0. Is there any way to solve this?&lt;/P&gt;&lt;P&gt;Thank you in advance&lt;/P&gt;</description>
    <pubDate>Tue, 22 Apr 2025 09:40:15 GMT</pubDate>
    <dc:creator>Rmpr</dc:creator>
    <dc:date>2025-04-22T09:40:15Z</dc:date>
    <item>
      <title>hse_interface.h missing from CRYPTO_43_HSE</title>
      <link>https://community.nxp.com/t5/S32K/hse-interface-h-missing-from-CRYPTO-43-HSE/m-p/2084508#M47986</link>
      <description>&lt;P&gt;Hello,&lt;/P&gt;&lt;P&gt;I want to try to encrypt some messages using the HSE, I've configured the CRYPTO_43_HSE to use the AES cypher. After updating the code in the peripherals, it says that the hse_interface.h file is missing.&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;My target device is the S32K342, and I'm using RTD's 4.0.0. Is there any way to solve this?&lt;/P&gt;&lt;P&gt;Thank you in advance&lt;/P&gt;</description>
      <pubDate>Tue, 22 Apr 2025 09:40:15 GMT</pubDate>
      <guid>https://community.nxp.com/t5/S32K/hse-interface-h-missing-from-CRYPTO-43-HSE/m-p/2084508#M47986</guid>
      <dc:creator>Rmpr</dc:creator>
      <dc:date>2025-04-22T09:40:15Z</dc:date>
    </item>
    <item>
      <title>Re: hse_interface.h missing from CRYPTO_43_HSE</title>
      <link>https://community.nxp.com/t5/S32K/hse-interface-h-missing-from-CRYPTO-43-HSE/m-p/2084595#M48000</link>
      <description>&lt;P&gt;Hi &lt;a href="https://community.nxp.com/t5/user/viewprofilepage/user-id/220829"&gt;@Rmpr&lt;/a&gt;&amp;nbsp;&lt;/P&gt;
&lt;P&gt;Please take a look at section "3.2.0.0.8 HSE Interface Files:" in the Crypto Integration Manual which can be found at this path:&lt;/P&gt;
&lt;P&gt;c:\NXP\S32DS.3.5\S32DS\software\PlatformSDK_S32K3\RTD\Crypto_43_HSE_TS_T40D34M40I0R0\doc\RTD_CRYPTO_43_HSE_IM.pdf&lt;/P&gt;
&lt;P&gt;It says that interface files need to be copied from HSE Firmware folder like this (just an example, it depends on used firmware version):&lt;/P&gt;
&lt;P&gt;c:\NXP\HSE_FW_S32K344_0_2_40_0\hse_ab_swap\interface\&lt;/P&gt;
&lt;P&gt;Regards,&lt;/P&gt;
&lt;P&gt;Lukas&lt;/P&gt;</description>
      <pubDate>Tue, 22 Apr 2025 11:24:21 GMT</pubDate>
      <guid>https://community.nxp.com/t5/S32K/hse-interface-h-missing-from-CRYPTO-43-HSE/m-p/2084595#M48000</guid>
      <dc:creator>lukaszadrapa</dc:creator>
      <dc:date>2025-04-22T11:24:21Z</dc:date>
    </item>
    <item>
      <title>Re: hse_interface.h missing from CRYPTO_43_HSE</title>
      <link>https://community.nxp.com/t5/S32K/hse-interface-h-missing-from-CRYPTO-43-HSE/m-p/2084611#M48002</link>
      <description>&lt;P&gt;I've located the files, but it doesn't say where I should copy them to.&lt;/P&gt;</description>
      <pubDate>Tue, 22 Apr 2025 11:54:51 GMT</pubDate>
      <guid>https://community.nxp.com/t5/S32K/hse-interface-h-missing-from-CRYPTO-43-HSE/m-p/2084611#M48002</guid>
      <dc:creator>Rmpr</dc:creator>
      <dc:date>2025-04-22T11:54:51Z</dc:date>
    </item>
  </channel>
</rss>