<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>topic Re: SENT TX emulation using FLEXIO or EMIOS in S32K</title>
    <link>https://community.nxp.com/t5/S32K/SENT-TX-emulation-using-FLEXIO-or-EMIOS/m-p/2082199#M47863</link>
    <description>&lt;P&gt;Hi&amp;nbsp;&lt;a href="https://community.nxp.com/t5/user/viewprofilepage/user-id/213150"&gt;@UmaMaheswaraReddy&lt;/a&gt;&amp;nbsp;,&lt;BR /&gt;&lt;BR /&gt;&lt;BR /&gt;&amp;gt;&amp;gt;&amp;nbsp;&lt;SPAN&gt;We need pulse width measurement feature and PWM generation feature on same pin. Is FLEXIO or EMIOS which is best suit for this need?&lt;/SPAN&gt;&lt;BR /&gt;Please find example using EMIOS.&lt;BR /&gt;&lt;BR /&gt;&lt;A href="https://community.nxp.com/t5/S32K-Knowledge-Base/Example-IP-S32K312-EMIO-PWM-Generation-amp-Duty-capture-using/ta-p/2011634" target="_blank"&gt;https://community.nxp.com/t5/S32K-Knowledge-Base/Example-IP-S32K312-EMIO-PWM-Generation-amp-Duty-capture-using/ta-p/2011634&lt;/A&gt;&lt;BR /&gt;&lt;BR /&gt;&lt;A href="https://community.nxp.com/t5/S32K-Knowledge-Base/Example-IP-S32K312-EMIO-PWM-Generation-amp-Duty-capture-using/ta-p/2011642" target="_blank"&gt;https://community.nxp.com/t5/S32K-Knowledge-Base/Example-IP-S32K312-EMIO-PWM-Generation-amp-Duty-capture-using/ta-p/2011642&lt;/A&gt;&lt;BR /&gt;&lt;BR /&gt;&lt;A href="https://community.nxp.com/t5/S32K-Knowledge-Base/Example-IP-S32K312-PWM-ICU-using-EMIOS-DS3-5-RTD300/ta-p/2005954" target="_blank"&gt;https://community.nxp.com/t5/S32K-Knowledge-Base/Example-IP-S32K312-PWM-ICU-using-EMIOS-DS3-5-RTD300/ta-p/2005954&lt;/A&gt;&lt;BR /&gt;&lt;BR /&gt;For sent please create separate ticket so that we can assign it to right person.&lt;BR /&gt;&lt;BR /&gt;Regards,&lt;BR /&gt;Dinesh&lt;/P&gt;</description>
    <pubDate>Thu, 17 Apr 2025 04:42:05 GMT</pubDate>
    <dc:creator>Dinesh_Guleria</dc:creator>
    <dc:date>2025-04-17T04:42:05Z</dc:date>
    <item>
      <title>SENT TX emulation using FLEXIO or EMIOS</title>
      <link>https://community.nxp.com/t5/S32K/SENT-TX-emulation-using-FLEXIO-or-EMIOS/m-p/2000484#M43579</link>
      <description>&lt;P&gt;Hi,&lt;/P&gt;&lt;P&gt;We need pulse width measurement feature and PWM generation feature on same pin. Is FLEXIO or EMIOS which is best suit for this need?&lt;/P&gt;&lt;P&gt;Can we measure pulse width using FLEXIO input capture? We are planning to use FLEXIO module as a SPC SENT transmitter emulator. In SENT SPC after receiving trigger pulse we will start sent transmission, as per the requirement I need to measure the trigger pulse width.&lt;/P&gt;&lt;P&gt;Below is the trigger pulse sample. Can we measure below pulse width using FLEXIO input capture mode?&lt;/P&gt;&lt;P&gt;&lt;span class="lia-inline-image-display-wrapper lia-image-align-inline" image-alt="UmaMaheswaraReddy_0-1732349136947.png" style="width: 400px;"&gt;&lt;img src="https://community.nxp.com/t5/image/serverpage/image-id/312137i9F13F47386D88C32/image-size/medium?v=v2&amp;amp;px=400" role="button" title="UmaMaheswaraReddy_0-1732349136947.png" alt="UmaMaheswaraReddy_0-1732349136947.png" /&gt;&lt;span class="lia-inline-image-caption" onclick="event.preventDefault();"&gt;UmaMaheswaraReddy_0-1732349136947.png&lt;/span&gt;&lt;/span&gt;&lt;/P&gt;&lt;P&gt;Thanks,&lt;/P&gt;&lt;P&gt;Y Uma Maheswara Reddy.&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;</description>
      <pubDate>Sat, 23 Nov 2024 08:08:44 GMT</pubDate>
      <guid>https://community.nxp.com/t5/S32K/SENT-TX-emulation-using-FLEXIO-or-EMIOS/m-p/2000484#M43579</guid>
      <dc:creator>UmaMaheswaraReddy</dc:creator>
      <dc:date>2024-11-23T08:08:44Z</dc:date>
    </item>
    <item>
      <title>Re: SENT TX emulation using FLEXIO or EMIOS</title>
      <link>https://community.nxp.com/t5/S32K/SENT-TX-emulation-using-FLEXIO-or-EMIOS/m-p/2082199#M47863</link>
      <description>&lt;P&gt;Hi&amp;nbsp;&lt;a href="https://community.nxp.com/t5/user/viewprofilepage/user-id/213150"&gt;@UmaMaheswaraReddy&lt;/a&gt;&amp;nbsp;,&lt;BR /&gt;&lt;BR /&gt;&lt;BR /&gt;&amp;gt;&amp;gt;&amp;nbsp;&lt;SPAN&gt;We need pulse width measurement feature and PWM generation feature on same pin. Is FLEXIO or EMIOS which is best suit for this need?&lt;/SPAN&gt;&lt;BR /&gt;Please find example using EMIOS.&lt;BR /&gt;&lt;BR /&gt;&lt;A href="https://community.nxp.com/t5/S32K-Knowledge-Base/Example-IP-S32K312-EMIO-PWM-Generation-amp-Duty-capture-using/ta-p/2011634" target="_blank"&gt;https://community.nxp.com/t5/S32K-Knowledge-Base/Example-IP-S32K312-EMIO-PWM-Generation-amp-Duty-capture-using/ta-p/2011634&lt;/A&gt;&lt;BR /&gt;&lt;BR /&gt;&lt;A href="https://community.nxp.com/t5/S32K-Knowledge-Base/Example-IP-S32K312-EMIO-PWM-Generation-amp-Duty-capture-using/ta-p/2011642" target="_blank"&gt;https://community.nxp.com/t5/S32K-Knowledge-Base/Example-IP-S32K312-EMIO-PWM-Generation-amp-Duty-capture-using/ta-p/2011642&lt;/A&gt;&lt;BR /&gt;&lt;BR /&gt;&lt;A href="https://community.nxp.com/t5/S32K-Knowledge-Base/Example-IP-S32K312-PWM-ICU-using-EMIOS-DS3-5-RTD300/ta-p/2005954" target="_blank"&gt;https://community.nxp.com/t5/S32K-Knowledge-Base/Example-IP-S32K312-PWM-ICU-using-EMIOS-DS3-5-RTD300/ta-p/2005954&lt;/A&gt;&lt;BR /&gt;&lt;BR /&gt;For sent please create separate ticket so that we can assign it to right person.&lt;BR /&gt;&lt;BR /&gt;Regards,&lt;BR /&gt;Dinesh&lt;/P&gt;</description>
      <pubDate>Thu, 17 Apr 2025 04:42:05 GMT</pubDate>
      <guid>https://community.nxp.com/t5/S32K/SENT-TX-emulation-using-FLEXIO-or-EMIOS/m-p/2082199#M47863</guid>
      <dc:creator>Dinesh_Guleria</dc:creator>
      <dc:date>2025-04-17T04:42:05Z</dc:date>
    </item>
  </channel>
</rss>