<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>S32KのトピックRe: LPI2C Mode</title>
    <link>https://community.nxp.com/t5/S32K/LPI2C-Mode/m-p/647292#M478</link>
    <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hi,&lt;/P&gt;&lt;P&gt;You can use only PTA3 and PTB7 for LPI2C_SCL and none of them are high-drive. &amp;nbsp;I have just checked SDK I2C driver for S32K144 and the baud rate can be set only up to 400kbps. So as per all the information I have so far, the S32K144 doesn’t support 1000kbps baud rate.&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;Regards,&lt;/P&gt;&lt;P&gt;Daniel&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
    <pubDate>Tue, 09 May 2017 15:32:19 GMT</pubDate>
    <dc:creator>danielmartynek</dc:creator>
    <dc:date>2017-05-09T15:32:19Z</dc:date>
    <item>
      <title>LPI2C Mode</title>
      <link>https://community.nxp.com/t5/S32K/LPI2C-Mode/m-p/647287#M473</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hi,&lt;/P&gt;&lt;P&gt;the reference manual says on page 1383 that&amp;nbsp;baudrates above 400 kbit/s are not supported on the LPI2C device.&lt;/P&gt;&lt;P&gt;But on page 1384 it says in &lt;STRONG&gt;Features&lt;/STRONG&gt;: LPI2C supports&amp;nbsp;e.g.1Mbit/s (Fast Mode +)...&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Now what is right?&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Regards,&lt;/P&gt;&lt;P&gt;Adrian&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Thu, 27 Apr 2017 08:51:13 GMT</pubDate>
      <guid>https://community.nxp.com/t5/S32K/LPI2C-Mode/m-p/647287#M473</guid>
      <dc:creator>adrianwenger</dc:creator>
      <dc:date>2017-04-27T08:51:13Z</dc:date>
    </item>
    <item>
      <title>Re: LPI2C Mode</title>
      <link>https://community.nxp.com/t5/S32K/LPI2C-Mode/m-p/647288#M474</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hi,&lt;/P&gt;&lt;P&gt;As per Device feature summary (Table 2-1), only high-drive pins are able to support 1 Mbps.&lt;/P&gt;&lt;P&gt;PTA2 and PTA3 are not high-drive pins. See IO Signal Description Input Multiplexing sheet(s) attached&lt;/P&gt;&lt;P&gt;to the RM. &lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;Regards,&lt;/P&gt;&lt;P&gt;Daniel&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Thu, 27 Apr 2017 12:49:24 GMT</pubDate>
      <guid>https://community.nxp.com/t5/S32K/LPI2C-Mode/m-p/647288#M474</guid>
      <dc:creator>danielmartynek</dc:creator>
      <dc:date>2017-04-27T12:49:24Z</dc:date>
    </item>
    <item>
      <title>Re: LPI2C Mode</title>
      <link>https://community.nxp.com/t5/S32K/LPI2C-Mode/m-p/647289#M475</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hi Daniel,&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;thank you for your reply.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;After getting in touch with the IO Signal Description Input Multiplexing sheet i assume that,&lt;/P&gt;&lt;P&gt;if i use the PTB6 high-drive pin (LPI2C0_SDA)&amp;nbsp;and the PTA3&amp;nbsp;(LPI2C0_SCL)&amp;nbsp;i&amp;nbsp;will&amp;nbsp;be able to send with 1MBit/s to the i²C slave.&lt;/P&gt;&lt;P&gt;Is that correct?&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Regards,&lt;/P&gt;&lt;P&gt;Adrian&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Wed, 03 May 2017 08:39:23 GMT</pubDate>
      <guid>https://community.nxp.com/t5/S32K/LPI2C-Mode/m-p/647289#M475</guid>
      <dc:creator>adrianwenger</dc:creator>
      <dc:date>2017-05-03T08:39:23Z</dc:date>
    </item>
    <item>
      <title>Re: LPI2C Mode</title>
      <link>https://community.nxp.com/t5/S32K/LPI2C-Mode/m-p/647290#M476</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hi Adrian,&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;The functionality at that rate is guaranteed (even with bus capacitance of 400pF) only using high-drive pins for both SDA, SCL. &amp;nbsp;If you use pins without high-drive capability, it might work in case the bus capacitance is not too high, but is not guaranteed.&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;Regards,&lt;/P&gt;&lt;P&gt;Daniel&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Fri, 05 May 2017 08:12:26 GMT</pubDate>
      <guid>https://community.nxp.com/t5/S32K/LPI2C-Mode/m-p/647290#M476</guid>
      <dc:creator>danielmartynek</dc:creator>
      <dc:date>2017-05-05T08:12:26Z</dc:date>
    </item>
    <item>
      <title>Re: LPI2C Mode</title>
      <link>https://community.nxp.com/t5/S32K/LPI2C-Mode/m-p/647291#M477</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hi Martin,&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;can i use any of the high-drive Pins for the LPI2C0_SCL to get the 1MBit/s garanteed?&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;&lt;span class="lia-inline-image-display-wrapper"&gt;&lt;img src="https://community.nxp.com/t5/image/serverpage/image-id/20333i533252B5444E9173/image-size/large?v=v2&amp;amp;px=999" title="Unbenannt.PNG" alt="Unbenannt.PNG" /&gt;&lt;/span&gt;&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Regards,&lt;/P&gt;&lt;P&gt;Adrian&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Mon, 08 May 2017 08:03:02 GMT</pubDate>
      <guid>https://community.nxp.com/t5/S32K/LPI2C-Mode/m-p/647291#M477</guid>
      <dc:creator>adrianwenger</dc:creator>
      <dc:date>2017-05-08T08:03:02Z</dc:date>
    </item>
    <item>
      <title>Re: LPI2C Mode</title>
      <link>https://community.nxp.com/t5/S32K/LPI2C-Mode/m-p/647292#M478</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hi,&lt;/P&gt;&lt;P&gt;You can use only PTA3 and PTB7 for LPI2C_SCL and none of them are high-drive. &amp;nbsp;I have just checked SDK I2C driver for S32K144 and the baud rate can be set only up to 400kbps. So as per all the information I have so far, the S32K144 doesn’t support 1000kbps baud rate.&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;Regards,&lt;/P&gt;&lt;P&gt;Daniel&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Tue, 09 May 2017 15:32:19 GMT</pubDate>
      <guid>https://community.nxp.com/t5/S32K/LPI2C-Mode/m-p/647292#M478</guid>
      <dc:creator>danielmartynek</dc:creator>
      <dc:date>2017-05-09T15:32:19Z</dc:date>
    </item>
    <item>
      <title>Re: LPI2C Mode</title>
      <link>https://community.nxp.com/t5/S32K/LPI2C-Mode/m-p/647293#M479</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hi Daniel,&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;thanks for clarification.&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Thu, 11 May 2017 06:36:18 GMT</pubDate>
      <guid>https://community.nxp.com/t5/S32K/LPI2C-Mode/m-p/647293#M479</guid>
      <dc:creator>adrianwenger</dc:creator>
      <dc:date>2017-05-11T06:36:18Z</dc:date>
    </item>
  </channel>
</rss>