<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>topic Re: S32k314 STM Clock question in S32K</title>
    <link>https://community.nxp.com/t5/S32K/S32k314-STM-Clock-question/m-p/2078775#M47675</link>
    <description>&lt;P&gt;Hi&lt;/P&gt;
&lt;P&gt;If it is a new project, it is recommended to use the latest S32K3 RTD, because many bugs are fixed.&lt;/P&gt;
&lt;P&gt;Have you tested the latest &lt;STRONG&gt;S32K3_S32M27x Real-Time Drivers ASR R21-11 Version 5.0.0&lt;/STRONG&gt;?&lt;/P&gt;
&lt;P&gt;Best Regards,&lt;BR /&gt;Robin&lt;/P&gt;</description>
    <pubDate>Fri, 11 Apr 2025 04:31:22 GMT</pubDate>
    <dc:creator>Robin_Shen</dc:creator>
    <dc:date>2025-04-11T04:31:22Z</dc:date>
    <item>
      <title>S32k314 STM Clock question</title>
      <link>https://community.nxp.com/t5/S32K/S32k314-STM-Clock-question/m-p/2077028#M47604</link>
      <description>&lt;P class=""&gt;We are currently migrating from the S32K344 environment to the S32K314.&lt;/P&gt;&lt;P class=""&gt;During the GPT initialization process, a core power-down occurs.&lt;/P&gt;&lt;P class=""&gt;One of the key differences we've identified between the S32K344 and the S32K314 is the generation of the STM1_CLK (STMB_CLK).&lt;BR /&gt;In the case of the S32K344, STMB_CLK is properly generated.&lt;/P&gt;&lt;P class=""&gt;In the S32K314 environment, we forcibly added the STMB_CLK configuration to the generated Clock_Ip_PBcfg.c file.&lt;BR /&gt;After doing so, the GPT initialization worked correctly and the system booted without any issues.&lt;/P&gt;&lt;P class=""&gt;However, we don’t understand why simply adding this configuration would cause the GPT init to work as expected.&lt;BR /&gt;We are trying to understand how this change alone resolves the issue.&lt;/P&gt;</description>
      <pubDate>Wed, 09 Apr 2025 10:05:54 GMT</pubDate>
      <guid>https://community.nxp.com/t5/S32K/S32k314-STM-Clock-question/m-p/2077028#M47604</guid>
      <dc:creator>dpsdprtmvl</dc:creator>
      <dc:date>2025-04-09T10:05:54Z</dc:date>
    </item>
    <item>
      <title>Re: S32k314 STM Clock question</title>
      <link>https://community.nxp.com/t5/S32K/S32k314-STM-Clock-question/m-p/2078775#M47675</link>
      <description>&lt;P&gt;Hi&lt;/P&gt;
&lt;P&gt;If it is a new project, it is recommended to use the latest S32K3 RTD, because many bugs are fixed.&lt;/P&gt;
&lt;P&gt;Have you tested the latest &lt;STRONG&gt;S32K3_S32M27x Real-Time Drivers ASR R21-11 Version 5.0.0&lt;/STRONG&gt;?&lt;/P&gt;
&lt;P&gt;Best Regards,&lt;BR /&gt;Robin&lt;/P&gt;</description>
      <pubDate>Fri, 11 Apr 2025 04:31:22 GMT</pubDate>
      <guid>https://community.nxp.com/t5/S32K/S32k314-STM-Clock-question/m-p/2078775#M47675</guid>
      <dc:creator>Robin_Shen</dc:creator>
      <dc:date>2025-04-11T04:31:22Z</dc:date>
    </item>
  </channel>
</rss>