<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>S32KのトピックResetting S32k344 through a function call/outside input</title>
    <link>https://community.nxp.com/t5/S32K/Resetting-S32k344-through-a-function-call-outside-input/m-p/2078704#M47668</link>
    <description>&lt;P&gt;I am currently using&amp;nbsp;&lt;SPAN&gt;Power_Ip_PerformReset(&amp;amp;Power_Ip_HwIPsConfigPB_BOARD_InitPeripherals); to reset my board when I call it through outside input, however this is appearing to cause some strange issues with my i2c where some values are getting messed up, I have a data request that should only return values in the 8th and 1st bit, but I am getting a 1 in the 3rd bit which should be impossible with the register I am reading from. When I cycle the power the issue goes away until I call the reboot again at which point I need to cycle power again.&lt;/SPAN&gt;&lt;/P&gt;&lt;P&gt;What other options do I have to reset the program to the start from a function call?&lt;/P&gt;</description>
    <pubDate>Fri, 11 Apr 2025 01:44:51 GMT</pubDate>
    <dc:creator>pb632146</dc:creator>
    <dc:date>2025-04-11T01:44:51Z</dc:date>
    <item>
      <title>Resetting S32k344 through a function call/outside input</title>
      <link>https://community.nxp.com/t5/S32K/Resetting-S32k344-through-a-function-call-outside-input/m-p/2078704#M47668</link>
      <description>&lt;P&gt;I am currently using&amp;nbsp;&lt;SPAN&gt;Power_Ip_PerformReset(&amp;amp;Power_Ip_HwIPsConfigPB_BOARD_InitPeripherals); to reset my board when I call it through outside input, however this is appearing to cause some strange issues with my i2c where some values are getting messed up, I have a data request that should only return values in the 8th and 1st bit, but I am getting a 1 in the 3rd bit which should be impossible with the register I am reading from. When I cycle the power the issue goes away until I call the reboot again at which point I need to cycle power again.&lt;/SPAN&gt;&lt;/P&gt;&lt;P&gt;What other options do I have to reset the program to the start from a function call?&lt;/P&gt;</description>
      <pubDate>Fri, 11 Apr 2025 01:44:51 GMT</pubDate>
      <guid>https://community.nxp.com/t5/S32K/Resetting-S32k344-through-a-function-call-outside-input/m-p/2078704#M47668</guid>
      <dc:creator>pb632146</dc:creator>
      <dc:date>2025-04-11T01:44:51Z</dc:date>
    </item>
    <item>
      <title>Re: Resetting S32k344 through a function call/outside input</title>
      <link>https://community.nxp.com/t5/S32K/Resetting-S32k344-through-a-function-call-outside-input/m-p/2079256#M47699</link>
      <description>&lt;P&gt;Hi&amp;nbsp;&lt;a href="https://community.nxp.com/t5/user/viewprofilepage/user-id/230291"&gt;@pb632146&lt;/a&gt;,&lt;/P&gt;
&lt;P&gt;Do you have available a project to share so I can replicate this issue in our boards? Also, could you try to read the reset reason just to confirm if a SW reset is being correctly performed?&amp;nbsp;&lt;/P&gt;
&lt;P&gt;Best regards,&lt;BR /&gt;Julián&lt;/P&gt;</description>
      <pubDate>Fri, 11 Apr 2025 18:05:58 GMT</pubDate>
      <guid>https://community.nxp.com/t5/S32K/Resetting-S32k344-through-a-function-call-outside-input/m-p/2079256#M47699</guid>
      <dc:creator>Julián_AragónM</dc:creator>
      <dc:date>2025-04-11T18:05:58Z</dc:date>
    </item>
  </channel>
</rss>