<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>S32KのトピックChange HSE Lifecycle</title>
    <link>https://community.nxp.com/t5/S32K/Change-HSE-Lifecycle/m-p/2078241#M47639</link>
    <description>&lt;P&gt;Hi,&lt;/P&gt;&lt;P&gt;I'm developing software based on S32K3xx Demo app.&lt;/P&gt;&lt;P&gt;In order to Update Secure Life Cycle, ADKP need to be is programmed.&lt;/P&gt;&lt;P&gt;After ADKP is programmed, the secure debug feature is enabled.&lt;/P&gt;&lt;P&gt;I got 2 questions:&lt;/P&gt;&lt;OL&gt;&lt;LI&gt;Does the secure debug feature always enabled when HSE Life cycle is&amp;nbsp;OEM_PROD/IN_FIELD?&lt;/LI&gt;&lt;LI&gt;Can secure debug feature be disabled when HSE Life cycle is&amp;nbsp;OEM_PROD/IN_FIELD? (No debug authorization script needed)&lt;/LI&gt;&lt;/OL&gt;&lt;P&gt;Thanks a lot.&lt;/P&gt;</description>
    <pubDate>Thu, 10 Apr 2025 10:23:09 GMT</pubDate>
    <dc:creator>HaiHoangSoftware</dc:creator>
    <dc:date>2025-04-10T10:23:09Z</dc:date>
    <item>
      <title>Change HSE Lifecycle</title>
      <link>https://community.nxp.com/t5/S32K/Change-HSE-Lifecycle/m-p/2078241#M47639</link>
      <description>&lt;P&gt;Hi,&lt;/P&gt;&lt;P&gt;I'm developing software based on S32K3xx Demo app.&lt;/P&gt;&lt;P&gt;In order to Update Secure Life Cycle, ADKP need to be is programmed.&lt;/P&gt;&lt;P&gt;After ADKP is programmed, the secure debug feature is enabled.&lt;/P&gt;&lt;P&gt;I got 2 questions:&lt;/P&gt;&lt;OL&gt;&lt;LI&gt;Does the secure debug feature always enabled when HSE Life cycle is&amp;nbsp;OEM_PROD/IN_FIELD?&lt;/LI&gt;&lt;LI&gt;Can secure debug feature be disabled when HSE Life cycle is&amp;nbsp;OEM_PROD/IN_FIELD? (No debug authorization script needed)&lt;/LI&gt;&lt;/OL&gt;&lt;P&gt;Thanks a lot.&lt;/P&gt;</description>
      <pubDate>Thu, 10 Apr 2025 10:23:09 GMT</pubDate>
      <guid>https://community.nxp.com/t5/S32K/Change-HSE-Lifecycle/m-p/2078241#M47639</guid>
      <dc:creator>HaiHoangSoftware</dc:creator>
      <dc:date>2025-04-10T10:23:09Z</dc:date>
    </item>
    <item>
      <title>Re: Change HSE Lifecycle</title>
      <link>https://community.nxp.com/t5/S32K/Change-HSE-Lifecycle/m-p/2078313#M47647</link>
      <description>&lt;P&gt;Hi &lt;a href="https://community.nxp.com/t5/user/viewprofilepage/user-id/247218"&gt;@HaiHoangSoftware&lt;/a&gt;&amp;nbsp;&lt;/P&gt;
&lt;P&gt;Here are two screenshots from the manual:&lt;/P&gt;
&lt;P&gt;&lt;span class="lia-inline-image-display-wrapper lia-image-align-inline" image-alt="image.png" style="width: 981px;"&gt;&lt;img src="https://community.nxp.com/t5/image/serverpage/image-id/332515i81C21809C5B3C2E2/image-size/large?v=v2&amp;amp;px=999" role="button" title="image.png" alt="image.png" /&gt;&lt;span class="lia-inline-image-caption" onclick="event.preventDefault();"&gt;image.png&lt;/span&gt;&lt;/span&gt;&lt;/P&gt;
&lt;P&gt;&lt;span class="lia-inline-image-display-wrapper lia-image-align-inline" image-alt="image.png" style="width: 999px;"&gt;&lt;img src="https://community.nxp.com/t5/image/serverpage/image-id/332516i04CB108B3190D574/image-size/large?v=v2&amp;amp;px=999" role="button" title="image.png" alt="image.png" /&gt;&lt;span class="lia-inline-image-caption" onclick="event.preventDefault();"&gt;image.png&lt;/span&gt;&lt;/span&gt;&amp;nbsp;&lt;/P&gt;
&lt;P&gt;So, it is mandatory to configure ADKP when advancing the life cycle and it's not possible to disable secure debug because it's programmed to OTP. &lt;/P&gt;
&lt;P&gt;Regards,&lt;/P&gt;
&lt;P&gt;Lukas&lt;/P&gt;</description>
      <pubDate>Thu, 10 Apr 2025 11:40:55 GMT</pubDate>
      <guid>https://community.nxp.com/t5/S32K/Change-HSE-Lifecycle/m-p/2078313#M47647</guid>
      <dc:creator>lukaszadrapa</dc:creator>
      <dc:date>2025-04-10T11:40:55Z</dc:date>
    </item>
  </channel>
</rss>