<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>topic Re: S32K144EVB: Dual Power Configuration for CAN and USB Debugging with FreeMASTER in S32K</title>
    <link>https://community.nxp.com/t5/S32K/S32K144EVB-Dual-Power-Configuration-for-CAN-and-USB-Debugging/m-p/2077203#M47608</link>
    <description>&lt;P&gt;Hi&amp;nbsp;&lt;a href="https://community.nxp.com/t5/user/viewprofilepage/user-id/199320"&gt;@_Leo_&lt;/a&gt;, thanks a lot!!&lt;/P&gt;&lt;P&gt;Can you confirm if it’s safe to supply pin 2 (P5V0) directly with an external 5V source, bypassing pins 1 and 3 (P5V_SBC&amp;nbsp;and P5V_SDA_PSW), and at the same time use 12V to supply CAN physical layer and debug using FreeMASTER via USB?&lt;/P&gt;</description>
    <pubDate>Wed, 09 Apr 2025 15:12:19 GMT</pubDate>
    <dc:creator>Matheus_Siqueira</dc:creator>
    <dc:date>2025-04-09T15:12:19Z</dc:date>
    <item>
      <title>S32K144EVB: Dual Power Configuration for CAN and USB Debugging with FreeMASTER</title>
      <link>https://community.nxp.com/t5/S32K/S32K144EVB-Dual-Power-Configuration-for-CAN-and-USB-Debugging/m-p/2076296#M47580</link>
      <description>&lt;P&gt;&lt;SPAN&gt;Hello everyone,&lt;/SPAN&gt;&lt;/P&gt;&lt;P&gt;&lt;SPAN&gt;I’m currently working with the&amp;nbsp;&lt;STRONG&gt;S32K144EVB&lt;/STRONG&gt;&amp;nbsp;and have been reviewing the power supply section of the datasheet. However, I’m a bit confused about the&amp;nbsp;&lt;STRONG&gt;power supply system&lt;/STRONG&gt;&amp;nbsp;and how to properly configure it. Could someone tell if it is possible to use two different power sources to enable CAN communication&amp;nbsp;&lt;/SPAN&gt;&lt;STRONG&gt;and&lt;/STRONG&gt;&lt;SPAN&gt;&amp;nbsp;USB (connected to a PC for FreeMASTER debugging)&amp;nbsp;&lt;/SPAN&gt;&lt;STRONG&gt;at the same time&lt;/STRONG&gt;&lt;SPAN&gt;? If so, specifically:&lt;/SPAN&gt;&lt;/P&gt;&lt;P&gt;&lt;SPAN&gt;1. If I keep J107 in the&amp;nbsp;&lt;/SPAN&gt;&lt;STRONG&gt;1-2 position&lt;/STRONG&gt;&lt;SPAN&gt;&amp;nbsp;(P5V_SBC = P5V0), can I independently connect USB for FreeMASTER debugging without any power conflicts?&lt;/SPAN&gt;&lt;/P&gt;&lt;P&gt;&lt;SPAN&gt;2. Alternatively, can I set J107 to&amp;nbsp;&lt;/SPAN&gt;&lt;STRONG&gt;2-3&lt;/STRONG&gt;&lt;SPAN&gt;&amp;nbsp;(P5V_SDA_PSW = P5V0) and use the external power source of 12V to supply only the UJA1169, while the rest of the system is supplied through P5V_SDA_PSW = P5V0&amp;nbsp;to enable USB debugging using FreeMASTER?&lt;/SPAN&gt;&lt;/P&gt;</description>
      <pubDate>Tue, 08 Apr 2025 15:20:23 GMT</pubDate>
      <guid>https://community.nxp.com/t5/S32K/S32K144EVB-Dual-Power-Configuration-for-CAN-and-USB-Debugging/m-p/2076296#M47580</guid>
      <dc:creator>Matheus_Siqueira</dc:creator>
      <dc:date>2025-04-08T15:20:23Z</dc:date>
    </item>
    <item>
      <title>Re: S32K144EVB: Dual Power Configuration for CAN and USB Debugging with FreeMASTER</title>
      <link>https://community.nxp.com/t5/S32K/S32K144EVB-Dual-Power-Configuration-for-CAN-and-USB-Debugging/m-p/2076416#M47583</link>
      <description>&lt;P&gt;Hi,&lt;/P&gt;
&lt;P&gt;Thank you so much for your interest in our products and for using our community.&lt;/P&gt;
&lt;P&gt;To power the SBC, connect an external 12V supply to the EVB and connect pins 1-2 on jumper J107. At the same time, a USB cable can still be connected to the EVB to allow debugging using FreeMASTER.&lt;/P&gt;
&lt;P&gt;Hope it helps you.&lt;/P&gt;
&lt;P&gt;Have a nice day!&lt;/P&gt;</description>
      <pubDate>Tue, 08 Apr 2025 18:19:25 GMT</pubDate>
      <guid>https://community.nxp.com/t5/S32K/S32K144EVB-Dual-Power-Configuration-for-CAN-and-USB-Debugging/m-p/2076416#M47583</guid>
      <dc:creator>_Leo_</dc:creator>
      <dc:date>2025-04-08T18:19:25Z</dc:date>
    </item>
    <item>
      <title>Re: S32K144EVB: Dual Power Configuration for CAN and USB Debugging with FreeMASTER</title>
      <link>https://community.nxp.com/t5/S32K/S32K144EVB-Dual-Power-Configuration-for-CAN-and-USB-Debugging/m-p/2077203#M47608</link>
      <description>&lt;P&gt;Hi&amp;nbsp;&lt;a href="https://community.nxp.com/t5/user/viewprofilepage/user-id/199320"&gt;@_Leo_&lt;/a&gt;, thanks a lot!!&lt;/P&gt;&lt;P&gt;Can you confirm if it’s safe to supply pin 2 (P5V0) directly with an external 5V source, bypassing pins 1 and 3 (P5V_SBC&amp;nbsp;and P5V_SDA_PSW), and at the same time use 12V to supply CAN physical layer and debug using FreeMASTER via USB?&lt;/P&gt;</description>
      <pubDate>Wed, 09 Apr 2025 15:12:19 GMT</pubDate>
      <guid>https://community.nxp.com/t5/S32K/S32K144EVB-Dual-Power-Configuration-for-CAN-and-USB-Debugging/m-p/2077203#M47608</guid>
      <dc:creator>Matheus_Siqueira</dc:creator>
      <dc:date>2025-04-09T15:12:19Z</dc:date>
    </item>
  </channel>
</rss>