<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>S32KのトピックS32K314 GPT Clock Issue</title>
    <link>https://community.nxp.com/t5/S32K/S32K314-GPT-Clock-Issue/m-p/2076864#M47599</link>
    <description>&lt;P class=""&gt;We are in the process of migrating from the S32K344 environment to the S32K314.&lt;/P&gt;&lt;P class=""&gt;(Using&amp;nbsp;SW32K3_RTD_R21-11_3.0.0_P07)&lt;/P&gt;&lt;P class=""&gt;During GPT initialization, a core power-down occurs.&lt;/P&gt;&lt;P class=""&gt;We identified that one of the differences between the S32K344 and the S32K314 is the generation of STM1_CLK (STMB_CLK).&lt;BR /&gt;(S32K344 successfully generates STMB_CLK.)&lt;/P&gt;&lt;P class=""&gt;In the generated file Clock_Ip_PBcfg.c from the S32K314 environment, we modified the configuration to forcibly change the STMA_CLK to STMB_CLK and recompiled.&lt;BR /&gt;After this change, the GPT initialization proceeds normally, and the system boots up without any issues.&lt;/P&gt;&lt;P class=""&gt;However, according to the RM.pdf, STM1_CLK (STMB_CLK) does not seem to exist in the S32K314.&lt;/P&gt;&lt;P class=""&gt;&amp;nbsp;&lt;/P&gt;&lt;UL&gt;&lt;LI&gt;&lt;P class=""&gt;How is it possible that the S32K314 operates with STM1_CLK (STMB_CLK), even though this clock is not documented as existing in the S32K314?&lt;/P&gt;&lt;/LI&gt;&lt;LI&gt;&lt;P class=""&gt;What is the correct way to configure the GPT module to use STM0_CLK instead of STM1_CLK as its clock source?&lt;/P&gt;&lt;/LI&gt;&lt;/UL&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;</description>
    <pubDate>Wed, 09 Apr 2025 08:22:29 GMT</pubDate>
    <dc:creator>dpsdprtmvl</dc:creator>
    <dc:date>2025-04-09T08:22:29Z</dc:date>
    <item>
      <title>S32K314 GPT Clock Issue</title>
      <link>https://community.nxp.com/t5/S32K/S32K314-GPT-Clock-Issue/m-p/2076864#M47599</link>
      <description>&lt;P class=""&gt;We are in the process of migrating from the S32K344 environment to the S32K314.&lt;/P&gt;&lt;P class=""&gt;(Using&amp;nbsp;SW32K3_RTD_R21-11_3.0.0_P07)&lt;/P&gt;&lt;P class=""&gt;During GPT initialization, a core power-down occurs.&lt;/P&gt;&lt;P class=""&gt;We identified that one of the differences between the S32K344 and the S32K314 is the generation of STM1_CLK (STMB_CLK).&lt;BR /&gt;(S32K344 successfully generates STMB_CLK.)&lt;/P&gt;&lt;P class=""&gt;In the generated file Clock_Ip_PBcfg.c from the S32K314 environment, we modified the configuration to forcibly change the STMA_CLK to STMB_CLK and recompiled.&lt;BR /&gt;After this change, the GPT initialization proceeds normally, and the system boots up without any issues.&lt;/P&gt;&lt;P class=""&gt;However, according to the RM.pdf, STM1_CLK (STMB_CLK) does not seem to exist in the S32K314.&lt;/P&gt;&lt;P class=""&gt;&amp;nbsp;&lt;/P&gt;&lt;UL&gt;&lt;LI&gt;&lt;P class=""&gt;How is it possible that the S32K314 operates with STM1_CLK (STMB_CLK), even though this clock is not documented as existing in the S32K314?&lt;/P&gt;&lt;/LI&gt;&lt;LI&gt;&lt;P class=""&gt;What is the correct way to configure the GPT module to use STM0_CLK instead of STM1_CLK as its clock source?&lt;/P&gt;&lt;/LI&gt;&lt;/UL&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;</description>
      <pubDate>Wed, 09 Apr 2025 08:22:29 GMT</pubDate>
      <guid>https://community.nxp.com/t5/S32K/S32K314-GPT-Clock-Issue/m-p/2076864#M47599</guid>
      <dc:creator>dpsdprtmvl</dc:creator>
      <dc:date>2025-04-09T08:22:29Z</dc:date>
    </item>
    <item>
      <title>Re: S32K314 GPT Clock Issue</title>
      <link>https://community.nxp.com/t5/S32K/S32K314-GPT-Clock-Issue/m-p/2078776#M47676</link>
      <description>&lt;P&gt;It looks like this question is a duplicate of &lt;A href="https://community.nxp.com/t5/S32K/S32k314-STM-Clock-question/m-p/2077028#M47604" target="_self"&gt;S32k314 STM Clock question&lt;/A&gt;. Let's discuss there.&lt;/P&gt;</description>
      <pubDate>Fri, 11 Apr 2025 04:32:37 GMT</pubDate>
      <guid>https://community.nxp.com/t5/S32K/S32K314-GPT-Clock-Issue/m-p/2078776#M47676</guid>
      <dc:creator>Robin_Shen</dc:creator>
      <dc:date>2025-04-11T04:32:37Z</dc:date>
    </item>
  </channel>
</rss>