<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>topic Re: S32K3 GPIO HIGH-Z in S32K</title>
    <link>https://community.nxp.com/t5/S32K/S32K3-GPIO-HIGH-Z/m-p/2075153#M47535</link>
    <description>&lt;P&gt;For anyone looking on using&amp;nbsp;&lt;SPAN&gt;Siul2_Port_Ip_SetPinDirection to set to Hi-Z, here is how to call the function:&lt;/SPAN&gt;&lt;BR /&gt;&lt;BR /&gt;&lt;SPAN&gt;Siul2_Port_Ip_SetPinDirection(PORT, PIN, SIUL2_PORT_HI_Z);&lt;BR /&gt;&lt;BR /&gt;&lt;BR /&gt;&lt;/SPAN&gt;For input variable 1 of the function, which is `Siul2_Port_Ip_PortType * const base`, you need to use the defines mentioned in `Siul2_Port_Ip_Defines.h` and not the ones `Siul2_Port_Ip_Cfg.h`. You can find out what define the Pin you are using belongs to by checking in&amp;nbsp;&amp;nbsp;`Siul2_Port_Ip_Cfg.h` as shown below:&lt;BR /&gt;&lt;BR /&gt;&lt;/P&gt;&lt;P&gt;&lt;span class="lia-inline-image-display-wrapper lia-image-align-inline" image-alt="ASN71_0-1744013239920.png" style="width: 400px;"&gt;&lt;img src="https://community.nxp.com/t5/image/serverpage/image-id/331578iFABC73EC70034F83/image-size/medium?v=v2&amp;amp;px=400" role="button" title="ASN71_0-1744013239920.png" alt="ASN71_0-1744013239920.png" /&gt;&lt;span class="lia-inline-image-caption" onclick="event.preventDefault();"&gt;ASN71_0-1744013239920.png&lt;/span&gt;&lt;/span&gt;&lt;/P&gt;&lt;P&gt;Now that PTD_H_HALF is known, which is Port D High Half Base, find it in `Siul2_Port_Ip_Defines.h` and use it as the first input argument.&amp;nbsp;&lt;/P&gt;&lt;P&gt;&lt;BR /&gt;&lt;BR /&gt;For input variable 2, you can use the defines mentioned in&amp;nbsp; `Siul2_Port_Ip_Cfg.h` which is nothing but the Pin Number.&amp;nbsp;&lt;BR /&gt;&lt;BR /&gt;Once the pin is set to &lt;SPAN&gt;SIUL2_PORT_HI_Z, you do not have to use&amp;nbsp;Siul2_Dio_Ip_WritePin function as it is only used to set the Pin to High or Low and not for SIUL2_PORT_HI_Z.&amp;nbsp;&amp;nbsp;&lt;BR /&gt;&lt;BR /&gt;&amp;nbsp;I hope this gives a bit more clarity.&amp;nbsp;&lt;/SPAN&gt;&lt;/P&gt;</description>
    <pubDate>Mon, 07 Apr 2025 12:09:56 GMT</pubDate>
    <dc:creator>ASN7</dc:creator>
    <dc:date>2025-04-07T12:09:56Z</dc:date>
    <item>
      <title>S32K3 GPIO HIGH-Z</title>
      <link>https://community.nxp.com/t5/S32K/S32K3-GPIO-HIGH-Z/m-p/2008049#M43919</link>
      <description>&lt;P&gt;Hi，NXP experts&lt;BR /&gt;In S32DS3.5, how do I configure pin to state HIGH-Z?&amp;nbsp; &amp;nbsp;S32K312+RTD4.0.0&lt;BR /&gt;In picture 1 it says can be configured as HIGH-Z，but&amp;nbsp;I can't find the configuration item.&lt;/P&gt;&lt;P&gt;&lt;span class="lia-inline-image-display-wrapper lia-image-align-inline" image-alt="Chenxu1_0-1733391241328.png" style="width: 400px;"&gt;&lt;img src="https://community.nxp.com/t5/image/serverpage/image-id/314295i414357A6A1C4507A/image-size/medium?v=v2&amp;amp;px=400" role="button" title="Chenxu1_0-1733391241328.png" alt="Chenxu1_0-1733391241328.png" /&gt;&lt;span class="lia-inline-image-caption" onclick="event.preventDefault();"&gt;Chenxu1_0-1733391241328.png&lt;/span&gt;&lt;/span&gt;&lt;/P&gt;&lt;P&gt;&lt;span class="lia-inline-image-display-wrapper lia-image-align-inline" image-alt="Chenxu1_1-1733391247913.png" style="width: 400px;"&gt;&lt;img src="https://community.nxp.com/t5/image/serverpage/image-id/314296iB718F0C4F2BF23F4/image-size/medium?v=v2&amp;amp;px=400" role="button" title="Chenxu1_1-1733391247913.png" alt="Chenxu1_1-1733391247913.png" /&gt;&lt;span class="lia-inline-image-caption" onclick="event.preventDefault();"&gt;Chenxu1_1-1733391247913.png&lt;/span&gt;&lt;/span&gt;&lt;/P&gt;&lt;P&gt;&lt;SPAN&gt;It is configurable in EB（picture 3）.&lt;BR /&gt;&lt;/SPAN&gt;&lt;/P&gt;&lt;P&gt;&lt;span class="lia-inline-image-display-wrapper lia-image-align-inline" image-alt="Chenxu1_2-1733391410995.png" style="width: 400px;"&gt;&lt;img src="https://community.nxp.com/t5/image/serverpage/image-id/314299iC4C8F7988CCE2040/image-size/medium?v=v2&amp;amp;px=400" role="button" title="Chenxu1_2-1733391410995.png" alt="Chenxu1_2-1733391410995.png" /&gt;&lt;span class="lia-inline-image-caption" onclick="event.preventDefault();"&gt;Chenxu1_2-1733391410995.png&lt;/span&gt;&lt;/span&gt;&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;&lt;SPAN&gt;&lt;BR /&gt;&lt;BR /&gt;&lt;/SPAN&gt;&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;</description>
      <pubDate>Thu, 05 Dec 2024 09:37:03 GMT</pubDate>
      <guid>https://community.nxp.com/t5/S32K/S32K3-GPIO-HIGH-Z/m-p/2008049#M43919</guid>
      <dc:creator>Chenxu1</dc:creator>
      <dc:date>2024-12-05T09:37:03Z</dc:date>
    </item>
    <item>
      <title>Re: S32K3 GPIO HIGH-Z</title>
      <link>https://community.nxp.com/t5/S32K/S32K3-GPIO-HIGH-Z/m-p/2008564#M43951</link>
      <description>&lt;P&gt;Hi&amp;nbsp;&lt;a href="https://community.nxp.com/t5/user/viewprofilepage/user-id/230296"&gt;@Chenxu1&lt;/a&gt;&amp;nbsp;&lt;/P&gt;
&lt;P&gt;Unlike EB Tresos, S32 ConfigTools does not have the option to set the PortPin Direction to PORT_PIN_HIGH_Z, as this is the default value. If you want to change it, you can use the functions Siul2_Port_Ip_SetPinDirection() or Port_SetPinDirection().&lt;/P&gt;
&lt;P&gt;&amp;nbsp;&lt;/P&gt;
&lt;P&gt;BR, VaneB&lt;/P&gt;</description>
      <pubDate>Thu, 05 Dec 2024 21:49:53 GMT</pubDate>
      <guid>https://community.nxp.com/t5/S32K/S32K3-GPIO-HIGH-Z/m-p/2008564#M43951</guid>
      <dc:creator>VaneB</dc:creator>
      <dc:date>2024-12-05T21:49:53Z</dc:date>
    </item>
    <item>
      <title>Re: S32K3 GPIO HIGH-Z</title>
      <link>https://community.nxp.com/t5/S32K/S32K3-GPIO-HIGH-Z/m-p/2075153#M47535</link>
      <description>&lt;P&gt;For anyone looking on using&amp;nbsp;&lt;SPAN&gt;Siul2_Port_Ip_SetPinDirection to set to Hi-Z, here is how to call the function:&lt;/SPAN&gt;&lt;BR /&gt;&lt;BR /&gt;&lt;SPAN&gt;Siul2_Port_Ip_SetPinDirection(PORT, PIN, SIUL2_PORT_HI_Z);&lt;BR /&gt;&lt;BR /&gt;&lt;BR /&gt;&lt;/SPAN&gt;For input variable 1 of the function, which is `Siul2_Port_Ip_PortType * const base`, you need to use the defines mentioned in `Siul2_Port_Ip_Defines.h` and not the ones `Siul2_Port_Ip_Cfg.h`. You can find out what define the Pin you are using belongs to by checking in&amp;nbsp;&amp;nbsp;`Siul2_Port_Ip_Cfg.h` as shown below:&lt;BR /&gt;&lt;BR /&gt;&lt;/P&gt;&lt;P&gt;&lt;span class="lia-inline-image-display-wrapper lia-image-align-inline" image-alt="ASN71_0-1744013239920.png" style="width: 400px;"&gt;&lt;img src="https://community.nxp.com/t5/image/serverpage/image-id/331578iFABC73EC70034F83/image-size/medium?v=v2&amp;amp;px=400" role="button" title="ASN71_0-1744013239920.png" alt="ASN71_0-1744013239920.png" /&gt;&lt;span class="lia-inline-image-caption" onclick="event.preventDefault();"&gt;ASN71_0-1744013239920.png&lt;/span&gt;&lt;/span&gt;&lt;/P&gt;&lt;P&gt;Now that PTD_H_HALF is known, which is Port D High Half Base, find it in `Siul2_Port_Ip_Defines.h` and use it as the first input argument.&amp;nbsp;&lt;/P&gt;&lt;P&gt;&lt;BR /&gt;&lt;BR /&gt;For input variable 2, you can use the defines mentioned in&amp;nbsp; `Siul2_Port_Ip_Cfg.h` which is nothing but the Pin Number.&amp;nbsp;&lt;BR /&gt;&lt;BR /&gt;Once the pin is set to &lt;SPAN&gt;SIUL2_PORT_HI_Z, you do not have to use&amp;nbsp;Siul2_Dio_Ip_WritePin function as it is only used to set the Pin to High or Low and not for SIUL2_PORT_HI_Z.&amp;nbsp;&amp;nbsp;&lt;BR /&gt;&lt;BR /&gt;&amp;nbsp;I hope this gives a bit more clarity.&amp;nbsp;&lt;/SPAN&gt;&lt;/P&gt;</description>
      <pubDate>Mon, 07 Apr 2025 12:09:56 GMT</pubDate>
      <guid>https://community.nxp.com/t5/S32K/S32K3-GPIO-HIGH-Z/m-p/2075153#M47535</guid>
      <dc:creator>ASN7</dc:creator>
      <dc:date>2025-04-07T12:09:56Z</dc:date>
    </item>
  </channel>
</rss>