<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>topic ADC triggering on the wrong pin in S32K</title>
    <link>https://community.nxp.com/t5/S32K/ADC-triggering-on-the-wrong-pin/m-p/2074572#M47499</link>
    <description>&lt;P&gt;Hello,&amp;nbsp;&lt;/P&gt;&lt;P&gt;I ran into an issue on the s32k311 with the RTD 5.0.0. I am using Tresos 29.0.0.&lt;/P&gt;&lt;P&gt;So, I want to use Adc0_s14 on the pin Ptc16 but it is triggering on the pin Ptb0. The channel is always reading close to max count because ptb0 is my Spi chip select. The channel is supposed to read close to 1.0V. To confirm, I changed Ptb0 to a Gpio and I triggered the Adc while toggling the pin. I was now reading values alternating between 0 and max count.&amp;nbsp;&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;I feel like the issue is similar to this one:&amp;nbsp;&lt;A href="https://community.nxp.com/t5/S32K/S32K3-ADC-Channcal-configure-problem/td-p/1527680" target="_blank"&gt;https://community.nxp.com/t5/S32K/S32K3-ADC-Channcal-configure-problem/td-p/1527680&lt;/A&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;Do we have a fix for the RTD 5.0.0 concerning this type of issue?&amp;nbsp;&lt;/P&gt;</description>
    <pubDate>Sat, 05 Apr 2025 12:21:53 GMT</pubDate>
    <dc:creator>AnthonyPinard</dc:creator>
    <dc:date>2025-04-05T12:21:53Z</dc:date>
    <item>
      <title>ADC triggering on the wrong pin</title>
      <link>https://community.nxp.com/t5/S32K/ADC-triggering-on-the-wrong-pin/m-p/2074572#M47499</link>
      <description>&lt;P&gt;Hello,&amp;nbsp;&lt;/P&gt;&lt;P&gt;I ran into an issue on the s32k311 with the RTD 5.0.0. I am using Tresos 29.0.0.&lt;/P&gt;&lt;P&gt;So, I want to use Adc0_s14 on the pin Ptc16 but it is triggering on the pin Ptb0. The channel is always reading close to max count because ptb0 is my Spi chip select. The channel is supposed to read close to 1.0V. To confirm, I changed Ptb0 to a Gpio and I triggered the Adc while toggling the pin. I was now reading values alternating between 0 and max count.&amp;nbsp;&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;I feel like the issue is similar to this one:&amp;nbsp;&lt;A href="https://community.nxp.com/t5/S32K/S32K3-ADC-Channcal-configure-problem/td-p/1527680" target="_blank"&gt;https://community.nxp.com/t5/S32K/S32K3-ADC-Channcal-configure-problem/td-p/1527680&lt;/A&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;Do we have a fix for the RTD 5.0.0 concerning this type of issue?&amp;nbsp;&lt;/P&gt;</description>
      <pubDate>Sat, 05 Apr 2025 12:21:53 GMT</pubDate>
      <guid>https://community.nxp.com/t5/S32K/ADC-triggering-on-the-wrong-pin/m-p/2074572#M47499</guid>
      <dc:creator>AnthonyPinard</dc:creator>
      <dc:date>2025-04-05T12:21:53Z</dc:date>
    </item>
    <item>
      <title>Re: ADC triggering on the wrong pin</title>
      <link>https://community.nxp.com/t5/S32K/ADC-triggering-on-the-wrong-pin/m-p/2074696#M47507</link>
      <description>&lt;P&gt;Hi&amp;nbsp;&lt;/P&gt;
&lt;P&gt;Sorry for the inconvenience we bring you!&lt;BR /&gt;This issue is discussed here: &lt;A href="https://community.nxp.com/t5/S32K/S32K311-S32K310-ADC-mux-mode-channels-was-abnormal/m-p/2015694#M44354" target="_self"&gt;S32K311_S32K310 ADC mux-mode channels was abnormal&lt;/A&gt;&lt;BR /&gt;I will send you the &lt;STRONG&gt;S32K311_ADC_Mux_Control.xlsx&lt;/STRONG&gt;.&lt;/P&gt;
&lt;P&gt;&lt;BR /&gt;Best Regards,&lt;BR /&gt;Robin&lt;BR /&gt;-------------------------------------------------------------------------------&lt;BR /&gt;Note:&lt;BR /&gt;- If this post answers your question, please click the "ACCEPT AS SOLUTION" button. Thank you!&lt;/P&gt;
&lt;P&gt;- We are following threads for 7 weeks after the last post, later replies are ignored&lt;BR /&gt;Please open a new thread and refer to the closed one, if you have a related question at a later point in time.&lt;BR /&gt;-------------------------------------------------------------------------------&lt;/P&gt;</description>
      <pubDate>Mon, 07 Apr 2025 02:12:50 GMT</pubDate>
      <guid>https://community.nxp.com/t5/S32K/ADC-triggering-on-the-wrong-pin/m-p/2074696#M47507</guid>
      <dc:creator>Robin_Shen</dc:creator>
      <dc:date>2025-04-07T02:12:50Z</dc:date>
    </item>
    <item>
      <title>Re: ADC triggering on the wrong pin</title>
      <link>https://community.nxp.com/t5/S32K/ADC-triggering-on-the-wrong-pin/m-p/2077160#M47607</link>
      <description>Thank you, Robin.&lt;BR /&gt;The solution mentioned is working.</description>
      <pubDate>Wed, 09 Apr 2025 13:28:49 GMT</pubDate>
      <guid>https://community.nxp.com/t5/S32K/ADC-triggering-on-the-wrong-pin/m-p/2077160#M47607</guid>
      <dc:creator>AnthonyPinard</dc:creator>
      <dc:date>2025-04-09T13:28:49Z</dc:date>
    </item>
  </channel>
</rss>