<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>S32K中的主题 Re: Use DMA to creat a Can Rx project in mcal</title>
    <link>https://community.nxp.com/t5/S32K/Use-DMA-to-creat-a-Can-Rx-project-in-mcal/m-p/2073462#M47448</link>
    <description>&lt;P&gt;Hi,&lt;/P&gt;
&lt;P&gt;not sure of the example directly, but necessary setting is outlined in driver manual in chapters&lt;BR /&gt;3.6.3 Legacy Rx FIFO Configuration&lt;BR /&gt;3.6.4 RxFifo Configuration with DMA support&lt;BR /&gt;Try to follow that&lt;/P&gt;
&lt;P&gt;BR, Petr&lt;/P&gt;</description>
    <pubDate>Thu, 03 Apr 2025 07:49:35 GMT</pubDate>
    <dc:creator>PetrS</dc:creator>
    <dc:date>2025-04-03T07:49:35Z</dc:date>
    <item>
      <title>Use DMA to creat a Can Rx project in mcal</title>
      <link>https://community.nxp.com/t5/S32K/Use-DMA-to-creat-a-Can-Rx-project-in-mcal/m-p/2072737#M47399</link>
      <description>&lt;P&gt;我使用mcal去配置can的DMA接收工程，同时使用can analyzer去发送消息，但是debug的时候，没有采集到can rx 消息，请问有可能是哪里的问题，platform and Rm 我都配置了？有没有实例来参考一下呢？&lt;/P&gt;</description>
      <pubDate>Wed, 02 Apr 2025 09:21:19 GMT</pubDate>
      <guid>https://community.nxp.com/t5/S32K/Use-DMA-to-creat-a-Can-Rx-project-in-mcal/m-p/2072737#M47399</guid>
      <dc:creator>fish</dc:creator>
      <dc:date>2025-04-02T09:21:19Z</dc:date>
    </item>
    <item>
      <title>Re: Use DMA to creat a Can Rx project in mcal</title>
      <link>https://community.nxp.com/t5/S32K/Use-DMA-to-creat-a-Can-Rx-project-in-mcal/m-p/2073462#M47448</link>
      <description>&lt;P&gt;Hi,&lt;/P&gt;
&lt;P&gt;not sure of the example directly, but necessary setting is outlined in driver manual in chapters&lt;BR /&gt;3.6.3 Legacy Rx FIFO Configuration&lt;BR /&gt;3.6.4 RxFifo Configuration with DMA support&lt;BR /&gt;Try to follow that&lt;/P&gt;
&lt;P&gt;BR, Petr&lt;/P&gt;</description>
      <pubDate>Thu, 03 Apr 2025 07:49:35 GMT</pubDate>
      <guid>https://community.nxp.com/t5/S32K/Use-DMA-to-creat-a-Can-Rx-project-in-mcal/m-p/2073462#M47448</guid>
      <dc:creator>PetrS</dc:creator>
      <dc:date>2025-04-03T07:49:35Z</dc:date>
    </item>
  </channel>
</rss>