<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>topic S32K3 GPIO Source Current in S32K</title>
    <link>https://community.nxp.com/t5/S32K/S32K3-GPIO-Source-Current/m-p/2073413#M47445</link>
    <description>&lt;P&gt;Hi,&lt;BR /&gt;&lt;BR /&gt;I want to use S32K3 in a Sensor Application to power some sensors and external circuitry directly from GPIOs. I&lt;SPAN&gt;n the Datasheet, there are specifications, where a minimum GPIO current is given &lt;SPAN&gt;(S32K3xx Data Sheet, Rev. 10, 07/2024&amp;nbsp;Table 24, 3.3V or Table 25, 5V)&lt;/SPAN&gt;.&lt;BR /&gt;&lt;/SPAN&gt;&lt;/P&gt;&lt;P&gt;&lt;SPAN&gt;Though I do not completely understand these specs.&lt;/SPAN&gt;&lt;/P&gt;&lt;P&gt;&lt;SPAN&gt;IOH_50_S is 1.6mA,min for VOH &amp;gt;= VDD_HV_A/B - 0.7V as example from Table 25.&lt;BR /&gt;&lt;BR /&gt;Does that mean, that I can only draw 1.6mA from an Standard GPIO running at 5V?&lt;BR /&gt;From the given measurement condition, can I also assume, that the Resistance of the GPIO-Structure is somewhere around 450Ohm (0.7V/1.6mA)?&lt;BR /&gt;&lt;BR /&gt;&lt;BR /&gt;&lt;/SPAN&gt;&lt;/P&gt;&lt;P&gt;&lt;SPAN&gt;Thank you!&lt;/SPAN&gt;&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;</description>
    <pubDate>Thu, 03 Apr 2025 07:10:05 GMT</pubDate>
    <dc:creator>FabianGeiger</dc:creator>
    <dc:date>2025-04-03T07:10:05Z</dc:date>
    <item>
      <title>S32K3 GPIO Source Current</title>
      <link>https://community.nxp.com/t5/S32K/S32K3-GPIO-Source-Current/m-p/2073413#M47445</link>
      <description>&lt;P&gt;Hi,&lt;BR /&gt;&lt;BR /&gt;I want to use S32K3 in a Sensor Application to power some sensors and external circuitry directly from GPIOs. I&lt;SPAN&gt;n the Datasheet, there are specifications, where a minimum GPIO current is given &lt;SPAN&gt;(S32K3xx Data Sheet, Rev. 10, 07/2024&amp;nbsp;Table 24, 3.3V or Table 25, 5V)&lt;/SPAN&gt;.&lt;BR /&gt;&lt;/SPAN&gt;&lt;/P&gt;&lt;P&gt;&lt;SPAN&gt;Though I do not completely understand these specs.&lt;/SPAN&gt;&lt;/P&gt;&lt;P&gt;&lt;SPAN&gt;IOH_50_S is 1.6mA,min for VOH &amp;gt;= VDD_HV_A/B - 0.7V as example from Table 25.&lt;BR /&gt;&lt;BR /&gt;Does that mean, that I can only draw 1.6mA from an Standard GPIO running at 5V?&lt;BR /&gt;From the given measurement condition, can I also assume, that the Resistance of the GPIO-Structure is somewhere around 450Ohm (0.7V/1.6mA)?&lt;BR /&gt;&lt;BR /&gt;&lt;BR /&gt;&lt;/SPAN&gt;&lt;/P&gt;&lt;P&gt;&lt;SPAN&gt;Thank you!&lt;/SPAN&gt;&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;</description>
      <pubDate>Thu, 03 Apr 2025 07:10:05 GMT</pubDate>
      <guid>https://community.nxp.com/t5/S32K/S32K3-GPIO-Source-Current/m-p/2073413#M47445</guid>
      <dc:creator>FabianGeiger</dc:creator>
      <dc:date>2025-04-03T07:10:05Z</dc:date>
    </item>
    <item>
      <title>Re: S32K3 GPIO Source Current</title>
      <link>https://community.nxp.com/t5/S32K/S32K3-GPIO-Source-Current/m-p/2073647#M47456</link>
      <description>&lt;P&gt;Hi Fabian,&lt;/P&gt;
&lt;P&gt;The specification means that NXP can guarantee that the voltage will not drop by more than 0.7V at 1.6mA source current.&lt;/P&gt;
&lt;P&gt;If the source current is higher, the voltage can drop further.&lt;/P&gt;
&lt;P&gt;The I–V characteristic is not exactly linear but exponential (especially at higher currents).&lt;/P&gt;
&lt;P&gt;Refer to this AN:&amp;nbsp;Input/Output (I/O) Pin Drivers on HCS12 Family MCUs&lt;/P&gt;
&lt;P&gt;&lt;A href="https://www.nxp.com/docs/en/application-note/AN2434.pdf" target="_blank" rel="noopener"&gt;https://www.nxp.com/docs/en/application-note/AN2434.pdf&lt;/A&gt;&lt;/P&gt;
&lt;P&gt;It is an older AN, but the principles remain the same.&lt;/P&gt;
&lt;P&gt;&amp;nbsp;&lt;/P&gt;
&lt;P&gt;There are also IBIS models available in the S32K3xx HW package.&lt;/P&gt;
&lt;P&gt;&lt;A href="https://www.nxp.com/webapp/Download?colCode=S32K3_HW-DesignPackage" target="_blank"&gt;https://www.nxp.com/webapp/Download?colCode=S32K3_HW-DesignPackage&lt;/A&gt;&lt;/P&gt;
&lt;P&gt;&amp;nbsp;&lt;/P&gt;
&lt;P&gt;Regards,&lt;/P&gt;
&lt;P&gt;Daniel&lt;/P&gt;
&lt;P&gt;&amp;nbsp;&lt;/P&gt;
&lt;P&gt;&amp;nbsp;&lt;/P&gt;
&lt;P&gt;&amp;nbsp;&lt;/P&gt;</description>
      <pubDate>Thu, 03 Apr 2025 11:12:30 GMT</pubDate>
      <guid>https://community.nxp.com/t5/S32K/S32K3-GPIO-Source-Current/m-p/2073647#M47456</guid>
      <dc:creator>danielmartynek</dc:creator>
      <dc:date>2025-04-03T11:12:30Z</dc:date>
    </item>
  </channel>
</rss>