<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>topic HSE firmware flash in S32K</title>
    <link>https://community.nxp.com/t5/S32K/HSE-firmware-flash/m-p/2072712#M47394</link>
    <description>&lt;P&gt;&lt;SPAN&gt;Hello I'm using s32k324 board and I'm trying to flash hse firmware&lt;/SPAN&gt;&lt;BR /&gt;&lt;SPAN&gt;I have some questions.&lt;/SPAN&gt;&lt;BR /&gt;&lt;BR /&gt;&lt;SPAN&gt;1. Is the flash method shown in the 데모 demo release notes the right way to flash hse to the board?&lt;/SPAN&gt;&lt;BR /&gt;&lt;BR /&gt;&lt;SPAN&gt;2. If I want to flash the hse firmware, does the debugger have to be trace32? I'm pemicro. According to the demo release notes, it only shows that I used trace32. And .cmm is only supported on trace32.&lt;/SPAN&gt;&lt;BR /&gt;&lt;BR /&gt;&lt;SPAN&gt;3. I'm using a pemicro debugger, how do I flash hse firmware on the board?&lt;/SPAN&gt;&lt;/P&gt;</description>
    <pubDate>Wed, 02 Apr 2025 08:51:22 GMT</pubDate>
    <dc:creator>minjaekang99</dc:creator>
    <dc:date>2025-04-02T08:51:22Z</dc:date>
    <item>
      <title>HSE firmware flash</title>
      <link>https://community.nxp.com/t5/S32K/HSE-firmware-flash/m-p/2072712#M47394</link>
      <description>&lt;P&gt;&lt;SPAN&gt;Hello I'm using s32k324 board and I'm trying to flash hse firmware&lt;/SPAN&gt;&lt;BR /&gt;&lt;SPAN&gt;I have some questions.&lt;/SPAN&gt;&lt;BR /&gt;&lt;BR /&gt;&lt;SPAN&gt;1. Is the flash method shown in the 데모 demo release notes the right way to flash hse to the board?&lt;/SPAN&gt;&lt;BR /&gt;&lt;BR /&gt;&lt;SPAN&gt;2. If I want to flash the hse firmware, does the debugger have to be trace32? I'm pemicro. According to the demo release notes, it only shows that I used trace32. And .cmm is only supported on trace32.&lt;/SPAN&gt;&lt;BR /&gt;&lt;BR /&gt;&lt;SPAN&gt;3. I'm using a pemicro debugger, how do I flash hse firmware on the board?&lt;/SPAN&gt;&lt;/P&gt;</description>
      <pubDate>Wed, 02 Apr 2025 08:51:22 GMT</pubDate>
      <guid>https://community.nxp.com/t5/S32K/HSE-firmware-flash/m-p/2072712#M47394</guid>
      <dc:creator>minjaekang99</dc:creator>
      <dc:date>2025-04-02T08:51:22Z</dc:date>
    </item>
    <item>
      <title>Re: HSE firmware flash</title>
      <link>https://community.nxp.com/t5/S32K/HSE-firmware-flash/m-p/2072914#M47414</link>
      <description>&lt;P&gt;Hi &lt;a href="https://community.nxp.com/t5/user/viewprofilepage/user-id/242600"&gt;@minjaekang99&lt;/a&gt;&amp;nbsp;&lt;/P&gt;
&lt;P&gt;HSE DemoApp requires Trace32 debugger. But we have also these HSE demo examples:&lt;BR /&gt;&lt;A href="https://www.nxp.com/webapp/Download?colCode=S32K3_HSE_DemoExamples" target="_blank"&gt;https://www.nxp.com/webapp/Download?colCode=S32K3_HSE_DemoExamples&lt;/A&gt;&lt;BR /&gt;In fact, it’s HSE DemoApp ported to individual simple SW examples and you can use any debugger to run it. &lt;BR /&gt;After installation of the package, you can find this example:&lt;BR /&gt;c:\NXP\S32K3_HSE_DemoExamples_1_0_0\S32K3_HSE_DemoExamples\Device_Configuration\S32K344_HSE_FW_INSTALL\&lt;BR /&gt;Follow included readme file. It's necessary to update the paths to HSE firmware pink file.&lt;/P&gt;
&lt;P&gt;HSE firmware can be installed by three methods - by default location, by IVT and by MU. It's described in HSE-B firmware reference manual (section "3 HSE Firmware Installation") which can be downloaded from :&lt;BR /&gt;&lt;A href="https://www.nxp.com/products/S32K3" target="_blank"&gt;https://www.nxp.com/products/S32K3&lt;/A&gt;&lt;BR /&gt;You can find it in section Documentation -&amp;gt; Secure Files.&lt;/P&gt;
&lt;P&gt;&lt;BR /&gt;Regards,&lt;BR /&gt;Lukas&lt;/P&gt;</description>
      <pubDate>Wed, 02 Apr 2025 13:56:24 GMT</pubDate>
      <guid>https://community.nxp.com/t5/S32K/HSE-firmware-flash/m-p/2072914#M47414</guid>
      <dc:creator>lukaszadrapa</dc:creator>
      <dc:date>2025-04-02T13:56:24Z</dc:date>
    </item>
  </channel>
</rss>