<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>S32KのトピックRe: Reception supported through both Rx FIFO and individual buffer at same instance</title>
    <link>https://community.nxp.com/t5/S32K/Reception-supported-through-both-Rx-FIFO-and-individual-buffer/m-p/914321#M4732</link>
    <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hi,&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;yes. this is possible.&lt;/P&gt;&lt;P&gt;You can refer to simple example on&amp;nbsp;&lt;A href="https://community.nxp.com/docs/DOC-343091"&gt;https://community.nxp.com/docs/DOC-343091&lt;/A&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;BR, Petr&amp;nbsp;&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
    <pubDate>Thu, 29 Aug 2019 06:35:22 GMT</pubDate>
    <dc:creator>PetrS</dc:creator>
    <dc:date>2019-08-29T06:35:22Z</dc:date>
    <item>
      <title>Reception supported through both Rx FIFO and individual buffer at same instance</title>
      <link>https://community.nxp.com/t5/S32K/Reception-supported-through-both-Rx-FIFO-and-individual-buffer/m-p/914320#M4731</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hi,&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;In S32K148, is reception supported through both &lt;STRONG&gt;Rx FIFO and individual buffer&lt;/STRONG&gt; at same instance.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;For Example:&lt;/P&gt;&lt;P&gt;-&amp;gt; I will enable FIFO.&lt;/P&gt;&lt;P&gt;-&amp;gt; 0-10 buffers are provided for FIFO reception.&lt;/P&gt;&lt;P&gt;-&amp;gt; 11-15&amp;nbsp;are provided for dedicated reception, will hardware try to find a match in&amp;nbsp;11-15 buffers if reception doesn't pass through FIFO filters.&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Wed, 28 Aug 2019 06:52:17 GMT</pubDate>
      <guid>https://community.nxp.com/t5/S32K/Reception-supported-through-both-Rx-FIFO-and-individual-buffer/m-p/914320#M4731</guid>
      <dc:creator>chandru_v</dc:creator>
      <dc:date>2019-08-28T06:52:17Z</dc:date>
    </item>
    <item>
      <title>Re: Reception supported through both Rx FIFO and individual buffer at same instance</title>
      <link>https://community.nxp.com/t5/S32K/Reception-supported-through-both-Rx-FIFO-and-individual-buffer/m-p/914321#M4732</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hi,&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;yes. this is possible.&lt;/P&gt;&lt;P&gt;You can refer to simple example on&amp;nbsp;&lt;A href="https://community.nxp.com/docs/DOC-343091"&gt;https://community.nxp.com/docs/DOC-343091&lt;/A&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;BR, Petr&amp;nbsp;&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Thu, 29 Aug 2019 06:35:22 GMT</pubDate>
      <guid>https://community.nxp.com/t5/S32K/Reception-supported-through-both-Rx-FIFO-and-individual-buffer/m-p/914321#M4732</guid>
      <dc:creator>PetrS</dc:creator>
      <dc:date>2019-08-29T06:35:22Z</dc:date>
    </item>
  </channel>
</rss>