<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>topic Re: S32K Crystal Drive, Gain Control in S32K</title>
    <link>https://community.nxp.com/t5/S32K/S32K-Crystal-Drive-Gain-Control/m-p/913590#M4730</link>
    <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hi Patrick Langlois&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Yes, there is an automatic control that will do this internally, customer has to connect the external resistors based in the crystal manufacture specifications.&amp;nbsp; When high gain is selected, provides better noise immunity but does draw/ higher current, with low gain power consuption will be lower and customer can see a smaller signal in the pins due to the power saving.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Regards&lt;/P&gt;&lt;P&gt;Jorge Alcala&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
    <pubDate>Tue, 18 Jun 2019 13:54:14 GMT</pubDate>
    <dc:creator>jorge_a_vazquez</dc:creator>
    <dc:date>2019-06-18T13:54:14Z</dc:date>
    <item>
      <title>S32K Crystal Drive, Gain Control</title>
      <link>https://community.nxp.com/t5/S32K/S32K-Crystal-Drive-Gain-Control/m-p/913589#M4729</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hi,&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Looking at the datasheet, reference manual and application notes for the S32K microcontrollers, I can't understand if there is a minimum automatic gain control additionally to the programmable one (HI/LO gain) for an external crystal drive (SOSC).&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;&lt;EM&gt; To be as clear as possible...&lt;/EM&gt;&lt;/P&gt;&lt;P&gt;For each range of crystal frequencies "covered" by each of both manual gain settings, is there some automatic control that will increase the crystal drive to provide a proper level of response on the inverter input?&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Regards.&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Wed, 12 Jun 2019 12:18:55 GMT</pubDate>
      <guid>https://community.nxp.com/t5/S32K/S32K-Crystal-Drive-Gain-Control/m-p/913589#M4729</guid>
      <dc:creator>patricklanglois</dc:creator>
      <dc:date>2019-06-12T12:18:55Z</dc:date>
    </item>
    <item>
      <title>Re: S32K Crystal Drive, Gain Control</title>
      <link>https://community.nxp.com/t5/S32K/S32K-Crystal-Drive-Gain-Control/m-p/913590#M4730</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hi Patrick Langlois&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Yes, there is an automatic control that will do this internally, customer has to connect the external resistors based in the crystal manufacture specifications.&amp;nbsp; When high gain is selected, provides better noise immunity but does draw/ higher current, with low gain power consuption will be lower and customer can see a smaller signal in the pins due to the power saving.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Regards&lt;/P&gt;&lt;P&gt;Jorge Alcala&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Tue, 18 Jun 2019 13:54:14 GMT</pubDate>
      <guid>https://community.nxp.com/t5/S32K/S32K-Crystal-Drive-Gain-Control/m-p/913590#M4730</guid>
      <dc:creator>jorge_a_vazquez</dc:creator>
      <dc:date>2019-06-18T13:54:14Z</dc:date>
    </item>
  </channel>
</rss>