<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>topic S32K3xx Interrupt vector table in S32K</title>
    <link>https://community.nxp.com/t5/S32K/S32K3xx-Interrupt-vector-table/m-p/2069204#M47201</link>
    <description>&lt;P&gt;Hi,&lt;BR /&gt;I have some doubts about the interrupt vector table (S32K344 and S32K358 MCU).&lt;BR /&gt;1. myproject -&amp;gt; Project_Settings -&amp;gt; Startup_Code -&amp;gt; Vector_Table.s—there is no CAN or other peripheral interrupt handler defined?&lt;BR /&gt;2. IntCtrl_Ip.h is used to initialize the CAN interrupt handler but is not shown in the Vector_Table, for example, the message buffer 0 to 31 IRQ number 110 place.how actualy IntCtrl_Ip used to initialized CAN&lt;BR /&gt;or other peripheral intrrupt handler working?&lt;BR /&gt;3. Is there any reason or difference to define vector table in RAM and ROM separately?&lt;BR /&gt;4. If I want my peripheral interrupt handler to be defined in ROM (interrupt_Vector_Table.s), then what do I want to do?&lt;BR /&gt;5. There is no information about the nested interrupt vector table in the reference manual. Then where do I want to learn for the S32K3xx MCU?&lt;/P&gt;&lt;P&gt;IDE - S32DS V3.5.14&lt;/P&gt;&lt;P&gt;HARDWARE—S32K344 and S32K358&lt;/P&gt;&lt;P&gt;SDK - V4.0.0&lt;/P&gt;</description>
    <pubDate>Thu, 27 Mar 2025 05:45:08 GMT</pubDate>
    <dc:creator>karmegancjk</dc:creator>
    <dc:date>2025-03-27T05:45:08Z</dc:date>
    <item>
      <title>S32K3xx Interrupt vector table</title>
      <link>https://community.nxp.com/t5/S32K/S32K3xx-Interrupt-vector-table/m-p/2069204#M47201</link>
      <description>&lt;P&gt;Hi,&lt;BR /&gt;I have some doubts about the interrupt vector table (S32K344 and S32K358 MCU).&lt;BR /&gt;1. myproject -&amp;gt; Project_Settings -&amp;gt; Startup_Code -&amp;gt; Vector_Table.s—there is no CAN or other peripheral interrupt handler defined?&lt;BR /&gt;2. IntCtrl_Ip.h is used to initialize the CAN interrupt handler but is not shown in the Vector_Table, for example, the message buffer 0 to 31 IRQ number 110 place.how actualy IntCtrl_Ip used to initialized CAN&lt;BR /&gt;or other peripheral intrrupt handler working?&lt;BR /&gt;3. Is there any reason or difference to define vector table in RAM and ROM separately?&lt;BR /&gt;4. If I want my peripheral interrupt handler to be defined in ROM (interrupt_Vector_Table.s), then what do I want to do?&lt;BR /&gt;5. There is no information about the nested interrupt vector table in the reference manual. Then where do I want to learn for the S32K3xx MCU?&lt;/P&gt;&lt;P&gt;IDE - S32DS V3.5.14&lt;/P&gt;&lt;P&gt;HARDWARE—S32K344 and S32K358&lt;/P&gt;&lt;P&gt;SDK - V4.0.0&lt;/P&gt;</description>
      <pubDate>Thu, 27 Mar 2025 05:45:08 GMT</pubDate>
      <guid>https://community.nxp.com/t5/S32K/S32K3xx-Interrupt-vector-table/m-p/2069204#M47201</guid>
      <dc:creator>karmegancjk</dc:creator>
      <dc:date>2025-03-27T05:45:08Z</dc:date>
    </item>
  </channel>
</rss>