<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>S32KのトピックIAR Compiler plugin for S32DS</title>
    <link>https://community.nxp.com/t5/S32K/IAR-Compiler-plugin-for-S32DS/m-p/2069190#M47199</link>
    <description>&lt;P class=""&gt;We are currently working on a project using &lt;STRONG&gt;S32K148&lt;/STRONG&gt; with &lt;STRONG&gt;S32 Design Studio 3.5 (S32DS 3.5)&lt;/STRONG&gt; and &lt;STRONG&gt;RTD 2.0.0&lt;/STRONG&gt; along with &lt;STRONG&gt;FreeRTOS&lt;/STRONG&gt;. As part of our development, we are considering switching to the &lt;STRONG&gt;IAR compiler&lt;/STRONG&gt; and need guidance on its compatibility with S32DS.&lt;/P&gt;&lt;H3&gt;&lt;STRONG&gt;Our Key Requirements:&lt;/STRONG&gt;&lt;/H3&gt;&lt;OL&gt;&lt;LI&gt;&lt;P class=""&gt;&lt;STRONG&gt;Which IAR compiler version is suitable&lt;/STRONG&gt; for integration with &lt;STRONG&gt;S32DS 3.5&lt;/STRONG&gt;?&lt;/P&gt;&lt;/LI&gt;&lt;LI&gt;&lt;P class=""&gt;&lt;STRONG&gt;Is there an official IAR plugin&lt;/STRONG&gt; available for S32DS 3.5, and how can we install it?&lt;/P&gt;&lt;/LI&gt;&lt;LI&gt;&lt;P class=""&gt;Are there any &lt;STRONG&gt;known issues or limitations&lt;/STRONG&gt; when using IAR with &lt;STRONG&gt;S32K148 + RTD 2.0.0 + FreeRTOS&lt;/STRONG&gt;?&lt;/P&gt;&lt;/LI&gt;&lt;LI&gt;&lt;P class=""&gt;Is there any &lt;STRONG&gt;migration guide&lt;/STRONG&gt; or documentation for transitioning from the default GCC toolchain to IAR within S32DS?&lt;/P&gt;&lt;/LI&gt;&lt;/OL&gt;&lt;P class=""&gt;Additionally, if IAR is not directly supported via a plugin, is there any alternative way to configure S32DS to &lt;STRONG&gt;build and debug&lt;/STRONG&gt; using the IAR toolchain?&lt;/P&gt;</description>
    <pubDate>Thu, 27 Mar 2025 05:10:54 GMT</pubDate>
    <dc:creator>AdithyaJayaram1996</dc:creator>
    <dc:date>2025-03-27T05:10:54Z</dc:date>
    <item>
      <title>IAR Compiler plugin for S32DS</title>
      <link>https://community.nxp.com/t5/S32K/IAR-Compiler-plugin-for-S32DS/m-p/2069190#M47199</link>
      <description>&lt;P class=""&gt;We are currently working on a project using &lt;STRONG&gt;S32K148&lt;/STRONG&gt; with &lt;STRONG&gt;S32 Design Studio 3.5 (S32DS 3.5)&lt;/STRONG&gt; and &lt;STRONG&gt;RTD 2.0.0&lt;/STRONG&gt; along with &lt;STRONG&gt;FreeRTOS&lt;/STRONG&gt;. As part of our development, we are considering switching to the &lt;STRONG&gt;IAR compiler&lt;/STRONG&gt; and need guidance on its compatibility with S32DS.&lt;/P&gt;&lt;H3&gt;&lt;STRONG&gt;Our Key Requirements:&lt;/STRONG&gt;&lt;/H3&gt;&lt;OL&gt;&lt;LI&gt;&lt;P class=""&gt;&lt;STRONG&gt;Which IAR compiler version is suitable&lt;/STRONG&gt; for integration with &lt;STRONG&gt;S32DS 3.5&lt;/STRONG&gt;?&lt;/P&gt;&lt;/LI&gt;&lt;LI&gt;&lt;P class=""&gt;&lt;STRONG&gt;Is there an official IAR plugin&lt;/STRONG&gt; available for S32DS 3.5, and how can we install it?&lt;/P&gt;&lt;/LI&gt;&lt;LI&gt;&lt;P class=""&gt;Are there any &lt;STRONG&gt;known issues or limitations&lt;/STRONG&gt; when using IAR with &lt;STRONG&gt;S32K148 + RTD 2.0.0 + FreeRTOS&lt;/STRONG&gt;?&lt;/P&gt;&lt;/LI&gt;&lt;LI&gt;&lt;P class=""&gt;Is there any &lt;STRONG&gt;migration guide&lt;/STRONG&gt; or documentation for transitioning from the default GCC toolchain to IAR within S32DS?&lt;/P&gt;&lt;/LI&gt;&lt;/OL&gt;&lt;P class=""&gt;Additionally, if IAR is not directly supported via a plugin, is there any alternative way to configure S32DS to &lt;STRONG&gt;build and debug&lt;/STRONG&gt; using the IAR toolchain?&lt;/P&gt;</description>
      <pubDate>Thu, 27 Mar 2025 05:10:54 GMT</pubDate>
      <guid>https://community.nxp.com/t5/S32K/IAR-Compiler-plugin-for-S32DS/m-p/2069190#M47199</guid>
      <dc:creator>AdithyaJayaram1996</dc:creator>
      <dc:date>2025-03-27T05:10:54Z</dc:date>
    </item>
    <item>
      <title>Re: IAR Compiler plugin for S32DS</title>
      <link>https://community.nxp.com/t5/S32K/IAR-Compiler-plugin-for-S32DS/m-p/2070310#M47269</link>
      <description>&lt;P&gt;Hi,&amp;nbsp;&lt;/P&gt;
&lt;P&gt;you can use for example IAR v9.32 - but any other version offered by IAR plugin manager can be used. Here is document how to install IAR plugin:&amp;nbsp;&lt;/P&gt;
&lt;P&gt;&lt;BR /&gt;&lt;A href="https://community.nxp.com/t5/S32-Design-Studio-Knowledge-Base/HOWTO-Install-IAR-Eclipse-plug-in-into-S32-Design-Studio-3-4/ta-p/1561369" target="_blank"&gt;https://community.nxp.com/t5/S32-Design-Studio-Knowledge-Base/HOWTO-Install-IAR-Eclipse-plug-in-into-S32-Design-Studio-3-4/ta-p/1561369&lt;/A&gt;&lt;BR /&gt;&lt;BR /&gt;&lt;/P&gt;</description>
      <pubDate>Fri, 28 Mar 2025 12:39:34 GMT</pubDate>
      <guid>https://community.nxp.com/t5/S32K/IAR-Compiler-plugin-for-S32DS/m-p/2070310#M47269</guid>
      <dc:creator>jiri_kral</dc:creator>
      <dc:date>2025-03-28T12:39:34Z</dc:date>
    </item>
  </channel>
</rss>