<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>topic Re: SPI : Multiple Slave communication over shared Slave Select line in S32K</title>
    <link>https://community.nxp.com/t5/S32K/SPI-Multiple-Slave-communication-over-shared-Slave-Select-line/m-p/909711#M4698</link>
    <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hi&amp;nbsp;Amarjeet,&lt;/P&gt;&lt;P&gt;I’m not sure if I understand.&lt;BR /&gt;All the ports that you mentioned (PTA9, PTC14, PTE11) can be used for LPSPI0_PCS0.&lt;BR /&gt;So, it would be as if you used just one PSC0 pin and route it to all the slaves.&lt;BR /&gt;Without the daisy chain, all the slave would transmit on the MISO line at the same time.&lt;/P&gt;&lt;P&gt;Could you please elaborate?&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;BR, Daniel&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
    <pubDate>Fri, 27 Sep 2019 13:33:48 GMT</pubDate>
    <dc:creator>danielmartynek</dc:creator>
    <dc:date>2019-09-27T13:33:48Z</dc:date>
    <item>
      <title>SPI : Multiple Slave communication over shared Slave Select line</title>
      <link>https://community.nxp.com/t5/S32K/SPI-Multiple-Slave-communication-over-shared-Slave-Select-line/m-p/909710#M4697</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hi All Community Members&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Is it possible to communicate to the slave over share slave select (peripheral chip select line) as per below config without using Daisy-chain SPI bus scheme:&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;For Example:&lt;/P&gt;&lt;P&gt;&lt;SPAN style="color: #51626f; background-color: #ffffff;"&gt;&lt;SPAN&gt;LPSPI2&amp;nbsp;&lt;/SPAN&gt;pcs0:&amp;nbsp;PTA9, PTC14, PTE11&lt;/SPAN&gt;&lt;/P&gt;&lt;P&gt;&lt;SPAN style="color: #51626f; background-color: #ffffff;"&gt;like pin &lt;SPAN&gt;PTA9&amp;nbsp;&lt;/SPAN&gt;is used for Slave-1, &lt;SPAN&gt;PTC14&amp;nbsp;&lt;/SPAN&gt;used for &lt;SPAN&gt;Slave-2&lt;/SPAN&gt;, &lt;SPAN&gt;PTE11&amp;nbsp;&lt;/SPAN&gt;used for &lt;SPAN&gt;Slave-3&lt;/SPAN&gt;.&lt;/SPAN&gt;&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;&lt;SPAN style="color: #51626f; background-color: #ffffff;"&gt;&lt;span class="lia-inline-image-display-wrapper" image-alt="1.PNG"&gt;&lt;img src="https://community.nxp.com/t5/image/serverpage/image-id/84947iCC3F691DB4C616AE/image-size/large?v=v2&amp;amp;px=999" role="button" title="1.PNG" alt="1.PNG" /&gt;&lt;/span&gt;&lt;/SPAN&gt;&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;&lt;SPAN style="color: #51626f; background-color: #ffffff;"&gt;can someone please share the test project for above configuration using SDK for s32k144 EVB-Q100.&lt;/SPAN&gt;&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;&lt;SPAN style="color: #51626f; background-color: #ffffff;"&gt;Thanks&lt;/SPAN&gt;&lt;/P&gt;&lt;P&gt;&lt;SPAN style="color: #51626f; background-color: #ffffff;"&gt;Amarjeet&lt;/SPAN&gt;&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Wed, 25 Sep 2019 13:21:45 GMT</pubDate>
      <guid>https://community.nxp.com/t5/S32K/SPI-Multiple-Slave-communication-over-shared-Slave-Select-line/m-p/909710#M4697</guid>
      <dc:creator>amarjeet_kumar</dc:creator>
      <dc:date>2019-09-25T13:21:45Z</dc:date>
    </item>
    <item>
      <title>Re: SPI : Multiple Slave communication over shared Slave Select line</title>
      <link>https://community.nxp.com/t5/S32K/SPI-Multiple-Slave-communication-over-shared-Slave-Select-line/m-p/909711#M4698</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hi&amp;nbsp;Amarjeet,&lt;/P&gt;&lt;P&gt;I’m not sure if I understand.&lt;BR /&gt;All the ports that you mentioned (PTA9, PTC14, PTE11) can be used for LPSPI0_PCS0.&lt;BR /&gt;So, it would be as if you used just one PSC0 pin and route it to all the slaves.&lt;BR /&gt;Without the daisy chain, all the slave would transmit on the MISO line at the same time.&lt;/P&gt;&lt;P&gt;Could you please elaborate?&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;BR, Daniel&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Fri, 27 Sep 2019 13:33:48 GMT</pubDate>
      <guid>https://community.nxp.com/t5/S32K/SPI-Multiple-Slave-communication-over-shared-Slave-Select-line/m-p/909711#M4698</guid>
      <dc:creator>danielmartynek</dc:creator>
      <dc:date>2019-09-27T13:33:48Z</dc:date>
    </item>
  </channel>
</rss>