<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>S32K中的主题 S32K3</title>
    <link>https://community.nxp.com/t5/S32K/S32K3/m-p/2064571#M46964</link>
    <description>&lt;P&gt;Application consultation about S32K314NHT1VPBST product&lt;BR /&gt;I used two batches of chips here (DC2322 and DC24+).&lt;BR /&gt;After using the DC24+chip, the static current is only 80uA.&lt;BR /&gt;But I found that the static current of the DC2322 batch of chips exceeded the standard, reaching 280uA.&lt;BR /&gt;I want to confirm why this is? Is there a difference between two different batches of chips? Or would circuit design lead to the existence of such differences?&lt;/P&gt;</description>
    <pubDate>Wed, 19 Mar 2025 09:17:20 GMT</pubDate>
    <dc:creator>yy12</dc:creator>
    <dc:date>2025-03-19T09:17:20Z</dc:date>
    <item>
      <title>S32K3</title>
      <link>https://community.nxp.com/t5/S32K/S32K3/m-p/2064571#M46964</link>
      <description>&lt;P&gt;Application consultation about S32K314NHT1VPBST product&lt;BR /&gt;I used two batches of chips here (DC2322 and DC24+).&lt;BR /&gt;After using the DC24+chip, the static current is only 80uA.&lt;BR /&gt;But I found that the static current of the DC2322 batch of chips exceeded the standard, reaching 280uA.&lt;BR /&gt;I want to confirm why this is? Is there a difference between two different batches of chips? Or would circuit design lead to the existence of such differences?&lt;/P&gt;</description>
      <pubDate>Wed, 19 Mar 2025 09:17:20 GMT</pubDate>
      <guid>https://community.nxp.com/t5/S32K/S32K3/m-p/2064571#M46964</guid>
      <dc:creator>yy12</dc:creator>
      <dc:date>2025-03-19T09:17:20Z</dc:date>
    </item>
  </channel>
</rss>