<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>topic Re: S32K344 BIST HSE_SWT reset in S32K</title>
    <link>https://community.nxp.com/t5/S32K/S32K344-BIST-HSE-SWT-reset/m-p/2064018#M46925</link>
    <description>&lt;P&gt;Hi&amp;nbsp;&lt;a href="https://community.nxp.com/t5/user/viewprofilepage/user-id/248181"&gt;@Jason22&lt;/a&gt;&amp;nbsp;&lt;/P&gt;
&lt;P&gt;HSE-enabled devices do not have the ability to disable HSE_SWT due to security concerns. The internal team performed the self-test from the application core on an SoC with the HSE installed, and no abnormalities were observed.&lt;/P&gt;
&lt;P&gt;During the self-test, the HSE is servicing the watchdog, so no reset will be triggered by the HSE. Therefore, the application does not need to disable anything to perform the self-test, as the HSE handles it.&lt;/P&gt;
&lt;P&gt;We understand that the documentation may cause confusion, so a ticket has already been raised to verify this situation.&lt;/P&gt;
&lt;P&gt;&amp;nbsp;&lt;/P&gt;
&lt;P&gt;BR, VaneB&lt;/P&gt;</description>
    <pubDate>Tue, 18 Mar 2025 19:04:02 GMT</pubDate>
    <dc:creator>VaneB</dc:creator>
    <dc:date>2025-03-18T19:04:02Z</dc:date>
    <item>
      <title>S32K344 BIST HSE_SWT reset</title>
      <link>https://community.nxp.com/t5/S32K/S32K344-BIST-HSE-SWT-reset/m-p/2063367#M46879</link>
      <description>&lt;P&gt;In the demo of SPD1.0.4, executing Bist_Run (BIS_SAFETYBOOT_CFG) will reset, but the reason for the reset is MCU_HSE_SWT_RST_RESET. I have reviewed the reference manual and found that HSE_SWT should be disabled.&lt;/P&gt;&lt;P&gt;&lt;span class="lia-inline-image-display-wrapper lia-image-align-inline" image-alt="Jason22_0-1742267782251.png" style="width: 400px;"&gt;&lt;img src="https://community.nxp.com/t5/image/serverpage/image-id/328522i63A8BC5F2CCFC0F4/image-size/medium?v=v2&amp;amp;px=400" role="button" title="Jason22_0-1742267782251.png" alt="Jason22_0-1742267782251.png" /&gt;&lt;/span&gt;&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;Do I need to manually disable it? If so, what should I do?&lt;/P&gt;</description>
      <pubDate>Tue, 18 Mar 2025 03:19:37 GMT</pubDate>
      <guid>https://community.nxp.com/t5/S32K/S32K344-BIST-HSE-SWT-reset/m-p/2063367#M46879</guid>
      <dc:creator>Jason22</dc:creator>
      <dc:date>2025-03-18T03:19:37Z</dc:date>
    </item>
    <item>
      <title>Re: S32K344 BIST HSE_SWT reset</title>
      <link>https://community.nxp.com/t5/S32K/S32K344-BIST-HSE-SWT-reset/m-p/2064018#M46925</link>
      <description>&lt;P&gt;Hi&amp;nbsp;&lt;a href="https://community.nxp.com/t5/user/viewprofilepage/user-id/248181"&gt;@Jason22&lt;/a&gt;&amp;nbsp;&lt;/P&gt;
&lt;P&gt;HSE-enabled devices do not have the ability to disable HSE_SWT due to security concerns. The internal team performed the self-test from the application core on an SoC with the HSE installed, and no abnormalities were observed.&lt;/P&gt;
&lt;P&gt;During the self-test, the HSE is servicing the watchdog, so no reset will be triggered by the HSE. Therefore, the application does not need to disable anything to perform the self-test, as the HSE handles it.&lt;/P&gt;
&lt;P&gt;We understand that the documentation may cause confusion, so a ticket has already been raised to verify this situation.&lt;/P&gt;
&lt;P&gt;&amp;nbsp;&lt;/P&gt;
&lt;P&gt;BR, VaneB&lt;/P&gt;</description>
      <pubDate>Tue, 18 Mar 2025 19:04:02 GMT</pubDate>
      <guid>https://community.nxp.com/t5/S32K/S32K344-BIST-HSE-SWT-reset/m-p/2064018#M46925</guid>
      <dc:creator>VaneB</dc:creator>
      <dc:date>2025-03-18T19:04:02Z</dc:date>
    </item>
  </channel>
</rss>