<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>topic S32k144 maintains normal operation of RTC in case of powerdown in S32K</title>
    <link>https://community.nxp.com/t5/S32K/S32k144-maintains-normal-operation-of-RTC-in-case-of-powerdown/m-p/2061974#M46784</link>
    <description>&lt;P&gt;I use S32K144 and now I have a requirement: when VDD loses power, the RTC clock should keep running normally and the power consumption should be less than 10ua. I have checked that there is no separate RTC power supply pin on the chip hardware. Can we only adopt the solution of using an external RTC clock chip?&lt;/P&gt;</description>
    <pubDate>Fri, 14 Mar 2025 09:30:04 GMT</pubDate>
    <dc:creator>kane123Hu</dc:creator>
    <dc:date>2025-03-14T09:30:04Z</dc:date>
    <item>
      <title>S32k144 maintains normal operation of RTC in case of powerdown</title>
      <link>https://community.nxp.com/t5/S32K/S32k144-maintains-normal-operation-of-RTC-in-case-of-powerdown/m-p/2061974#M46784</link>
      <description>&lt;P&gt;I use S32K144 and now I have a requirement: when VDD loses power, the RTC clock should keep running normally and the power consumption should be less than 10ua. I have checked that there is no separate RTC power supply pin on the chip hardware. Can we only adopt the solution of using an external RTC clock chip?&lt;/P&gt;</description>
      <pubDate>Fri, 14 Mar 2025 09:30:04 GMT</pubDate>
      <guid>https://community.nxp.com/t5/S32K/S32k144-maintains-normal-operation-of-RTC-in-case-of-powerdown/m-p/2061974#M46784</guid>
      <dc:creator>kane123Hu</dc:creator>
      <dc:date>2025-03-14T09:30:04Z</dc:date>
    </item>
    <item>
      <title>Re: S32k144 maintains normal operation of RTC in case of powerdown</title>
      <link>https://community.nxp.com/t5/S32K/S32k144-maintains-normal-operation-of-RTC-in-case-of-powerdown/m-p/2063905#M46917</link>
      <description>&lt;P&gt;Yes, it will be needed to use external RTC device.&lt;/P&gt;</description>
      <pubDate>Tue, 18 Mar 2025 15:09:20 GMT</pubDate>
      <guid>https://community.nxp.com/t5/S32K/S32k144-maintains-normal-operation-of-RTC-in-case-of-powerdown/m-p/2063905#M46917</guid>
      <dc:creator>davidtosenovjan</dc:creator>
      <dc:date>2025-03-18T15:09:20Z</dc:date>
    </item>
  </channel>
</rss>