<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>S32KのトピックRTD version for S32K3 microcontrollers that supports Fls component</title>
    <link>https://community.nxp.com/t5/S32K/RTD-version-for-S32K3-microcontrollers-that-supports-Fls/m-p/2061553#M46753</link>
    <description>&lt;P&gt;Hello,&lt;/P&gt;&lt;P&gt;What is the latest RTD version for K3 microcontrollers,&amp;nbsp;specifically S32K344, that has a Fls component?&lt;BR /&gt;I have a problem in source code with backward compatibility,&amp;nbsp;because Fls is now divided into two components.&lt;BR /&gt;&lt;BR /&gt;&lt;/P&gt;&lt;P&gt;I see that the Fls component is present in S32K3 Real-Time Drivers Version 3.0.0 P01 HotFix 02, and not in&amp;nbsp;S32K3_M27X Real-Time Drivers Version 3.0.0 P07&lt;/P&gt;&lt;P&gt;Q1:&amp;nbsp; &amp;nbsp;Are there any RTD driver versions between these two that have a Fls component ?&lt;/P&gt;&lt;P&gt;Q2:&amp;nbsp; &amp;nbsp;Which&amp;nbsp;FS26 SBC AUTOSAR drivers is compatible with&amp;nbsp;S32K3 Real-Time Drivers Version 3.0.0 P01 HotFix 02 ?&lt;/P&gt;</description>
    <pubDate>Thu, 13 Mar 2025 19:52:35 GMT</pubDate>
    <dc:creator>Djuric</dc:creator>
    <dc:date>2025-03-13T19:52:35Z</dc:date>
    <item>
      <title>RTD version for S32K3 microcontrollers that supports Fls component</title>
      <link>https://community.nxp.com/t5/S32K/RTD-version-for-S32K3-microcontrollers-that-supports-Fls/m-p/2061553#M46753</link>
      <description>&lt;P&gt;Hello,&lt;/P&gt;&lt;P&gt;What is the latest RTD version for K3 microcontrollers,&amp;nbsp;specifically S32K344, that has a Fls component?&lt;BR /&gt;I have a problem in source code with backward compatibility,&amp;nbsp;because Fls is now divided into two components.&lt;BR /&gt;&lt;BR /&gt;&lt;/P&gt;&lt;P&gt;I see that the Fls component is present in S32K3 Real-Time Drivers Version 3.0.0 P01 HotFix 02, and not in&amp;nbsp;S32K3_M27X Real-Time Drivers Version 3.0.0 P07&lt;/P&gt;&lt;P&gt;Q1:&amp;nbsp; &amp;nbsp;Are there any RTD driver versions between these two that have a Fls component ?&lt;/P&gt;&lt;P&gt;Q2:&amp;nbsp; &amp;nbsp;Which&amp;nbsp;FS26 SBC AUTOSAR drivers is compatible with&amp;nbsp;S32K3 Real-Time Drivers Version 3.0.0 P01 HotFix 02 ?&lt;/P&gt;</description>
      <pubDate>Thu, 13 Mar 2025 19:52:35 GMT</pubDate>
      <guid>https://community.nxp.com/t5/S32K/RTD-version-for-S32K3-microcontrollers-that-supports-Fls/m-p/2061553#M46753</guid>
      <dc:creator>Djuric</dc:creator>
      <dc:date>2025-03-13T19:52:35Z</dc:date>
    </item>
    <item>
      <title>Re: RTD version for S32K3 microcontrollers that supports Fls component</title>
      <link>https://community.nxp.com/t5/S32K/RTD-version-for-S32K3-microcontrollers-that-supports-Fls/m-p/2061593#M46756</link>
      <description>&lt;P&gt;Hi&amp;nbsp;&lt;a href="https://community.nxp.com/t5/user/viewprofilepage/user-id/232904"&gt;@Djuric&lt;/a&gt;&lt;/P&gt;
&lt;P&gt;In Autosar R21-11, the Fls Driver has been replaced by Mem_InFls/Mem_ExFls. RTD 3.0.0 P07 is ASR 4.7 (R21-11) compliant, while P01 is ASR 4.4. The latest RTD package which still contains the Fls component is&amp;nbsp;&lt;STRONG&gt;S32K3_S32M27x Real-Time Drivers AUTOSAR 4.4 Version 4.0.0 P24.&lt;/STRONG&gt;&lt;/P&gt;
&lt;P&gt;Q1. I'm guessing you mean between P01 and P07? Unfortunately, there is not.&lt;/P&gt;
&lt;P&gt;Q2. I'm not sure if there is a specific package, as the only ones I've seen only support&amp;nbsp;3.0.0 P07. Since I mainly support S32K3 devices, and not FS26 SBC, please enter another post (or a case) so an engineer from the analog team can support you instead.&lt;/P&gt;
&lt;P&gt;Best regards,&lt;BR /&gt;Julián&amp;nbsp;&amp;nbsp;&lt;/P&gt;</description>
      <pubDate>Thu, 13 Mar 2025 21:14:14 GMT</pubDate>
      <guid>https://community.nxp.com/t5/S32K/RTD-version-for-S32K3-microcontrollers-that-supports-Fls/m-p/2061593#M46756</guid>
      <dc:creator>Julián_AragónM</dc:creator>
      <dc:date>2025-03-13T21:14:14Z</dc:date>
    </item>
    <item>
      <title>Re: RTD version for S32K3 microcontrollers that supports Fls component</title>
      <link>https://community.nxp.com/t5/S32K/RTD-version-for-S32K3-microcontrollers-that-supports-Fls/m-p/2061617#M46758</link>
      <description>&lt;P&gt;Thank you for your answer.&lt;/P&gt;</description>
      <pubDate>Thu, 13 Mar 2025 22:22:04 GMT</pubDate>
      <guid>https://community.nxp.com/t5/S32K/RTD-version-for-S32K3-microcontrollers-that-supports-Fls/m-p/2061617#M46758</guid>
      <dc:creator>Djuric</dc:creator>
      <dc:date>2025-03-13T22:22:04Z</dc:date>
    </item>
  </channel>
</rss>