<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>S32KのトピックQuestions about receiving various CAN Msgs</title>
    <link>https://community.nxp.com/t5/S32K/Questions-about-receiving-various-CAN-Msgs/m-p/908198#M4666</link>
    <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hello&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;We are considering using multiple MAILBOXs to handle the received Multi CAN Msg.&lt;BR /&gt;However, the test result shows that MAILBOX (0,1) with maximum 2ea including Tx/Rx can be used and 'STATUS_CAN_BUFF_OUT_OF_RANGE' is generated when using more than this.&lt;BR /&gt;ex) &lt;BR /&gt;#define RX_BUFF_IDX 0U, #define TX_BUFF_IDX 1U - ok&lt;BR /&gt;#define RX_BUFF_IDX 0U, #define RX_BUFF_IDX_2 1U - ok&lt;BR /&gt;#define RX_BUFF_IDX 0U, #define RX_BUFF_IDX_2 1U, &lt;STRONG&gt;#define RX_BUFF_IDX_3 2U&lt;/STRONG&gt; - fail&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;How can I receive various CAN Msgs?&lt;BR /&gt;I was refer to example code of can_pal_s32k144&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Thanks&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
    <pubDate>Mon, 27 May 2019 05:08:04 GMT</pubDate>
    <dc:creator>jm_shin</dc:creator>
    <dc:date>2019-05-27T05:08:04Z</dc:date>
    <item>
      <title>Questions about receiving various CAN Msgs</title>
      <link>https://community.nxp.com/t5/S32K/Questions-about-receiving-various-CAN-Msgs/m-p/908198#M4666</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hello&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;We are considering using multiple MAILBOXs to handle the received Multi CAN Msg.&lt;BR /&gt;However, the test result shows that MAILBOX (0,1) with maximum 2ea including Tx/Rx can be used and 'STATUS_CAN_BUFF_OUT_OF_RANGE' is generated when using more than this.&lt;BR /&gt;ex) &lt;BR /&gt;#define RX_BUFF_IDX 0U, #define TX_BUFF_IDX 1U - ok&lt;BR /&gt;#define RX_BUFF_IDX 0U, #define RX_BUFF_IDX_2 1U - ok&lt;BR /&gt;#define RX_BUFF_IDX 0U, #define RX_BUFF_IDX_2 1U, &lt;STRONG&gt;#define RX_BUFF_IDX_3 2U&lt;/STRONG&gt; - fail&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;How can I receive various CAN Msgs?&lt;BR /&gt;I was refer to example code of can_pal_s32k144&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Thanks&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Mon, 27 May 2019 05:08:04 GMT</pubDate>
      <guid>https://community.nxp.com/t5/S32K/Questions-about-receiving-various-CAN-Msgs/m-p/908198#M4666</guid>
      <dc:creator>jm_shin</dc:creator>
      <dc:date>2019-05-27T05:08:04Z</dc:date>
    </item>
    <item>
      <title>Re: Questions about receiving various CAN Msgs</title>
      <link>https://community.nxp.com/t5/S32K/Questions-about-receiving-various-CAN-Msgs/m-p/908199#M4667</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hi,&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;see&amp;nbsp;&lt;A _jive_internal="true" href="https://community.nxp.com/thread/503840"&gt;https://community.nxp.com/thread/503840&lt;/A&gt;&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;BR, Petr&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Mon, 27 May 2019 11:41:09 GMT</pubDate>
      <guid>https://community.nxp.com/t5/S32K/Questions-about-receiving-various-CAN-Msgs/m-p/908199#M4667</guid>
      <dc:creator>PetrS</dc:creator>
      <dc:date>2019-05-27T11:41:09Z</dc:date>
    </item>
  </channel>
</rss>