<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>topic Re: Difference between different HSE subsystems in S32K</title>
    <link>https://community.nxp.com/t5/S32K/Difference-between-different-HSE-subsystems/m-p/2053822#M46336</link>
    <description>Hi &lt;a href="https://community.nxp.com/t5/user/viewprofilepage/user-id/201913"&gt;@VaneB&lt;/a&gt;&lt;BR /&gt;&lt;BR /&gt;thank you for your quick response.&lt;BR /&gt;Unfortunately, this only answers the first part of my question.&lt;BR /&gt;&lt;BR /&gt;However, I am also interested in whether there are functional differences or whether the functionality is identical. I don't expect a detailed answer here, but I think you are allowed to answer yes or no &lt;LI-EMOJI id="lia_slightly-smiling-face" title=":slightly_smiling_face:"&gt;&lt;/LI-EMOJI&gt;&lt;BR /&gt;&lt;BR /&gt;Since you also mentioned Base, Medium and High, can I assume that this refers to the security rating?&lt;BR /&gt;In other words, if I have a project with a high security level, then I can't use an S32K3XX, but have to use an S32G2, for example?&lt;BR /&gt;&lt;BR /&gt;Kind regards&lt;BR /&gt;joma</description>
    <pubDate>Fri, 28 Feb 2025 14:24:30 GMT</pubDate>
    <dc:creator>joma</dc:creator>
    <dc:date>2025-02-28T14:24:30Z</dc:date>
    <item>
      <title>Difference between different HSE subsystems</title>
      <link>https://community.nxp.com/t5/S32K/Difference-between-different-HSE-subsystems/m-p/2048257#M46090</link>
      <description>&lt;P&gt;Hello everyone,&lt;/P&gt;&lt;P&gt;I was wondering what the difference is between the HSE subsystems HSE_H, HSE_M and HSE_B?&lt;/P&gt;&lt;P&gt;Is the difference just in which board they run on, or are there functional differences as well?&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;Thank you!&lt;/P&gt;</description>
      <pubDate>Thu, 20 Feb 2025 14:18:52 GMT</pubDate>
      <guid>https://community.nxp.com/t5/S32K/Difference-between-different-HSE-subsystems/m-p/2048257#M46090</guid>
      <dc:creator>joma</dc:creator>
      <dc:date>2025-02-20T14:18:52Z</dc:date>
    </item>
    <item>
      <title>Re: Difference between different HSE subsystems</title>
      <link>https://community.nxp.com/t5/S32K/Difference-between-different-HSE-subsystems/m-p/2048485#M46099</link>
      <description>&lt;P&gt;Hi&amp;nbsp;&lt;a href="https://community.nxp.com/t5/user/viewprofilepage/user-id/245879"&gt;@joma&lt;/a&gt;&amp;nbsp;&lt;/P&gt;
&lt;P&gt;The HSE subsystem exists in three variants, depending on the device in which it integrates:&lt;/P&gt;
&lt;P&gt;- HSE_H (High) is available on Flash-less S32x product variants (such as S32G2, S32G3, S32ZE, and S32R45). &lt;BR /&gt;- HSE_M (Medium) is available on Flash-less S32x product variants (such as S32R41, SAF85XX, and SAF86XX). &lt;BR /&gt;- HSE_B (Base) is available in S32x product variants with embedded Flash (such as S32K3XX, S32M27X, and MWCT2XX3A).&lt;/P&gt;
&lt;P&gt;Unfortunately, due to security restrictions related to working with automotive components, I am unable to share further details. The HSE reference manuals are accessible only through secure files.&lt;/P&gt;
&lt;P&gt;If you have not previously accessed secure files, please follow the guide below to request safety documentation:&amp;nbsp;&lt;A href="https://www.nxp.com/webapp/Download?colCode=SAFETY-DOC-PROCESS" target="_blank" rel="noopener" shape="rect"&gt;How to request safety documentation: Support Information&lt;/A&gt;&lt;/P&gt;
&lt;P&gt;&amp;nbsp;&lt;/P&gt;
&lt;P&gt;BR, VaneB&lt;/P&gt;</description>
      <pubDate>Thu, 20 Feb 2025 18:53:25 GMT</pubDate>
      <guid>https://community.nxp.com/t5/S32K/Difference-between-different-HSE-subsystems/m-p/2048485#M46099</guid>
      <dc:creator>VaneB</dc:creator>
      <dc:date>2025-02-20T18:53:25Z</dc:date>
    </item>
    <item>
      <title>Re: Difference between different HSE subsystems</title>
      <link>https://community.nxp.com/t5/S32K/Difference-between-different-HSE-subsystems/m-p/2053822#M46336</link>
      <description>Hi &lt;a href="https://community.nxp.com/t5/user/viewprofilepage/user-id/201913"&gt;@VaneB&lt;/a&gt;&lt;BR /&gt;&lt;BR /&gt;thank you for your quick response.&lt;BR /&gt;Unfortunately, this only answers the first part of my question.&lt;BR /&gt;&lt;BR /&gt;However, I am also interested in whether there are functional differences or whether the functionality is identical. I don't expect a detailed answer here, but I think you are allowed to answer yes or no &lt;LI-EMOJI id="lia_slightly-smiling-face" title=":slightly_smiling_face:"&gt;&lt;/LI-EMOJI&gt;&lt;BR /&gt;&lt;BR /&gt;Since you also mentioned Base, Medium and High, can I assume that this refers to the security rating?&lt;BR /&gt;In other words, if I have a project with a high security level, then I can't use an S32K3XX, but have to use an S32G2, for example?&lt;BR /&gt;&lt;BR /&gt;Kind regards&lt;BR /&gt;joma</description>
      <pubDate>Fri, 28 Feb 2025 14:24:30 GMT</pubDate>
      <guid>https://community.nxp.com/t5/S32K/Difference-between-different-HSE-subsystems/m-p/2053822#M46336</guid>
      <dc:creator>joma</dc:creator>
      <dc:date>2025-02-28T14:24:30Z</dc:date>
    </item>
    <item>
      <title>Re: Difference between different HSE subsystems</title>
      <link>https://community.nxp.com/t5/S32K/Difference-between-different-HSE-subsystems/m-p/2054901#M46395</link>
      <description>&lt;P&gt;Hi&amp;nbsp;&lt;a href="https://community.nxp.com/t5/user/viewprofilepage/user-id/245879"&gt;@joma&lt;/a&gt;&amp;nbsp;&lt;/P&gt;
&lt;P&gt;The main differences between each version lie in the host system images required to operate on Flash-less devices or devices with embedded Flash. The HSE-H&amp;amp;M runs on a Cortex-M7 core, while the HSE-B runs on a Cortex-M0+ core.&lt;/P&gt;
&lt;P&gt;All versions provide the following services, divided into the following classes:&lt;/P&gt;
&lt;UL&gt;
&lt;LI&gt;Administration services: installation, configuration, and testing of the HSE.&lt;/LI&gt;
&lt;LI&gt;Key management services: management of different key sets handled by the HSE, for example, through cryptographic services.&lt;/LI&gt;
&lt;LI&gt;Cryptographic services: providing the application with cryptographic primitives used by high-level security stacks in the application.&lt;/LI&gt;
&lt;LI&gt;Random number services: generating random streams that can be used in various security protocols.&lt;/LI&gt;
&lt;LI&gt;Memory verification services: allowing the application to verify different memory areas during startup (after reset) and runtime.&lt;/LI&gt;
&lt;LI&gt;Monotonic counter services: providing the application with a set of monotonic counters that can only be read and incremented.&lt;/LI&gt;
&lt;/UL&gt;
&lt;P&gt;The difference between versions lies in the feature support.&lt;/P&gt;</description>
      <pubDate>Mon, 03 Mar 2025 18:15:30 GMT</pubDate>
      <guid>https://community.nxp.com/t5/S32K/Difference-between-different-HSE-subsystems/m-p/2054901#M46395</guid>
      <dc:creator>VaneB</dc:creator>
      <dc:date>2025-03-03T18:15:30Z</dc:date>
    </item>
  </channel>
</rss>