<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>S32KのトピックS32K118 BOOTLOADER</title>
    <link>https://community.nxp.com/t5/S32K/S32K118-BOOTLOADER/m-p/906436#M4627</link>
    <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hi,&lt;/P&gt;&lt;P&gt;I want to implement bootloader for s32k118 EVB. If I am flashing the code with debugger from any start address, after jumping to that address my application is running properly. But if I am writing same application hex file&amp;nbsp;using FTFC then after jumping it reset the controller.&lt;/P&gt;&lt;P&gt;I have tested Flash read, write and erase. It is working fine.&amp;nbsp;And I have disabled watchdog also. what is the issue I am not able to find?&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Please help with the required information.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Thanks and regards,&lt;/P&gt;&lt;P&gt;Ravi Ranjan Kumar.&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
    <pubDate>Fri, 24 May 2019 05:51:45 GMT</pubDate>
    <dc:creator>raviranjankumar</dc:creator>
    <dc:date>2019-05-24T05:51:45Z</dc:date>
    <item>
      <title>S32K118 BOOTLOADER</title>
      <link>https://community.nxp.com/t5/S32K/S32K118-BOOTLOADER/m-p/906436#M4627</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hi,&lt;/P&gt;&lt;P&gt;I want to implement bootloader for s32k118 EVB. If I am flashing the code with debugger from any start address, after jumping to that address my application is running properly. But if I am writing same application hex file&amp;nbsp;using FTFC then after jumping it reset the controller.&lt;/P&gt;&lt;P&gt;I have tested Flash read, write and erase. It is working fine.&amp;nbsp;And I have disabled watchdog also. what is the issue I am not able to find?&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Please help with the required information.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Thanks and regards,&lt;/P&gt;&lt;P&gt;Ravi Ranjan Kumar.&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Fri, 24 May 2019 05:51:45 GMT</pubDate>
      <guid>https://community.nxp.com/t5/S32K/S32K118-BOOTLOADER/m-p/906436#M4627</guid>
      <dc:creator>raviranjankumar</dc:creator>
      <dc:date>2019-05-24T05:51:45Z</dc:date>
    </item>
    <item>
      <title>Re: S32K118 BOOTLOADER</title>
      <link>https://community.nxp.com/t5/S32K/S32K118-BOOTLOADER/m-p/906437#M4628</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Can anybody help me with required information..?&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Fri, 31 May 2019 05:37:07 GMT</pubDate>
      <guid>https://community.nxp.com/t5/S32K/S32K118-BOOTLOADER/m-p/906437#M4628</guid>
      <dc:creator>raviranjankumar</dc:creator>
      <dc:date>2019-05-31T05:37:07Z</dc:date>
    </item>
    <item>
      <title>Re: S32K118 BOOTLOADER</title>
      <link>https://community.nxp.com/t5/S32K/S32K118-BOOTLOADER/m-p/906438#M4629</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hello Ravi Ranjan Kumar,&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Sorry for the late response. I recommend you checking the application note AN12218 (&lt;A href="https://www.nxp.com/docs/en/application-note/AN12218.pdf"&gt;link&lt;/A&gt;). This application note explains how to make a bootloader for the S32K. You can download the software from the following &lt;A href="https://www.nxp.com/docs/en/application-note-software/AN12218SW.zip"&gt;link&lt;/A&gt;.&lt;/P&gt;&lt;P&gt;&lt;BR /&gt;Have a great day,&lt;BR /&gt;TIC&lt;/P&gt;&lt;P&gt;-------------------------------------------------------------------------------&lt;BR /&gt;Note:&lt;BR /&gt;- If this post answers your question, please click the "Mark Correct" button. Thank you!&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;- We are following threads for 7 weeks after the last post, later replies are ignored&lt;BR /&gt; Please open a new thread and refer to the closed one, if you have a related question at a later point in time.&lt;BR /&gt;-------------------------------------------------------------------------------&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Fri, 31 May 2019 21:30:22 GMT</pubDate>
      <guid>https://community.nxp.com/t5/S32K/S32K118-BOOTLOADER/m-p/906438#M4629</guid>
      <dc:creator>victorjimenez</dc:creator>
      <dc:date>2019-05-31T21:30:22Z</dc:date>
    </item>
  </channel>
</rss>