<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>S32KのトピックRe: How can I configure SysTick timer interrupt priority ?</title>
    <link>https://community.nxp.com/t5/S32K/How-can-I-configure-SysTick-timer-interrupt-priority/m-p/2051288#M46244</link>
    <description>&lt;P&gt;Hello friends of the forum, I have a question or rather I do not understand how to define the priorities of the interruptions for the M0+ processor. More specifically I don't understand when the priorities are defined NVIC_SetPriority (SysTick_IRQn, (1UL &amp;lt;&amp;lt; __NVIC_PRIO_BITS) - 1UL);&lt;/P&gt;&lt;P&gt;referred to in (1UL &amp;lt;&amp;lt; __NVIC_PRIO_BITS). According to reviewing the documentation, __NVIC_PRIO_BIT has a value of 2. I do not understand why the displacement that is made, a value between 0-3 can be set instead of "(1UL &amp;lt;&amp;lt; __NVIC_PRIO_BITS)" Can someone clarify this doubt for me. Thank you so much.&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;Alvaro&lt;/P&gt;</description>
    <pubDate>Wed, 26 Feb 2025 03:25:58 GMT</pubDate>
    <dc:creator>ingtasco</dc:creator>
    <dc:date>2025-02-26T03:25:58Z</dc:date>
    <item>
      <title>How can I configure SysTick timer interrupt priority ?</title>
      <link>https://community.nxp.com/t5/S32K/How-can-I-configure-SysTick-timer-interrupt-priority/m-p/1586031#M20151</link>
      <description>&lt;P&gt;Hello NXP team.&lt;/P&gt;&lt;P&gt;I've tried to config SysTick interrupt without success.&lt;/P&gt;&lt;P&gt;&lt;STRONG&gt;&lt;FONT color="#FF0000"&gt;Question 1: &lt;/FONT&gt;&lt;/STRONG&gt;&lt;FONT color="#000000"&gt;How can I change the SysTick IRQ priority ?&lt;BR /&gt;&lt;/FONT&gt;&lt;/P&gt;&lt;P&gt;I've used the two methods mentioned bellow:&lt;/P&gt;&lt;P&gt;1.&amp;nbsp;&amp;nbsp; &lt;span class="lia-inline-image-display-wrapper lia-image-align-inline" image-alt="kyf_2-1674216968640.png"&gt;&lt;img src="https://community.nxp.com/t5/image/serverpage/image-id/208028iC0007EA9A09064C5/image-size/medium?v=v2&amp;amp;px=400" alt="kyf_2-1674216968640.png" title="kyf_2-1674216968640.png" /&gt;&lt;/span&gt;&lt;/P&gt;&lt;P&gt;2.&amp;nbsp;&amp;nbsp; &lt;span class="lia-inline-image-display-wrapper lia-image-align-inline" image-alt="kyf_3-1674216997264.png"&gt;&lt;img src="https://community.nxp.com/t5/image/serverpage/image-id/208029i158431A3051FF979/image-size/medium?v=v2&amp;amp;px=400" alt="kyf_3-1674216997264.png" title="kyf_3-1674216997264.png" /&gt;&lt;/span&gt;&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;Solution 2 ends in DevAsser due to the guard that exists in the RTD function.&lt;/P&gt;&lt;P&gt;&lt;span class="lia-inline-image-display-wrapper lia-image-align-inline" image-alt="kyf_5-1674217073007.png"&gt;&lt;img src="https://community.nxp.com/t5/image/serverpage/image-id/208031iCF5605ED02BEEF7D/image-size/medium?v=v2&amp;amp;px=400" alt="kyf_5-1674217073007.png" title="kyf_5-1674217073007.png" /&gt;&lt;/span&gt;&lt;/P&gt;&lt;P&gt;My main problem is that I can't find anywhere the correct IRQnumber of SysTic. Not even in the CortexM7 documentation. The IRQn of SysTick into the "S32K344_COMMON.h" has a negative number as an enum but this IRQn can't be used in order to change the SysTick IRQ priority.&lt;/P&gt;&lt;P&gt;&lt;span class="lia-inline-image-display-wrapper lia-image-align-inline" image-alt="kyf_7-1674218487513.png"&gt;&lt;img src="https://community.nxp.com/t5/image/serverpage/image-id/208039i68D0745513AFB87B/image-size/small?v=v2&amp;amp;px=200" alt="kyf_7-1674218487513.png" title="kyf_7-1674218487513.png" /&gt;&lt;/span&gt;&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;I've also seen into the 5.1.4 Core configuration section that the IRQ priority width configuration is 4 (This means that there is only 16 interrupt priority level).&lt;/P&gt;&lt;P&gt;&lt;STRONG&gt;&lt;FONT color="#FF0000"&gt;Question 2:&lt;/FONT&gt;&lt;/STRONG&gt; Can't I change the priority width configuration as I want ? Is this a fixed value or the 4 is the just the default number ??&lt;/P&gt;&lt;P&gt;&lt;span class="lia-inline-image-display-wrapper lia-image-align-inline" image-alt="kyf_6-1674218411904.png"&gt;&lt;img src="https://community.nxp.com/t5/image/serverpage/image-id/208038iC82F8C0797D3D7F8/image-size/medium?v=v2&amp;amp;px=400" alt="kyf_6-1674218411904.png" title="kyf_6-1674218411904.png" /&gt;&lt;/span&gt;&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;Kind regards,&lt;/P&gt;&lt;P&gt;kyf.&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;</description>
      <pubDate>Fri, 20 Jan 2023 12:47:00 GMT</pubDate>
      <guid>https://community.nxp.com/t5/S32K/How-can-I-configure-SysTick-timer-interrupt-priority/m-p/1586031#M20151</guid>
      <dc:creator>kyf</dc:creator>
      <dc:date>2023-01-20T12:47:00Z</dc:date>
    </item>
    <item>
      <title>Re: How can I configure SysTick timer interrupt priority ?</title>
      <link>https://community.nxp.com/t5/S32K/How-can-I-configure-SysTick-timer-interrupt-priority/m-p/1591277#M20346</link>
      <description>&lt;P&gt;Hi kyf,&lt;/P&gt;
&lt;P&gt;&lt;STRONG&gt;&lt;FONT color="#FF0000"&gt;Question 1:&lt;SPAN&gt;&amp;nbsp;&lt;/SPAN&gt;&lt;/FONT&gt;&lt;/STRONG&gt;&lt;FONT color="#000000"&gt;How can I change the SysTick IRQ priority ?&lt;/FONT&gt;&lt;/P&gt;
&lt;P&gt;&lt;FONT color="#000000"&gt;=&amp;gt; Because the Systick is a core interrupt. So, you can't use NVIC to change the priority of SysTick.&lt;/FONT&gt;&lt;/P&gt;
&lt;P&gt;&lt;FONT color="#000000"&gt;Unfortunately, The RTD driver didn't support functions to change the priority of core interrupts.&lt;/FONT&gt;&lt;/P&gt;
&lt;P&gt;&lt;FONT color="#000000"&gt;So, you must interact with the PRI_15 bit field in the &lt;SPAN class="fontstyle0"&gt;SHPR3 ( System Handler Priority Register 3)&lt;/SPAN&gt;&amp;nbsp;to change&amp;nbsp;the priority of SysTick.&lt;/FONT&gt;&lt;/P&gt;
&lt;P&gt;&lt;span class="lia-inline-image-display-wrapper lia-image-align-inline" image-alt="nxf78987_0-1675252420442.png" style="width: 400px;"&gt;&lt;img src="https://community.nxp.com/t5/image/serverpage/image-id/209124iC8A194CC37461CF2/image-size/medium?v=v2&amp;amp;px=400" role="button" title="nxf78987_0-1675252420442.png" alt="nxf78987_0-1675252420442.png" /&gt;&lt;span class="lia-inline-image-caption" onclick="event.preventDefault();"&gt;nxf78987_0-1675252420442.png&lt;/span&gt;&lt;/span&gt;&lt;/P&gt;
&lt;P&gt;&lt;STRONG&gt;&lt;FONT color="#FF0000"&gt;Question 2:&lt;/FONT&gt;&lt;/STRONG&gt;&lt;SPAN&gt;&amp;nbsp;Can't I change the priority width configuration as I want?&amp;nbsp;Is this a fixed value or the 4 is the just the default number ??&lt;/SPAN&gt;&lt;/P&gt;
&lt;P&gt;&lt;SPAN&gt;=&amp;gt; Yes, this a fixed value. Because&amp;nbsp;the priority width equal&amp;nbsp;width of the PRI_n bit field = 4 bits.&lt;/SPAN&gt;&lt;/P&gt;
&lt;P&gt;&lt;SPAN&gt;This meaning is the priority of interrupts can change from 0 to 15.&lt;/SPAN&gt;&lt;/P&gt;
&lt;P&gt;&lt;SPAN&gt;Best regards,&lt;/SPAN&gt;&lt;/P&gt;
&lt;P&gt;&lt;SPAN&gt;Dan&lt;/SPAN&gt;&lt;/P&gt;
&lt;P&gt;&amp;nbsp;&lt;/P&gt;
&lt;P&gt;&amp;nbsp;&lt;/P&gt;</description>
      <pubDate>Wed, 01 Feb 2023 12:00:59 GMT</pubDate>
      <guid>https://community.nxp.com/t5/S32K/How-can-I-configure-SysTick-timer-interrupt-priority/m-p/1591277#M20346</guid>
      <dc:creator>DanNguyenDuy</dc:creator>
      <dc:date>2023-02-01T12:00:59Z</dc:date>
    </item>
    <item>
      <title>Re: How can I configure SysTick timer interrupt priority ?</title>
      <link>https://community.nxp.com/t5/S32K/How-can-I-configure-SysTick-timer-interrupt-priority/m-p/1591295#M20347</link>
      <description>&lt;P&gt;Hello &lt;a href="https://community.nxp.com/t5/user/viewprofilepage/user-id/199019"&gt;@DanNguyenDuy&lt;/a&gt; ,&lt;/P&gt;&lt;P&gt;Thank you for your input. I've gone throught the RTD and I've seen that it does not include prigroup register handling and either the system exception priority handling. So I've added my self.&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;It's a pity though because those stuff are free and are provided from CMSIS drivers of ARM.&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;Kind regards,&lt;/P&gt;&lt;P&gt;kyf&lt;/P&gt;</description>
      <pubDate>Wed, 01 Feb 2023 12:27:32 GMT</pubDate>
      <guid>https://community.nxp.com/t5/S32K/How-can-I-configure-SysTick-timer-interrupt-priority/m-p/1591295#M20347</guid>
      <dc:creator>kyf</dc:creator>
      <dc:date>2023-02-01T12:27:32Z</dc:date>
    </item>
    <item>
      <title>Re: How can I configure SysTick timer interrupt priority ?</title>
      <link>https://community.nxp.com/t5/S32K/How-can-I-configure-SysTick-timer-interrupt-priority/m-p/2051288#M46244</link>
      <description>&lt;P&gt;Hello friends of the forum, I have a question or rather I do not understand how to define the priorities of the interruptions for the M0+ processor. More specifically I don't understand when the priorities are defined NVIC_SetPriority (SysTick_IRQn, (1UL &amp;lt;&amp;lt; __NVIC_PRIO_BITS) - 1UL);&lt;/P&gt;&lt;P&gt;referred to in (1UL &amp;lt;&amp;lt; __NVIC_PRIO_BITS). According to reviewing the documentation, __NVIC_PRIO_BIT has a value of 2. I do not understand why the displacement that is made, a value between 0-3 can be set instead of "(1UL &amp;lt;&amp;lt; __NVIC_PRIO_BITS)" Can someone clarify this doubt for me. Thank you so much.&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;Alvaro&lt;/P&gt;</description>
      <pubDate>Wed, 26 Feb 2025 03:25:58 GMT</pubDate>
      <guid>https://community.nxp.com/t5/S32K/How-can-I-configure-SysTick-timer-interrupt-priority/m-p/2051288#M46244</guid>
      <dc:creator>ingtasco</dc:creator>
      <dc:date>2025-02-26T03:25:58Z</dc:date>
    </item>
  </channel>
</rss>