<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>S32KのトピックRe: UART issue in K388</title>
    <link>https://community.nxp.com/t5/S32K/UART-issue-in-K388/m-p/2051126#M46238</link>
    <description>&lt;P&gt;Hi&amp;nbsp;&lt;a href="https://community.nxp.com/t5/user/viewprofilepage/user-id/247300"&gt;@nxg12018&lt;/a&gt;,&lt;/P&gt;
&lt;P&gt;I assume you are using "LpuartFlexio_Uart_Ip_Example_S32K388". If not, just confirm the pins are correctly configured and initialized. Also, check if the baud rate is correctly set between the MCU and the uart module as well.&lt;/P&gt;
&lt;P&gt;Best regards,&lt;BR /&gt;Julián&lt;/P&gt;</description>
    <pubDate>Tue, 25 Feb 2025 22:02:34 GMT</pubDate>
    <dc:creator>Julián_AragónM</dc:creator>
    <dc:date>2025-02-25T22:02:34Z</dc:date>
    <item>
      <title>UART issue in K388</title>
      <link>https://community.nxp.com/t5/S32K/UART-issue-in-K388/m-p/2050706#M46223</link>
      <description>&lt;P&gt;I am working on S32 Design Studio Version 3.5, using RTD version 5.0.0 for S32K388 board. My objective is to execute an example of UART provided by the mentioned RTD package, I am able to build this example project but when I try to debug the same using Trace32 I am not getting print messages in my Serial Terminal (I am using Tera Term for this purpose). The onboard UART does not work in S32K388, so I am using external connections for TX (PTA 3) and RX (PTA 2) pins which are connected to J695 pin set of the board. Looking for a solution to this issue&amp;nbsp;&lt;BR /&gt;Thanks in advance.&lt;/P&gt;
&lt;P&gt; &lt;/P&gt;
&lt;P&gt;&lt;span class="lia-inline-image-display-wrapper lia-image-align-inline" image-alt="Media.jpg" style="width: 400px;"&gt;&lt;img src="https://community.nxp.com/t5/image/serverpage/image-id/325522i43398E2F35A2C087/image-size/medium?v=v2&amp;amp;px=400" role="button" title="Media.jpg" alt="Media.jpg" /&gt;&lt;/span&gt;S32K388 BOARD&lt;/P&gt;
&lt;P&gt; &lt;/P&gt;
&lt;P&gt;&lt;span class="lia-inline-image-display-wrapper lia-image-align-inline" image-alt="Media (1).jpg" style="width: 400px;"&gt;&lt;img src="https://community.nxp.com/t5/image/serverpage/image-id/325523iE0A00C5B7B9C2515/image-size/medium?v=v2&amp;amp;px=400" role="button" title="Media (1).jpg" alt="Media (1).jpg" /&gt;&lt;/span&gt;UART MODULE USED&lt;/P&gt;
&lt;P&gt; &lt;/P&gt;</description>
      <pubDate>Tue, 25 Feb 2025 10:02:10 GMT</pubDate>
      <guid>https://community.nxp.com/t5/S32K/UART-issue-in-K388/m-p/2050706#M46223</guid>
      <dc:creator>nxg12018</dc:creator>
      <dc:date>2025-02-25T10:02:10Z</dc:date>
    </item>
    <item>
      <title>Re: UART issue in K388</title>
      <link>https://community.nxp.com/t5/S32K/UART-issue-in-K388/m-p/2051126#M46238</link>
      <description>&lt;P&gt;Hi&amp;nbsp;&lt;a href="https://community.nxp.com/t5/user/viewprofilepage/user-id/247300"&gt;@nxg12018&lt;/a&gt;,&lt;/P&gt;
&lt;P&gt;I assume you are using "LpuartFlexio_Uart_Ip_Example_S32K388". If not, just confirm the pins are correctly configured and initialized. Also, check if the baud rate is correctly set between the MCU and the uart module as well.&lt;/P&gt;
&lt;P&gt;Best regards,&lt;BR /&gt;Julián&lt;/P&gt;</description>
      <pubDate>Tue, 25 Feb 2025 22:02:34 GMT</pubDate>
      <guid>https://community.nxp.com/t5/S32K/UART-issue-in-K388/m-p/2051126#M46238</guid>
      <dc:creator>Julián_AragónM</dc:creator>
      <dc:date>2025-02-25T22:02:34Z</dc:date>
    </item>
  </channel>
</rss>