<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>S32K中的主题 software will get reset if HSE firmware installed</title>
    <link>https://community.nxp.com/t5/S32K/software-will-get-reset-if-HSE-firmware-installed/m-p/2048808#M46115</link>
    <description>&lt;P&gt;dear NXP expert:&lt;/P&gt;&lt;P&gt;I got a problem after installing HSE firmware.&lt;/P&gt;&lt;P&gt;I installed the HSE firmware by the project provided from FAE and the HSE seems be installed successfully by the information in&amp;nbsp;&lt;A href="https://community.nxp.com/t5/S32K/Access-HSE-service-by-MU-B-channel-0/m-p/2045320#M45957" target="_blank"&gt;Access HSE service by MU_B channel_0 - NXP Community&lt;/A&gt;&lt;/P&gt;&lt;P&gt;now I download the bootloader code (developed by our side) and the boot can runs only about 9 seconds and it will reset and I check the reset reason and it shows that HSE trigger the reset .if the boot runs in a hardware without HSE firmware installed, it will runs ok.&lt;/P&gt;&lt;P&gt;I download and debug the boot by PE and the S32DS would erase 0x1B000000 by default option.&lt;/P&gt;</description>
    <pubDate>Fri, 21 Feb 2025 06:21:49 GMT</pubDate>
    <dc:creator>yin_qiu</dc:creator>
    <dc:date>2025-02-21T06:21:49Z</dc:date>
    <item>
      <title>software will get reset if HSE firmware installed</title>
      <link>https://community.nxp.com/t5/S32K/software-will-get-reset-if-HSE-firmware-installed/m-p/2048808#M46115</link>
      <description>&lt;P&gt;dear NXP expert:&lt;/P&gt;&lt;P&gt;I got a problem after installing HSE firmware.&lt;/P&gt;&lt;P&gt;I installed the HSE firmware by the project provided from FAE and the HSE seems be installed successfully by the information in&amp;nbsp;&lt;A href="https://community.nxp.com/t5/S32K/Access-HSE-service-by-MU-B-channel-0/m-p/2045320#M45957" target="_blank"&gt;Access HSE service by MU_B channel_0 - NXP Community&lt;/A&gt;&lt;/P&gt;&lt;P&gt;now I download the bootloader code (developed by our side) and the boot can runs only about 9 seconds and it will reset and I check the reset reason and it shows that HSE trigger the reset .if the boot runs in a hardware without HSE firmware installed, it will runs ok.&lt;/P&gt;&lt;P&gt;I download and debug the boot by PE and the S32DS would erase 0x1B000000 by default option.&lt;/P&gt;</description>
      <pubDate>Fri, 21 Feb 2025 06:21:49 GMT</pubDate>
      <guid>https://community.nxp.com/t5/S32K/software-will-get-reset-if-HSE-firmware-installed/m-p/2048808#M46115</guid>
      <dc:creator>yin_qiu</dc:creator>
      <dc:date>2025-02-21T06:21:49Z</dc:date>
    </item>
    <item>
      <title>Re: software will get reset if HSE firmware installed</title>
      <link>https://community.nxp.com/t5/S32K/software-will-get-reset-if-HSE-firmware-installed/m-p/2048819#M46118</link>
      <description>&lt;P&gt;I checked the content in 0x1B000000 by PE and it shows it has been written which is not the 0xFF, the content in utest shows the HSE has been activated .&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;</description>
      <pubDate>Fri, 21 Feb 2025 06:31:44 GMT</pubDate>
      <guid>https://community.nxp.com/t5/S32K/software-will-get-reset-if-HSE-firmware-installed/m-p/2048819#M46118</guid>
      <dc:creator>yin_qiu</dc:creator>
      <dc:date>2025-02-21T06:31:44Z</dc:date>
    </item>
    <item>
      <title>Re: software will get reset if HSE firmware installed</title>
      <link>https://community.nxp.com/t5/S32K/software-will-get-reset-if-HSE-firmware-installed/m-p/2048929#M46135</link>
      <description>&lt;P&gt;hello :&lt;/P&gt;&lt;P&gt;I get the reminder from&amp;nbsp;&lt;A href="https://community.nxp.com/t5/S32K/%E8%A7%A6%E5%8F%91MCU-HSE-SWT-RST-RESET%E5%A4%8D%E4%BD%8D/m-p/1761816" target="_blank"&gt;触发MCU HSE SWT RST RESET复位 - NXP Community&lt;/A&gt;&lt;/P&gt;&lt;P&gt;and I change the clock of HSE , the boot will not trigger reset&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;</description>
      <pubDate>Fri, 21 Feb 2025 08:58:26 GMT</pubDate>
      <guid>https://community.nxp.com/t5/S32K/software-will-get-reset-if-HSE-firmware-installed/m-p/2048929#M46135</guid>
      <dc:creator>yin_qiu</dc:creator>
      <dc:date>2025-02-21T08:58:26Z</dc:date>
    </item>
    <item>
      <title>Re: software will get reset if HSE firmware installed</title>
      <link>https://community.nxp.com/t5/S32K/software-will-get-reset-if-HSE-firmware-installed/m-p/2050216#M46201</link>
      <description>&lt;P&gt;Hi&amp;nbsp;&lt;a href="https://community.nxp.com/t5/user/viewprofilepage/user-id/239863"&gt;@yin_qiu&lt;/a&gt;&amp;nbsp;&lt;/P&gt;
&lt;P&gt;The HSE SWT RST issue is typically caused by an incorrect clock configuration. For further assistance, please refer to the following post: &lt;A href="https://community.nxp.com/t5/S32K/HSE-provides-RSP-NOT-SUPPORTED-response/m-p/1712323/highlight/true#M26508" target="_blank" rel="noopener"&gt;HSE provides RSP_NOT_SUPPORTED response&lt;/A&gt;. It contains valuable information that should help resolve the problem.&lt;/P&gt;
&lt;P&gt;&amp;nbsp;&lt;/P&gt;
&lt;P&gt;BR. VaneB&lt;/P&gt;</description>
      <pubDate>Mon, 24 Feb 2025 20:30:18 GMT</pubDate>
      <guid>https://community.nxp.com/t5/S32K/software-will-get-reset-if-HSE-firmware-installed/m-p/2050216#M46201</guid>
      <dc:creator>VaneB</dc:creator>
      <dc:date>2025-02-24T20:30:18Z</dc:date>
    </item>
  </channel>
</rss>