<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>topic XRDC clock enable in S32K</title>
    <link>https://community.nxp.com/t5/S32K/XRDC-clock-enable/m-p/2048201#M46088</link>
    <description>&lt;P&gt;Hello,&lt;BR /&gt;&lt;BR /&gt;I'm using EB tresos with&amp;nbsp;&lt;SPAN&gt;RTD 4.0.0 P20 D2403.&lt;/SPAN&gt;&lt;/P&gt;&lt;P&gt;I don't find in&amp;nbsp; MCU =&amp;gt; McuModeSettingConf=&amp;gt;McuPeripheral&amp;nbsp;PRTN1_COFB0_CLKEN[REQ30] to enable the clock for the module ?&lt;/P&gt;&lt;P&gt;How can I enable the clock for XRDC ?&lt;/P&gt;&lt;P&gt;In the code when i call RM_init() I have got a hard fault in&amp;nbsp;Xrdc_Ip_Init_Privileged()&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;Sophie&lt;/P&gt;</description>
    <pubDate>Thu, 20 Feb 2025 12:45:19 GMT</pubDate>
    <dc:creator>sobo</dc:creator>
    <dc:date>2025-02-20T12:45:19Z</dc:date>
    <item>
      <title>XRDC clock enable</title>
      <link>https://community.nxp.com/t5/S32K/XRDC-clock-enable/m-p/2048201#M46088</link>
      <description>&lt;P&gt;Hello,&lt;BR /&gt;&lt;BR /&gt;I'm using EB tresos with&amp;nbsp;&lt;SPAN&gt;RTD 4.0.0 P20 D2403.&lt;/SPAN&gt;&lt;/P&gt;&lt;P&gt;I don't find in&amp;nbsp; MCU =&amp;gt; McuModeSettingConf=&amp;gt;McuPeripheral&amp;nbsp;PRTN1_COFB0_CLKEN[REQ30] to enable the clock for the module ?&lt;/P&gt;&lt;P&gt;How can I enable the clock for XRDC ?&lt;/P&gt;&lt;P&gt;In the code when i call RM_init() I have got a hard fault in&amp;nbsp;Xrdc_Ip_Init_Privileged()&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;Sophie&lt;/P&gt;</description>
      <pubDate>Thu, 20 Feb 2025 12:45:19 GMT</pubDate>
      <guid>https://community.nxp.com/t5/S32K/XRDC-clock-enable/m-p/2048201#M46088</guid>
      <dc:creator>sobo</dc:creator>
      <dc:date>2025-02-20T12:45:19Z</dc:date>
    </item>
    <item>
      <title>Re: XRDC clock enable</title>
      <link>https://community.nxp.com/t5/S32K/XRDC-clock-enable/m-p/2048896#M46131</link>
      <description>&lt;P&gt;Which specific MCU derivative is the question related to?&lt;/P&gt;</description>
      <pubDate>Fri, 21 Feb 2025 08:12:21 GMT</pubDate>
      <guid>https://community.nxp.com/t5/S32K/XRDC-clock-enable/m-p/2048896#M46131</guid>
      <dc:creator>davidtosenovjan</dc:creator>
      <dc:date>2025-02-21T08:12:21Z</dc:date>
    </item>
    <item>
      <title>Re: XRDC clock enable</title>
      <link>https://community.nxp.com/t5/S32K/XRDC-clock-enable/m-p/2048899#M46132</link>
      <description>&lt;P&gt;It's on a S32K358.&lt;/P&gt;&lt;P&gt;after further tests, it's seems that it's because i don't configure XRDC memory domain correctly.&lt;BR /&gt;&lt;BR /&gt;I only want to use SEMA42, and it's quite annoying because it's seems i must use XRDC that for now i don"t need.&lt;BR /&gt;There is another way to implement "spinlock" / atomic instruction on S32K358 ?&lt;BR /&gt;&lt;BR /&gt;&lt;/P&gt;</description>
      <pubDate>Fri, 21 Feb 2025 08:18:30 GMT</pubDate>
      <guid>https://community.nxp.com/t5/S32K/XRDC-clock-enable/m-p/2048899#M46132</guid>
      <dc:creator>sobo</dc:creator>
      <dc:date>2025-02-21T08:18:30Z</dc:date>
    </item>
    <item>
      <title>Re: XRDC clock enable</title>
      <link>https://community.nxp.com/t5/S32K/XRDC-clock-enable/m-p/2048993#M46138</link>
      <description>&lt;DIV id="tinyMceEditordavidtosenovjan_0" class="mceNonEditable lia-copypaste-placeholder"&gt;&amp;nbsp;&lt;/DIV&gt;
&lt;P&gt;No, it cannot be used separately. Trying to disable XRDC, having enabled SEMA42 lead in error.&lt;/P&gt;
&lt;P&gt;&lt;span class="lia-inline-image-display-wrapper lia-image-align-inline" image-alt="image.png" style="width: 969px;"&gt;&lt;img src="https://community.nxp.com/t5/image/serverpage/image-id/325143i420C18D52BB76524/image-size/large?v=v2&amp;amp;px=999" role="button" title="image.png" alt="image.png" /&gt;&lt;span class="lia-inline-image-caption" onclick="event.preventDefault();"&gt;image.png&lt;/span&gt;&lt;/span&gt;&lt;/P&gt;</description>
      <pubDate>Fri, 21 Feb 2025 09:59:53 GMT</pubDate>
      <guid>https://community.nxp.com/t5/S32K/XRDC-clock-enable/m-p/2048993#M46138</guid>
      <dc:creator>davidtosenovjan</dc:creator>
      <dc:date>2025-02-21T09:59:53Z</dc:date>
    </item>
  </channel>
</rss>