<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>topic When using Flash to emulate EEPROM, the data is only written to FlexRAM and not to FlexNVM in S32K</title>
    <link>https://community.nxp.com/t5/S32K/When-using-Flash-to-emulate-EEPROM-the-data-is-only-written-to/m-p/2046872#M46025</link>
    <description>&lt;DIV class=""&gt;When using the Flash EEPROM emulation feature of the S32K146 chip, I configured 32KB of FlexNVM as EEPROM Backup and 2KB of FlexRAM as EEPROM. During emulation, upon checking the memory, I found that the written data only resides in FlexRAM and has not been written to FlexNVM.&lt;/DIV&gt;&lt;DIV class=""&gt;I am unsure of the reason behind this and would appreciate any assistance.&lt;/DIV&gt;</description>
    <pubDate>Wed, 19 Feb 2025 03:44:45 GMT</pubDate>
    <dc:creator>813270556</dc:creator>
    <dc:date>2025-02-19T03:44:45Z</dc:date>
    <item>
      <title>When using Flash to emulate EEPROM, the data is only written to FlexRAM and not to FlexNVM</title>
      <link>https://community.nxp.com/t5/S32K/When-using-Flash-to-emulate-EEPROM-the-data-is-only-written-to/m-p/2046872#M46025</link>
      <description>&lt;DIV class=""&gt;When using the Flash EEPROM emulation feature of the S32K146 chip, I configured 32KB of FlexNVM as EEPROM Backup and 2KB of FlexRAM as EEPROM. During emulation, upon checking the memory, I found that the written data only resides in FlexRAM and has not been written to FlexNVM.&lt;/DIV&gt;&lt;DIV class=""&gt;I am unsure of the reason behind this and would appreciate any assistance.&lt;/DIV&gt;</description>
      <pubDate>Wed, 19 Feb 2025 03:44:45 GMT</pubDate>
      <guid>https://community.nxp.com/t5/S32K/When-using-Flash-to-emulate-EEPROM-the-data-is-only-written-to/m-p/2046872#M46025</guid>
      <dc:creator>813270556</dc:creator>
      <dc:date>2025-02-19T03:44:45Z</dc:date>
    </item>
    <item>
      <title>Re: When using Flash to emulate EEPROM, the data is only written to FlexRAM and not to FlexNVM</title>
      <link>https://community.nxp.com/t5/S32K/When-using-Flash-to-emulate-EEPROM-the-data-is-only-written-to/m-p/2046926#M46026</link>
      <description>&lt;P&gt;Hi@&lt;SPAN&gt;813270556&lt;/SPAN&gt;&lt;/P&gt;
&lt;SECTION&gt;After successfully executing the EEE partition command,the FlexNVM area (EEE_Flash) used as EEE backup is not visible to the CPU, and user code cannot directly access (read and write) this address mapping area, otherwise a bus error will occur and enter the kernel HardFault exception (default configuration) or BusFault exception (after using BusFault exception).&lt;/SECTION&gt;
&lt;SECTION&gt;&lt;/SECTION&gt;
&lt;SECTION&gt;At the same time, in the Memory window of the debug interface, the EEE_Flash area is displayed as an unknown state (???).&lt;/SECTION&gt;
&lt;SECTION&gt;&lt;/SECTION&gt;
&lt;SECTION&gt;&lt;A href="https://mp.weixin.qq.com/s?__biz=MzI0MDk0ODcxMw==&amp;amp;mid=2247486584&amp;amp;idx=1&amp;amp;sn=3b8651b928edd19c642b17838a8c75bd&amp;amp;chksm=e91248fede65c1e87214ce913baab45431f816d0bfd0362e00aea1ed4232f200d5ae2720cd71&amp;amp;scene=21#wechat_redirect" target="_blank"&gt;https://mp.weixin.qq.com/s?__biz=MzI0MDk0ODcxMw==&amp;amp;mid=2247486584&amp;amp;idx=1&amp;amp;sn=3b8651b928edd19c642b17838a8c75bd&amp;amp;chksm=e91248fede65c1e87214ce913baab45431f816d0bfd0362e00aea1ed4232f200d5ae2720cd71&amp;amp;scene=21#wechat_redirect&lt;/A&gt;&lt;/SECTION&gt;
&lt;SECTION&gt;&lt;/SECTION&gt;</description>
      <pubDate>Wed, 19 Feb 2025 05:31:11 GMT</pubDate>
      <guid>https://community.nxp.com/t5/S32K/When-using-Flash-to-emulate-EEPROM-the-data-is-only-written-to/m-p/2046926#M46026</guid>
      <dc:creator>Senlent</dc:creator>
      <dc:date>2025-02-19T05:31:11Z</dc:date>
    </item>
    <item>
      <title>Re: When using Flash to emulate EEPROM, the data is only written to FlexRAM and not to FlexNVM</title>
      <link>https://community.nxp.com/t5/S32K/When-using-Flash-to-emulate-EEPROM-the-data-is-only-written-to/m-p/2046992#M46030</link>
      <description>How can I prove that the data I have written has been backed up to FlexNVM?</description>
      <pubDate>Wed, 19 Feb 2025 06:30:13 GMT</pubDate>
      <guid>https://community.nxp.com/t5/S32K/When-using-Flash-to-emulate-EEPROM-the-data-is-only-written-to/m-p/2046992#M46030</guid>
      <dc:creator>813270556</dc:creator>
      <dc:date>2025-02-19T06:30:13Z</dc:date>
    </item>
    <item>
      <title>Re: When using Flash to emulate EEPROM, the data is only written to FlexRAM and not to FlexNVM</title>
      <link>https://community.nxp.com/t5/S32K/When-using-Flash-to-emulate-EEPROM-the-data-is-only-written-to/m-p/2047032#M46031</link>
      <description>&lt;P&gt;Hi@&lt;SPAN&gt;813270556&lt;/SPAN&gt;&lt;/P&gt;
&lt;P&gt;After the MCU is powered off and restarted, FlexNVM can synchronize the backed-up data to the FlexRAM area. You can use this principle to confirm whether your last backup was successful.&lt;/P&gt;</description>
      <pubDate>Wed, 19 Feb 2025 07:25:18 GMT</pubDate>
      <guid>https://community.nxp.com/t5/S32K/When-using-Flash-to-emulate-EEPROM-the-data-is-only-written-to/m-p/2047032#M46031</guid>
      <dc:creator>Senlent</dc:creator>
      <dc:date>2025-02-19T07:25:18Z</dc:date>
    </item>
    <item>
      <title>Re: When using Flash to emulate EEPROM, the data is only written to FlexRAM and not to FlexNVM</title>
      <link>https://community.nxp.com/t5/S32K/When-using-Flash-to-emulate-EEPROM-the-data-is-only-written-to/m-p/2047055#M46033</link>
      <description>&lt;P&gt;&lt;a href="https://community.nxp.com/t5/user/viewprofilepage/user-id/188029"&gt;@Senlent&lt;/a&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;&lt;SPAN&gt;FlexRAM is used as EEPROM (with a size of 4KB), and FlexNVM is used as EEPROM Backup (with a size of 32KB).&amp;nbsp;The chip I am using is S32K146.&lt;/SPAN&gt;&lt;/P&gt;&lt;P&gt;&lt;SPAN&gt;When I write data, can the size of the written data exceed 4KB? &lt;/SPAN&gt;&lt;/P&gt;&lt;P&gt;&lt;SPAN&gt;If so, how can the data exceeding 4KB be read from FlexNVM?&lt;/SPAN&gt;&lt;/P&gt;</description>
      <pubDate>Wed, 19 Feb 2025 07:43:24 GMT</pubDate>
      <guid>https://community.nxp.com/t5/S32K/When-using-Flash-to-emulate-EEPROM-the-data-is-only-written-to/m-p/2047055#M46033</guid>
      <dc:creator>813270556</dc:creator>
      <dc:date>2025-02-19T07:43:24Z</dc:date>
    </item>
    <item>
      <title>Re: When using Flash to emulate EEPROM, the data is only written to FlexRAM and not to FlexNVM</title>
      <link>https://community.nxp.com/t5/S32K/When-using-Flash-to-emulate-EEPROM-the-data-is-only-written-to/m-p/2047108#M46038</link>
      <description>&lt;P&gt;Hi@&lt;SPAN&gt;813270556&lt;/SPAN&gt;&lt;/P&gt;
&lt;P&gt;This is not feasible&lt;/P&gt;</description>
      <pubDate>Wed, 19 Feb 2025 08:33:10 GMT</pubDate>
      <guid>https://community.nxp.com/t5/S32K/When-using-Flash-to-emulate-EEPROM-the-data-is-only-written-to/m-p/2047108#M46038</guid>
      <dc:creator>Senlent</dc:creator>
      <dc:date>2025-02-19T08:33:10Z</dc:date>
    </item>
  </channel>
</rss>