<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>S32KのトピックCryptoLib</title>
    <link>https://community.nxp.com/t5/S32K/CryptoLib/m-p/2045484#M45964</link>
    <description>&lt;P&gt;Hello Support Team,&lt;BR /&gt;&lt;BR /&gt;i wanted to use the crypto hardware (Cryptolib) of the S32K146, especially the SHA256()-Function for a better performance. For this i have to include :&amp;nbsp; &lt;SPAN class=""&gt;"fsl_crypto.h"&lt;/SPAN&gt;&lt;/P&gt;&lt;P&gt;Where can i find this header-file for downloading on the NXP page (this header wasnt included with the other Csec files).&lt;BR /&gt;&lt;BR /&gt;Also, do i require additional headers to use the SHA256()-function ?&lt;BR /&gt;&lt;BR /&gt;Thanks.&lt;/P&gt;</description>
    <pubDate>Mon, 17 Feb 2025 12:39:00 GMT</pubDate>
    <dc:creator>tz9</dc:creator>
    <dc:date>2025-02-17T12:39:00Z</dc:date>
    <item>
      <title>CryptoLib</title>
      <link>https://community.nxp.com/t5/S32K/CryptoLib/m-p/2045484#M45964</link>
      <description>&lt;P&gt;Hello Support Team,&lt;BR /&gt;&lt;BR /&gt;i wanted to use the crypto hardware (Cryptolib) of the S32K146, especially the SHA256()-Function for a better performance. For this i have to include :&amp;nbsp; &lt;SPAN class=""&gt;"fsl_crypto.h"&lt;/SPAN&gt;&lt;/P&gt;&lt;P&gt;Where can i find this header-file for downloading on the NXP page (this header wasnt included with the other Csec files).&lt;BR /&gt;&lt;BR /&gt;Also, do i require additional headers to use the SHA256()-function ?&lt;BR /&gt;&lt;BR /&gt;Thanks.&lt;/P&gt;</description>
      <pubDate>Mon, 17 Feb 2025 12:39:00 GMT</pubDate>
      <guid>https://community.nxp.com/t5/S32K/CryptoLib/m-p/2045484#M45964</guid>
      <dc:creator>tz9</dc:creator>
      <dc:date>2025-02-17T12:39:00Z</dc:date>
    </item>
    <item>
      <title>Re: CryptoLib</title>
      <link>https://community.nxp.com/t5/S32K/CryptoLib/m-p/2046552#M46006</link>
      <description>&lt;P&gt;Hi &lt;a href="https://community.nxp.com/t5/user/viewprofilepage/user-id/184895"&gt;@tz9&lt;/a&gt;&amp;nbsp;,&lt;/P&gt;
&lt;P&gt;S32K1xx devices does not have an engine to support SHA256, but you can refer the following community thread: &lt;A href="https://community.nxp.com/t5/S32K/How-to-support-SHA256-in-S32K1-with-CSEc/td-p/1193810" target="_blank" rel="noopener"&gt;Solved: How to support SHA256 in S32K1 with CSEc? - NXP Community&lt;/A&gt;, where you can find a library to be able to implement SHA256 via software.&lt;/P&gt;
&lt;P&gt;BR,&lt;BR /&gt;IsaulO.&lt;/P&gt;</description>
      <pubDate>Tue, 18 Feb 2025 17:48:41 GMT</pubDate>
      <guid>https://community.nxp.com/t5/S32K/CryptoLib/m-p/2046552#M46006</guid>
      <dc:creator>IsaulO</dc:creator>
      <dc:date>2025-02-18T17:48:41Z</dc:date>
    </item>
  </channel>
</rss>