<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>topic Re: S32K312 ADC List using DMA and SW trigger in S32K</title>
    <link>https://community.nxp.com/t5/S32K/S32K312-ADC-List-using-DMA-and-SW-trigger/m-p/2045271#M45952</link>
    <description>&lt;P&gt;Hi,&lt;/P&gt;
&lt;P&gt;maybe you can refer to this one&lt;BR /&gt;&lt;A href="https://community.nxp.com/t5/S32K-Knowledge-Base/Example-S32K344-PIT-BTCU-parallel-ADC-FIFO-DMA-DS3-5-RTD300/ta-p/1732444" target="_blank"&gt;https://community.nxp.com/t5/S32K-Knowledge-Base/Example-S32K344-PIT-BTCU-parallel-ADC-FIFO-DMA-DS3-5-RTD300/ta-p/1732444&lt;/A&gt;&lt;/P&gt;
&lt;P&gt;BR, Petr&lt;/P&gt;</description>
    <pubDate>Mon, 17 Feb 2025 08:23:51 GMT</pubDate>
    <dc:creator>PetrS</dc:creator>
    <dc:date>2025-02-17T08:23:51Z</dc:date>
    <item>
      <title>S32K312 ADC List using DMA and SW trigger</title>
      <link>https://community.nxp.com/t5/S32K/S32K312-ADC-List-using-DMA-and-SW-trigger/m-p/2045086#M45944</link>
      <description>&lt;P&gt;Hi, I was trying to modify this example "&lt;A href="https://community.nxp.com/t5/S32K-Knowledge-Base/Example-S32K312-ADC-DS3-5-RTD300/ta-p/1789282" target="_blank"&gt;Example S32K312 ADC DS3.5 RTD300 - NXP Community&lt;/A&gt;" in order to use DMA and allow to read all converted channels at once using sw trigger. The example has been successfully upgrade to use sdk5 but I need some instruction about how to enable dma and trigger the list to convert.&amp;nbsp;&lt;/P&gt;&lt;P&gt;really appreciate if someone can guide me through the change or what need to be included/changed. Other examples use DMA and Bctu + HW trigger which I do not think I need in my case but I may be wrong.&amp;nbsp;&lt;/P&gt;&lt;P&gt;regards,&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;</description>
      <pubDate>Mon, 17 Feb 2025 03:54:30 GMT</pubDate>
      <guid>https://community.nxp.com/t5/S32K/S32K312-ADC-List-using-DMA-and-SW-trigger/m-p/2045086#M45944</guid>
      <dc:creator>PaoloRB</dc:creator>
      <dc:date>2025-02-17T03:54:30Z</dc:date>
    </item>
    <item>
      <title>Re: S32K312 ADC List using DMA and SW trigger</title>
      <link>https://community.nxp.com/t5/S32K/S32K312-ADC-List-using-DMA-and-SW-trigger/m-p/2045271#M45952</link>
      <description>&lt;P&gt;Hi,&lt;/P&gt;
&lt;P&gt;maybe you can refer to this one&lt;BR /&gt;&lt;A href="https://community.nxp.com/t5/S32K-Knowledge-Base/Example-S32K344-PIT-BTCU-parallel-ADC-FIFO-DMA-DS3-5-RTD300/ta-p/1732444" target="_blank"&gt;https://community.nxp.com/t5/S32K-Knowledge-Base/Example-S32K344-PIT-BTCU-parallel-ADC-FIFO-DMA-DS3-5-RTD300/ta-p/1732444&lt;/A&gt;&lt;/P&gt;
&lt;P&gt;BR, Petr&lt;/P&gt;</description>
      <pubDate>Mon, 17 Feb 2025 08:23:51 GMT</pubDate>
      <guid>https://community.nxp.com/t5/S32K/S32K312-ADC-List-using-DMA-and-SW-trigger/m-p/2045271#M45952</guid>
      <dc:creator>PetrS</dc:creator>
      <dc:date>2025-02-17T08:23:51Z</dc:date>
    </item>
  </channel>
</rss>