<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>S32KのトピックRe: Example usage CMU_FM_1 (without using MCAL)</title>
    <link>https://community.nxp.com/t5/S32K/Example-usage-CMU-FM-1-without-using-MCAL/m-p/2042688#M45846</link>
    <description>I tried to enable CMU_FM_1 to monitor the FIRC_CLK frequency and enable the interrupt FMCIE from IER register to be fired after the measurement is completed by these steps:&lt;BR /&gt;&lt;BR /&gt;IP_CMU_1-&amp;gt;RCCR = CMU_FM_RCCR_REF_CNT(50);&lt;BR /&gt;IP_CMU_1-&amp;gt;IER |= CMU_FM_IER_FMCIE_MASK;&lt;BR /&gt;IP_CMU_1-&amp;gt;GCR |= CMU_FM_GCR_FME_MASK;&lt;BR /&gt;&lt;BR /&gt;But I faced the following behavior that the interrupt was not fired after the completed window and went to power on reset.&lt;BR /&gt;&lt;BR /&gt;Did you face this behavior or something similar like this?&lt;BR /&gt;</description>
    <pubDate>Wed, 12 Feb 2025 15:04:31 GMT</pubDate>
    <dc:creator>narimanelashkar</dc:creator>
    <dc:date>2025-02-12T15:04:31Z</dc:date>
    <item>
      <title>Example usage CMU_FM_1 (without using MCAL)</title>
      <link>https://community.nxp.com/t5/S32K/Example-usage-CMU-FM-1-without-using-MCAL/m-p/2023968#M44908</link>
      <description>&lt;P&gt;I would like to enable CMU_FM_1 to monitor the FIRC_CLK frequency, but have a hard time.&lt;/P&gt;&lt;P&gt;Could someone point me to a tutorial or a step by step method to enable the meter? Ideally using RTD 3.0.0 function calls, but direct register accesses may be done as well.&lt;/P&gt;</description>
      <pubDate>Wed, 08 Jan 2025 10:00:07 GMT</pubDate>
      <guid>https://community.nxp.com/t5/S32K/Example-usage-CMU-FM-1-without-using-MCAL/m-p/2023968#M44908</guid>
      <dc:creator>abemat</dc:creator>
      <dc:date>2025-01-08T10:00:07Z</dc:date>
    </item>
    <item>
      <title>Re: Example usage CMU_FM_1 (without using MCAL)</title>
      <link>https://community.nxp.com/t5/S32K/Example-usage-CMU-FM-1-without-using-MCAL/m-p/2024841#M44968</link>
      <description>&lt;P&gt;Hello &lt;a href="https://community.nxp.com/t5/user/viewprofilepage/user-id/197500"&gt;@abemat&lt;/a&gt;,&lt;/P&gt;
&lt;P&gt;The full version of SAF has API for CMU_FM.&lt;/P&gt;
&lt;P&gt;&lt;A href="https://www.nxp.com/design/design-center/software/functional-safety-software/s32-safety-software-framework-saf-and-safety-peripheral-drivers-spd:SAF" target="_blank"&gt;https://www.nxp.com/design/design-center/software/functional-safety-software/s32-safety-software-framework-saf-and-safety-peripheral-drivers-spd:SAF&lt;/A&gt;&lt;/P&gt;
&lt;P&gt;&amp;nbsp;&lt;/P&gt;
&lt;P&gt;sCheck/srs/sCheck_CmuFmTest.c&lt;/P&gt;
&lt;P&gt;&lt;span class="lia-inline-image-display-wrapper lia-image-align-inline" image-alt="danielmartynek_0-1736425611448.png" style="width: 400px;"&gt;&lt;img src="https://community.nxp.com/t5/image/serverpage/image-id/318810iDD968F200DE27A4C/image-size/medium?v=v2&amp;amp;px=400" role="button" title="danielmartynek_0-1736425611448.png" alt="danielmartynek_0-1736425611448.png" /&gt;&lt;span class="lia-inline-image-caption" onclick="event.preventDefault();"&gt;danielmartynek_0-1736425611448.png&lt;/span&gt;&lt;/span&gt;&lt;/P&gt;
&lt;P&gt;&amp;nbsp;&lt;/P&gt;
&lt;P&gt;It is not present in the evaluation version.&lt;/P&gt;
&lt;P&gt;&amp;nbsp;&lt;/P&gt;
&lt;P&gt;We have also some non-RTD baremetal code that I can share with you privately.&lt;/P&gt;
&lt;P&gt;&amp;nbsp;&lt;/P&gt;
&lt;P&gt;Regards,&lt;/P&gt;
&lt;P&gt;Daniel&lt;/P&gt;</description>
      <pubDate>Thu, 09 Jan 2025 12:28:50 GMT</pubDate>
      <guid>https://community.nxp.com/t5/S32K/Example-usage-CMU-FM-1-without-using-MCAL/m-p/2024841#M44968</guid>
      <dc:creator>danielmartynek</dc:creator>
      <dc:date>2025-01-09T12:28:50Z</dc:date>
    </item>
    <item>
      <title>Re: Example usage CMU_FM_1 (without using MCAL)</title>
      <link>https://community.nxp.com/t5/S32K/Example-usage-CMU-FM-1-without-using-MCAL/m-p/2042688#M45846</link>
      <description>I tried to enable CMU_FM_1 to monitor the FIRC_CLK frequency and enable the interrupt FMCIE from IER register to be fired after the measurement is completed by these steps:&lt;BR /&gt;&lt;BR /&gt;IP_CMU_1-&amp;gt;RCCR = CMU_FM_RCCR_REF_CNT(50);&lt;BR /&gt;IP_CMU_1-&amp;gt;IER |= CMU_FM_IER_FMCIE_MASK;&lt;BR /&gt;IP_CMU_1-&amp;gt;GCR |= CMU_FM_GCR_FME_MASK;&lt;BR /&gt;&lt;BR /&gt;But I faced the following behavior that the interrupt was not fired after the completed window and went to power on reset.&lt;BR /&gt;&lt;BR /&gt;Did you face this behavior or something similar like this?&lt;BR /&gt;</description>
      <pubDate>Wed, 12 Feb 2025 15:04:31 GMT</pubDate>
      <guid>https://community.nxp.com/t5/S32K/Example-usage-CMU-FM-1-without-using-MCAL/m-p/2042688#M45846</guid>
      <dc:creator>narimanelashkar</dc:creator>
      <dc:date>2025-02-12T15:04:31Z</dc:date>
    </item>
  </channel>
</rss>