<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>S32K中的主题 Re: LPUART Demos Issue</title>
    <link>https://community.nxp.com/t5/S32K/LPUART-Demos-Issue/m-p/903690#M4583</link>
    <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hi,&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;this demo works this way. It&amp;nbsp;waits for string (either finished by new line character or until buffer is full) and then it sends the string back.&lt;/P&gt;&lt;P&gt;Terminal program must be configured to sent '\n' character for new line, then after ENTER is pressed whole received string is sent back.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;BR, Petr&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
    <pubDate>Wed, 22 May 2019 06:38:13 GMT</pubDate>
    <dc:creator>PetrS</dc:creator>
    <dc:date>2019-05-22T06:38:13Z</dc:date>
    <item>
      <title>LPUART Demos Issue</title>
      <link>https://community.nxp.com/t5/S32K/LPUART-Demos-Issue/m-p/903689#M4582</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Dears,&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;I built a new 'lpuart_echo_s32k146' project from S32SDK RTM3.0.0 with S32K146EVB, and I can see RX data, it can not reply to PC Monitor, it stuck at&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;&lt;EM&gt; while(LPUART_DRV_GetReceiveStatus(INST_LPUART1, &amp;amp;bytesRemaining) == STATUS_BUSY);&lt;/EM&gt;&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;&lt;EM&gt;Can you help to advice, attached the monitor result,&lt;/EM&gt;&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;&lt;EM&gt;BRs,&lt;/EM&gt;&lt;/P&gt;&lt;P&gt;&lt;EM&gt;Ray&lt;/EM&gt;&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Wed, 22 May 2019 02:54:23 GMT</pubDate>
      <guid>https://community.nxp.com/t5/S32K/LPUART-Demos-Issue/m-p/903689#M4582</guid>
      <dc:creator>dannydeng</dc:creator>
      <dc:date>2019-05-22T02:54:23Z</dc:date>
    </item>
    <item>
      <title>Re: LPUART Demos Issue</title>
      <link>https://community.nxp.com/t5/S32K/LPUART-Demos-Issue/m-p/903690#M4583</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hi,&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;this demo works this way. It&amp;nbsp;waits for string (either finished by new line character or until buffer is full) and then it sends the string back.&lt;/P&gt;&lt;P&gt;Terminal program must be configured to sent '\n' character for new line, then after ENTER is pressed whole received string is sent back.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;BR, Petr&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Wed, 22 May 2019 06:38:13 GMT</pubDate>
      <guid>https://community.nxp.com/t5/S32K/LPUART-Demos-Issue/m-p/903690#M4583</guid>
      <dc:creator>PetrS</dc:creator>
      <dc:date>2019-05-22T06:38:13Z</dc:date>
    </item>
    <item>
      <title>Re: LPUART Demos Issue</title>
      <link>https://community.nxp.com/t5/S32K/LPUART-Demos-Issue/m-p/903691#M4584</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hi Petr,&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;&amp;nbsp;&amp;nbsp; Thanks for your response, &lt;/P&gt;&lt;P&gt;&amp;nbsp; Seems I need to chage ‘\n’ to '\r‘&amp;nbsp; in Windows system, otherwise it cannot work,&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;BRs,&lt;/P&gt;&lt;P&gt;Ray&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Wed, 22 May 2019 12:59:37 GMT</pubDate>
      <guid>https://community.nxp.com/t5/S32K/LPUART-Demos-Issue/m-p/903691#M4584</guid>
      <dc:creator>dannydeng</dc:creator>
      <dc:date>2019-05-22T12:59:37Z</dc:date>
    </item>
  </channel>
</rss>