<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>topic MR-CANHUBK344 Extended ID in S32K</title>
    <link>https://community.nxp.com/t5/S32K/MR-CANHUBK344-Extended-ID/m-p/2041646#M45789</link>
    <description>&lt;P&gt;How can i transceive extended ID at can1 ~ can5?&lt;/P&gt;</description>
    <pubDate>Tue, 11 Feb 2025 09:23:57 GMT</pubDate>
    <dc:creator>236</dc:creator>
    <dc:date>2025-02-11T09:23:57Z</dc:date>
    <item>
      <title>MR-CANHUBK344 Extended ID</title>
      <link>https://community.nxp.com/t5/S32K/MR-CANHUBK344-Extended-ID/m-p/2041646#M45789</link>
      <description>&lt;P&gt;How can i transceive extended ID at can1 ~ can5?&lt;/P&gt;</description>
      <pubDate>Tue, 11 Feb 2025 09:23:57 GMT</pubDate>
      <guid>https://community.nxp.com/t5/S32K/MR-CANHUBK344-Extended-ID/m-p/2041646#M45789</guid>
      <dc:creator>236</dc:creator>
      <dc:date>2025-02-11T09:23:57Z</dc:date>
    </item>
    <item>
      <title>Re: MR-CANHUBK344 Extended ID</title>
      <link>https://community.nxp.com/t5/S32K/MR-CANHUBK344-Extended-ID/m-p/2041730#M45790</link>
      <description>&lt;P&gt;Hi,&lt;/P&gt;
&lt;P&gt;type of ID to be sent/receive is set within code using&amp;nbsp;msg_id_type parameter, like below&lt;/P&gt;
&lt;LI-CODE lang="markup"&gt;Flexcan_Ip_DataInfoType tx_info = {
		.msg_id_type = FLEXCAN_MSG_ID_STD,
		.data_length = 8u,
		.fd_enable = FALSE,
		.fd_padding = FALSE,
		.enable_brs = FALSE,
		.is_polling = FALSE,
		.is_remote = FALSE
	};
Flexcan_Ip_DataInfoType rx_info = {
		.msg_id_type = FLEXCAN_MSG_ID_STD,
		.data_length = 8u,
		.fd_enable = FALSE,
		.fd_padding = FALSE,
		.enable_brs = FALSE,
		.is_polling = FALSE,
		.is_remote = FALSE
	};

    rx_info.msg_id_type = FLEXCAN_MSG_ID_EXT;
    FlexCAN_Ip_ConfigRxMb(INST_FLEXCAN_0, 1, &amp;amp;rx_info, 0x1234);
    rx_info.msg_id_type = FLEXCAN_MSG_ID_STD;
    FlexCAN_Ip_ConfigRxMb(INST_FLEXCAN_0, 2, &amp;amp;rx_info, 0x1);

    tx_info.msg_id_type = FLEXCAN_MSG_ID_EXT;
    FlexCAN_Ip_Send(INST_FLEXCAN_0, 0, &amp;amp;tx_info, 0x4567, (uint8 *)&amp;amp;dummyData);

    FlexCAN_Ip_Receive(INST_FLEXCAN_0, 1, &amp;amp;rxData, false);
    FlexCAN_Ip_Receive(INST_FLEXCAN_0, 2, &amp;amp;rxData, false);
&lt;/LI-CODE&gt;
&lt;P&gt;&amp;nbsp;&lt;/P&gt;
&lt;P&gt;BR, Petr&lt;/P&gt;</description>
      <pubDate>Tue, 11 Feb 2025 11:26:50 GMT</pubDate>
      <guid>https://community.nxp.com/t5/S32K/MR-CANHUBK344-Extended-ID/m-p/2041730#M45790</guid>
      <dc:creator>PetrS</dc:creator>
      <dc:date>2025-02-11T11:26:50Z</dc:date>
    </item>
  </channel>
</rss>