<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>S32KのトピックS32K312 HSE CLK &amp;amp; UTEST write error</title>
    <link>https://community.nxp.com/t5/S32K/S32K312-HSE-CLK-amp-UTEST-write-error/m-p/2040275#M45709</link>
    <description>&lt;P&gt;MCU:S32k312; MCAL:MCAL4.0; FXOSC:24MHz.&lt;/P&gt;&lt;P&gt;when config HSE clock to 120MHz and write data to UTEST(0x1B00 0000), then there will be a&amp;nbsp;Hardfault.&lt;/P&gt;&lt;P&gt;when config HSE clock to 60MHz, we can write the data to UTEST successful.&lt;/P&gt;&lt;P&gt;We didn't have this problem when we used MCAL1.0 before.&lt;/P&gt;</description>
    <pubDate>Sat, 08 Feb 2025 03:13:01 GMT</pubDate>
    <dc:creator>David2024</dc:creator>
    <dc:date>2025-02-08T03:13:01Z</dc:date>
    <item>
      <title>S32K312 HSE CLK &amp; UTEST write error</title>
      <link>https://community.nxp.com/t5/S32K/S32K312-HSE-CLK-amp-UTEST-write-error/m-p/2040275#M45709</link>
      <description>&lt;P&gt;MCU:S32k312; MCAL:MCAL4.0; FXOSC:24MHz.&lt;/P&gt;&lt;P&gt;when config HSE clock to 120MHz and write data to UTEST(0x1B00 0000), then there will be a&amp;nbsp;Hardfault.&lt;/P&gt;&lt;P&gt;when config HSE clock to 60MHz, we can write the data to UTEST successful.&lt;/P&gt;&lt;P&gt;We didn't have this problem when we used MCAL1.0 before.&lt;/P&gt;</description>
      <pubDate>Sat, 08 Feb 2025 03:13:01 GMT</pubDate>
      <guid>https://community.nxp.com/t5/S32K/S32K312-HSE-CLK-amp-UTEST-write-error/m-p/2040275#M45709</guid>
      <dc:creator>David2024</dc:creator>
      <dc:date>2025-02-08T03:13:01Z</dc:date>
    </item>
    <item>
      <title>Re: S32K312 HSE CLK &amp; UTEST write error</title>
      <link>https://community.nxp.com/t5/S32K/S32K312-HSE-CLK-amp-UTEST-write-error/m-p/2040386#M45723</link>
      <description>&lt;P&gt;Hi&lt;/P&gt;
&lt;P&gt;What is version of RTD?&lt;BR /&gt;Have you referred to the methods described in &lt;EM&gt;chapter 9.3. Improve performance&lt;/EM&gt; of &lt;A href="https://www.nxp.com/webapp/sd/collateral/1649311370710712344865?version=1.1" target="_self"&gt;Secure Boot Application note v0.1.1.0&lt;/A&gt;?&lt;/P&gt;
&lt;P&gt;&lt;STRONG&gt;&lt;SPAN class="uiOutputText"&gt;IMPORTANT&lt;/SPAN&gt;&lt;/STRONG&gt;&lt;SPAN class="uiOutputText"&gt;: The 120MHz cannot be set by software directly. It won’t work. Please check the following post. It has information related to this problem:&amp;nbsp;&lt;/SPAN&gt;&lt;A title="https://community.nxp.com/t5/S32K/HSE-provides-RSP-NOT-SUPPORTED-response/m-p/1712323/highlight/true#M26508" href="https://community.nxp.com/t5/S32K/HSE-provides-RSP-NOT-SUPPORTED-response/m-p/1712323/highlight/true#M26508" target="_blank" rel="noopener noreferrer"&gt;&lt;SPAN class="uiOutputText"&gt;HSE provides RSP_NOT_SUPPORTED response&amp;nbsp;&lt;/SPAN&gt;&lt;/A&gt;&lt;/P&gt;
&lt;P&gt;&lt;BR /&gt;Best Regards,&lt;BR /&gt;Robin&lt;BR /&gt;-------------------------------------------------------------------------------&lt;BR /&gt;Note:&lt;BR /&gt;- If this post answers your question, please click the "ACCEPT AS SOLUTION" button. Thank you!&lt;/P&gt;
&lt;P&gt;- We are following threads for 7 weeks after the last post, later replies are ignored&lt;BR /&gt;Please open a new thread and refer to the closed one, if you have a related question at a later point in time.&lt;BR /&gt;-------------------------------------------------------------------------------&lt;/P&gt;</description>
      <pubDate>Sat, 08 Feb 2025 10:56:57 GMT</pubDate>
      <guid>https://community.nxp.com/t5/S32K/S32K312-HSE-CLK-amp-UTEST-write-error/m-p/2040386#M45723</guid>
      <dc:creator>Robin_Shen</dc:creator>
      <dc:date>2025-02-08T10:56:57Z</dc:date>
    </item>
  </channel>
</rss>