<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>S32KのトピックRe: S32DS v3.4 Clock tool not working correctly?</title>
    <link>https://community.nxp.com/t5/S32K/S32DS-v3-4-Clock-tool-not-working-correctly/m-p/2038555#M45640</link>
    <description>&lt;P&gt;It's like sometimes it works and other times it doesn't. Sometimes changes have an affect, other times they don't. Seems like a defective tool.&lt;/P&gt;&lt;P&gt;And I can't install v3.6 because it is impossible to get it to work with S32K1.&lt;/P&gt;</description>
    <pubDate>Wed, 05 Feb 2025 10:48:15 GMT</pubDate>
    <dc:creator>bananium</dc:creator>
    <dc:date>2025-02-05T10:48:15Z</dc:date>
    <item>
      <title>S32DS v3.4 Clock tool not working correctly?</title>
      <link>https://community.nxp.com/t5/S32K/S32DS-v3-4-Clock-tool-not-working-correctly/m-p/2038528#M45639</link>
      <description>&lt;P&gt;I try to configure the clocks with the clock tool in S32DS v3.4 and it says there are no errors, and everything should be in line with the S32K144 datasheet, yet I get STATUS_ERROR from CLOCK_DRV_Init function.&lt;/P&gt;&lt;P&gt;Is this a known issue or what might I be doing wrong? Is the tool producing invalid configurations?&lt;/P&gt;&lt;P&gt;And is there a way to get more information why the clock initialization fails?&lt;/P&gt;</description>
      <pubDate>Wed, 05 Feb 2025 10:33:07 GMT</pubDate>
      <guid>https://community.nxp.com/t5/S32K/S32DS-v3-4-Clock-tool-not-working-correctly/m-p/2038528#M45639</guid>
      <dc:creator>bananium</dc:creator>
      <dc:date>2025-02-05T10:33:07Z</dc:date>
    </item>
    <item>
      <title>Re: S32DS v3.4 Clock tool not working correctly?</title>
      <link>https://community.nxp.com/t5/S32K/S32DS-v3-4-Clock-tool-not-working-correctly/m-p/2038555#M45640</link>
      <description>&lt;P&gt;It's like sometimes it works and other times it doesn't. Sometimes changes have an affect, other times they don't. Seems like a defective tool.&lt;/P&gt;&lt;P&gt;And I can't install v3.6 because it is impossible to get it to work with S32K1.&lt;/P&gt;</description>
      <pubDate>Wed, 05 Feb 2025 10:48:15 GMT</pubDate>
      <guid>https://community.nxp.com/t5/S32K/S32DS-v3-4-Clock-tool-not-working-correctly/m-p/2038555#M45640</guid>
      <dc:creator>bananium</dc:creator>
      <dc:date>2025-02-05T10:48:15Z</dc:date>
    </item>
    <item>
      <title>Re: S32DS v3.4 Clock tool not working correctly?</title>
      <link>https://community.nxp.com/t5/S32K/S32DS-v3-4-Clock-tool-not-working-correctly/m-p/2038560#M45641</link>
      <description>&lt;P&gt;I now have core clock configured as 15.6MHz yet through an SDK function the device reports 78MHz. The changes don't take effect.&lt;/P&gt;</description>
      <pubDate>Wed, 05 Feb 2025 10:50:55 GMT</pubDate>
      <guid>https://community.nxp.com/t5/S32K/S32DS-v3-4-Clock-tool-not-working-correctly/m-p/2038560#M45641</guid>
      <dc:creator>bananium</dc:creator>
      <dc:date>2025-02-05T10:50:55Z</dc:date>
    </item>
    <item>
      <title>Re: S32DS v3.4 Clock tool not working correctly?</title>
      <link>https://community.nxp.com/t5/S32K/S32DS-v3-4-Clock-tool-not-working-correctly/m-p/2038749#M45653</link>
      <description>&lt;P&gt;Hi,&lt;/P&gt;
&lt;P&gt;Thank you so much for your interest in our products and for using our community.&lt;/P&gt;
&lt;P&gt;Regarding the clock issue, please share your project to test the issue and to see in more detail what you are doing.&lt;/P&gt;
&lt;P&gt;Regarding S32K144 working on S32DS 3.6 please refer to the following community post:&lt;/P&gt;
&lt;P&gt;&lt;A href="https://community.nxp.com/t5/S32-Design-Studio/S32K1xx-SDK-in-S32DS/td-p/2032492" target="_blank" rel="noopener"&gt;https://community.nxp.com/t5/S32-Design-Studio/S32K1xx-SDK-in-S32DS/td-p/2032492&lt;/A&gt;&lt;/P&gt;
&lt;P&gt;Have a nice day!&lt;/P&gt;</description>
      <pubDate>Wed, 05 Feb 2025 17:22:44 GMT</pubDate>
      <guid>https://community.nxp.com/t5/S32K/S32DS-v3-4-Clock-tool-not-working-correctly/m-p/2038749#M45653</guid>
      <dc:creator>_Leo_</dc:creator>
      <dc:date>2025-02-05T17:22:44Z</dc:date>
    </item>
  </channel>
</rss>