<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>S32KのトピックS32K312 UART</title>
    <link>https://community.nxp.com/t5/S32K/S32K312-UART/m-p/2037587#M45602</link>
    <description>&lt;P&gt;Hello&lt;BR /&gt;I would like to ask if there are any other LPUART interrupts besides the 4 shown below?&lt;/P&gt;&lt;P&gt;&lt;span class="lia-inline-image-display-wrapper lia-image-align-inline" image-alt="LPUART.png" style="width: 713px;"&gt;&lt;img src="https://community.nxp.com/t5/image/serverpage/image-id/322293i4713F12E01F8D837/image-size/large?v=v2&amp;amp;px=999" role="button" title="LPUART.png" alt="LPUART.png" /&gt;&lt;span class="lia-inline-image-caption" onclick="event.preventDefault();"&gt;LPUART.png&lt;/span&gt;&lt;/span&gt;&lt;/P&gt;&lt;P&gt;I want a receive interrupt to occur when the UART receives a character&lt;BR /&gt;Then store the characters in the Call back function&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;</description>
    <pubDate>Tue, 04 Feb 2025 08:33:21 GMT</pubDate>
    <dc:creator>lua40927</dc:creator>
    <dc:date>2025-02-04T08:33:21Z</dc:date>
    <item>
      <title>S32K312 UART</title>
      <link>https://community.nxp.com/t5/S32K/S32K312-UART/m-p/2037587#M45602</link>
      <description>&lt;P&gt;Hello&lt;BR /&gt;I would like to ask if there are any other LPUART interrupts besides the 4 shown below?&lt;/P&gt;&lt;P&gt;&lt;span class="lia-inline-image-display-wrapper lia-image-align-inline" image-alt="LPUART.png" style="width: 713px;"&gt;&lt;img src="https://community.nxp.com/t5/image/serverpage/image-id/322293i4713F12E01F8D837/image-size/large?v=v2&amp;amp;px=999" role="button" title="LPUART.png" alt="LPUART.png" /&gt;&lt;span class="lia-inline-image-caption" onclick="event.preventDefault();"&gt;LPUART.png&lt;/span&gt;&lt;/span&gt;&lt;/P&gt;&lt;P&gt;I want a receive interrupt to occur when the UART receives a character&lt;BR /&gt;Then store the characters in the Call back function&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;</description>
      <pubDate>Tue, 04 Feb 2025 08:33:21 GMT</pubDate>
      <guid>https://community.nxp.com/t5/S32K/S32K312-UART/m-p/2037587#M45602</guid>
      <dc:creator>lua40927</dc:creator>
      <dc:date>2025-02-04T08:33:21Z</dc:date>
    </item>
    <item>
      <title>Re: S32K312 UART</title>
      <link>https://community.nxp.com/t5/S32K/S32K312-UART/m-p/2038053#M45621</link>
      <description>&lt;P&gt;Hello&amp;nbsp;&lt;a href="https://community.nxp.com/t5/user/viewprofilepage/user-id/200168"&gt;@lua40927&lt;/a&gt;.&lt;/P&gt;
&lt;P&gt;Those are the only events which trigger the interrupts. However, you can configure the receive buffer size to meet your specific requirements, as shown in the below image:&lt;/P&gt;
&lt;P&gt;&lt;span class="lia-inline-image-display-wrapper lia-image-align-inline" image-alt="2025-02-04_16-01-35.jpg" style="width: 999px;"&gt;&lt;img src="https://community.nxp.com/t5/image/serverpage/image-id/322404i8471580EA1FF07F5/image-size/large?v=v2&amp;amp;px=999" role="button" title="2025-02-04_16-01-35.jpg" alt="2025-02-04_16-01-35.jpg" /&gt;&lt;span class="lia-inline-image-caption" onclick="event.preventDefault();"&gt;2025-02-04_16-01-35.jpg&lt;/span&gt;&lt;/span&gt;&lt;/P&gt;
&lt;P&gt;I recommend to trying the "&lt;A href="https://community.nxp.com/t5/S32K-Knowledge-Base/Example-S32K312-UART-Transmit-amp-Receive-Using-Interrupt-DS3-5/ta-p/1818775" target="_blank" rel="noopener"&gt;Example S32K312 UART Transmit &amp;amp; Receive Using Interrupt DS3.5 RTD300&lt;/A&gt;" to&amp;nbsp;familiarize yourself with the UART driver and APIs, which are useful to configure the Rx buffer to trigger the Rx_Full event with one character and access to the configured callback. Also, please refer to de S32K3XX Reference Manual Rev. 9 for more information about the LPUART module.&lt;/P&gt;
&lt;P&gt;Please let me know if this was helpful.&lt;/P&gt;
&lt;P&gt;- RomanVR.&lt;/P&gt;</description>
      <pubDate>Tue, 04 Feb 2025 22:05:45 GMT</pubDate>
      <guid>https://community.nxp.com/t5/S32K/S32K312-UART/m-p/2038053#M45621</guid>
      <dc:creator>RomanVR</dc:creator>
      <dc:date>2025-02-04T22:05:45Z</dc:date>
    </item>
  </channel>
</rss>