<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>topic Re: daisy chain problem in S32K</title>
    <link>https://community.nxp.com/t5/S32K/daisy-chain-problem/m-p/2034868#M45478</link>
    <description>&lt;P&gt;The evaluation Board came with one 12 V power supply so we used a 5V power supply which came with the other evaluation kit for the AFEs , so this issue showed up , it was showing UV and was giving the Safety library(SL) issue.&amp;nbsp; &amp;nbsp;&lt;/P&gt;</description>
    <pubDate>Tue, 28 Jan 2025 04:06:10 GMT</pubDate>
    <dc:creator>Shreyas_Bhat_Karkala</dc:creator>
    <dc:date>2025-01-28T04:06:10Z</dc:date>
    <item>
      <title>daisy chain problem</title>
      <link>https://community.nxp.com/t5/S32K/daisy-chain-problem/m-p/2021843#M44773</link>
      <description>&lt;P&gt;Hi there,&lt;/P&gt;&lt;P&gt;We are currently attempting to initialize RDBMSCTBNU by leveraging the example code provided for HVBMS (HvBms400_775_722_TPL_Bring_Up) using the TPL 665a variant. The goal is to read measurement registers from the 775a. However, we are encountering an issue related to SL extraction.&lt;/P&gt;&lt;P&gt;The problem arises when the start measurement write operation is broadcasted to all devices simultaneously. In this scenario, SL extraction fails. Conversely, if the start measurement register is written individually for each device, the measurement values for all four AFEs become visible.&lt;/P&gt;&lt;P&gt;For reference, I have attached the CMU.c code with and without the implemented changes.&lt;/P&gt;&lt;P&gt;Best regards.&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;</description>
      <pubDate>Fri, 03 Jan 2025 10:16:53 GMT</pubDate>
      <guid>https://community.nxp.com/t5/S32K/daisy-chain-problem/m-p/2021843#M44773</guid>
      <dc:creator>Shreyas_Bhat_Karkala</dc:creator>
      <dc:date>2025-01-03T10:16:53Z</dc:date>
    </item>
    <item>
      <title>Re: daisy chain problem</title>
      <link>https://community.nxp.com/t5/S32K/daisy-chain-problem/m-p/2022048#M44786</link>
      <description>&lt;P&gt;I had attached the files in the previous post but it was not present so i am re attaching the code .&lt;BR /&gt;BR&lt;/P&gt;</description>
      <pubDate>Sat, 04 Jan 2025 04:11:49 GMT</pubDate>
      <guid>https://community.nxp.com/t5/S32K/daisy-chain-problem/m-p/2022048#M44786</guid>
      <dc:creator>Shreyas_Bhat_Karkala</dc:creator>
      <dc:date>2025-01-04T04:11:49Z</dc:date>
    </item>
    <item>
      <title>Re: daisy chain problem</title>
      <link>https://community.nxp.com/t5/S32K/daisy-chain-problem/m-p/2023523#M44880</link>
      <description>&lt;P&gt;Okay&lt;/P&gt;
&lt;P&gt;Thanks for your interest in NXP products.&lt;/P&gt;
&lt;P&gt;I will contact you soon, I need to check more details about the problem.&lt;/P&gt;
&lt;P&gt;&amp;nbsp;&lt;/P&gt;
&lt;P&gt;Have a great day and best of luck.&lt;/P&gt;</description>
      <pubDate>Tue, 07 Jan 2025 22:29:34 GMT</pubDate>
      <guid>https://community.nxp.com/t5/S32K/daisy-chain-problem/m-p/2023523#M44880</guid>
      <dc:creator>RafaR</dc:creator>
      <dc:date>2025-01-07T22:29:34Z</dc:date>
    </item>
    <item>
      <title>Re: daisy chain problem</title>
      <link>https://community.nxp.com/t5/S32K/daisy-chain-problem/m-p/2034868#M45478</link>
      <description>&lt;P&gt;The evaluation Board came with one 12 V power supply so we used a 5V power supply which came with the other evaluation kit for the AFEs , so this issue showed up , it was showing UV and was giving the Safety library(SL) issue.&amp;nbsp; &amp;nbsp;&lt;/P&gt;</description>
      <pubDate>Tue, 28 Jan 2025 04:06:10 GMT</pubDate>
      <guid>https://community.nxp.com/t5/S32K/daisy-chain-problem/m-p/2034868#M45478</guid>
      <dc:creator>Shreyas_Bhat_Karkala</dc:creator>
      <dc:date>2025-01-28T04:06:10Z</dc:date>
    </item>
  </channel>
</rss>