<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>S32KのトピックRe: LPSPI_IP_BUSY state while transmitting data from Lpspi_Ip_AsyncTransmit() function</title>
    <link>https://community.nxp.com/t5/S32K/LPSPI-IP-BUSY-state-while-transmitting-data-from-Lpspi-Ip/m-p/2032870#M45394</link>
    <description>&lt;P&gt;Thanks Petr&lt;/P&gt;&lt;P&gt;using this example I can use SPI, and the issue is resolved&amp;nbsp;&lt;/P&gt;</description>
    <pubDate>Thu, 23 Jan 2025 05:56:31 GMT</pubDate>
    <dc:creator>prasadrashinkar</dc:creator>
    <dc:date>2025-01-23T05:56:31Z</dc:date>
    <item>
      <title>LPSPI_IP_BUSY state while transmitting data from Lpspi_Ip_AsyncTransmit() function</title>
      <link>https://community.nxp.com/t5/S32K/LPSPI-IP-BUSY-state-while-transmitting-data-from-Lpspi-Ip/m-p/2024641#M44949</link>
      <description>&lt;P&gt;We have&amp;nbsp; an issue With S32k44,&lt;/P&gt;&lt;P&gt;configured LPSPI using EB tresos and tried to transmit data using&amp;nbsp;Lpspi_Ip_AsyncTransmit()&lt;/P&gt;&lt;P&gt;call gets executed once&amp;nbsp;Other calls are rejected because the drivers stay in the LPSPI_IP_BUSY state.&lt;/P&gt;&lt;P&gt;Can you please share an Example project of S32K344(with EB tresos configuration)&lt;/P&gt;&lt;P&gt;for&amp;nbsp;Lpspi_Ip_AsyncTransmit(); using DMA?&lt;/P&gt;&lt;P&gt;#S32K344&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;</description>
      <pubDate>Thu, 09 Jan 2025 08:31:33 GMT</pubDate>
      <guid>https://community.nxp.com/t5/S32K/LPSPI-IP-BUSY-state-while-transmitting-data-from-Lpspi-Ip/m-p/2024641#M44949</guid>
      <dc:creator>prasadrashinkar</dc:creator>
      <dc:date>2025-01-09T08:31:33Z</dc:date>
    </item>
    <item>
      <title>Re: LPSPI_IP_BUSY state while transmitting data from Lpspi_Ip_AsyncTransmit() function</title>
      <link>https://community.nxp.com/t5/S32K/LPSPI-IP-BUSY-state-while-transmitting-data-from-Lpspi-Ip/m-p/2024845#M44969</link>
      <description>&lt;P&gt;Hi,&lt;/P&gt;
&lt;P&gt;try to look over below example, not for EB but&amp;nbsp;is using HLD driver as well.&lt;BR /&gt;&lt;A href="https://community.nxp.com/t5/S32K-Knowledge-Base/Example-S32K344-SPI-Transmit-amp-Receive-Using-DMA-DS3-5-RTD500/ta-p/1992224" target="_blank"&gt;https://community.nxp.com/t5/S32K-Knowledge-Base/Example-S32K344-SPI-Transmit-amp-Receive-Using-DMA-DS3-5-RTD500/ta-p/1992224&lt;/A&gt;&lt;BR /&gt;Also this one could be useful&lt;BR /&gt;&lt;A href="https://community.nxp.com/t5/S32K/S32K344-SPI-DMA-with-MCAL-configuration-not-send-out-all-bytes/td-p/1767072" target="_blank"&gt;https://community.nxp.com/t5/S32K/S32K344-SPI-DMA-with-MCAL-configuration-not-send-out-all-bytes/td-p/1767072&lt;/A&gt;&lt;/P&gt;
&lt;P&gt;BR, Petr&lt;/P&gt;</description>
      <pubDate>Thu, 09 Jan 2025 12:30:31 GMT</pubDate>
      <guid>https://community.nxp.com/t5/S32K/LPSPI-IP-BUSY-state-while-transmitting-data-from-Lpspi-Ip/m-p/2024845#M44969</guid>
      <dc:creator>PetrS</dc:creator>
      <dc:date>2025-01-09T12:30:31Z</dc:date>
    </item>
    <item>
      <title>Re: LPSPI_IP_BUSY state while transmitting data from Lpspi_Ip_AsyncTransmit() function</title>
      <link>https://community.nxp.com/t5/S32K/LPSPI-IP-BUSY-state-while-transmitting-data-from-Lpspi-Ip/m-p/2032870#M45394</link>
      <description>&lt;P&gt;Thanks Petr&lt;/P&gt;&lt;P&gt;using this example I can use SPI, and the issue is resolved&amp;nbsp;&lt;/P&gt;</description>
      <pubDate>Thu, 23 Jan 2025 05:56:31 GMT</pubDate>
      <guid>https://community.nxp.com/t5/S32K/LPSPI-IP-BUSY-state-while-transmitting-data-from-Lpspi-Ip/m-p/2032870#M45394</guid>
      <dc:creator>prasadrashinkar</dc:creator>
      <dc:date>2025-01-23T05:56:31Z</dc:date>
    </item>
  </channel>
</rss>