<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>topic Re: S32K312 to get random numbers in S32K</title>
    <link>https://community.nxp.com/t5/S32K/S32K312-to-get-random-numbers/m-p/2032238#M45374</link>
    <description>Installed HSE FW is Version 2.40</description>
    <pubDate>Wed, 22 Jan 2025 09:47:58 GMT</pubDate>
    <dc:creator>joma</dc:creator>
    <dc:date>2025-01-22T09:47:58Z</dc:date>
    <item>
      <title>S32K312 to get random numbers</title>
      <link>https://community.nxp.com/t5/S32K/S32K312-to-get-random-numbers/m-p/1645346#M22641</link>
      <description>&lt;P class=""&gt;I want a sample S32K312 to get random numbers&lt;/P&gt;</description>
      <pubDate>Fri, 05 May 2023 08:41:25 GMT</pubDate>
      <guid>https://community.nxp.com/t5/S32K/S32K312-to-get-random-numbers/m-p/1645346#M22641</guid>
      <dc:creator>MengWang1</dc:creator>
      <dc:date>2023-05-05T08:41:25Z</dc:date>
    </item>
    <item>
      <title>Re: S32K312 to get random numbers</title>
      <link>https://community.nxp.com/t5/S32K/S32K312-to-get-random-numbers/m-p/1647099#M22743</link>
      <description>&lt;P&gt;Attached is the same project ported to S32K312. &lt;BR clear="none" /&gt;What I did:&lt;BR clear="none" /&gt;- I installed fullmem firmware 0.2.6.0 to new S32K312 board (see FW_version.jpg)&lt;BR clear="none" /&gt;- created new application project with RTD 2.0.2.&lt;BR clear="none" /&gt;- added HSE module&lt;BR clear="none" /&gt;- copied hse_interface files from firmware 0.2.6.0 folder to include folder in the project&lt;BR clear="none" /&gt;- copied files from src folder (I just had to change s32k344.h to s32k312.h in some files)&lt;BR clear="none" /&gt;- as I already mentioned, it is either necessary to disable data cache memory or the data structures needs to be forced to noncacheable space. In this project, I disabled the data cache - see screenshot cache.jpg, I deleted D_CACHE_ENABLE in Preprocessor&lt;BR clear="none" /&gt;- and then you can see the result in result.jpg. Random number is generated and I got HSE_SRV_RSP_OK / 0x55A5AA33&lt;/P&gt;</description>
      <pubDate>Tue, 09 May 2023 10:47:41 GMT</pubDate>
      <guid>https://community.nxp.com/t5/S32K/S32K312-to-get-random-numbers/m-p/1647099#M22743</guid>
      <dc:creator>lukaszadrapa</dc:creator>
      <dc:date>2023-05-09T10:47:41Z</dc:date>
    </item>
    <item>
      <title>Re: S32K312 to get random numbers</title>
      <link>https://community.nxp.com/t5/S32K/S32K312-to-get-random-numbers/m-p/2032230#M45373</link>
      <description>&lt;P&gt;Unfortunately, I can't get it to run at the moment and therefore have the following question:&lt;/P&gt;&lt;P&gt;What do I have to adapt so that the project works for the S32K312 with RTD 5.0.0 and S32DS 3.6?&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;I have also tried it on the basis of the HSE_Install_FW example (project in the appendix). Unfortunately, I only get HSE_SRV_RSP_NOT_ALLOWED as response.&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;Could you help?&lt;/P&gt;</description>
      <pubDate>Wed, 22 Jan 2025 09:43:59 GMT</pubDate>
      <guid>https://community.nxp.com/t5/S32K/S32K312-to-get-random-numbers/m-p/2032230#M45373</guid>
      <dc:creator>joma</dc:creator>
      <dc:date>2025-01-22T09:43:59Z</dc:date>
    </item>
    <item>
      <title>Re: S32K312 to get random numbers</title>
      <link>https://community.nxp.com/t5/S32K/S32K312-to-get-random-numbers/m-p/2032238#M45374</link>
      <description>Installed HSE FW is Version 2.40</description>
      <pubDate>Wed, 22 Jan 2025 09:47:58 GMT</pubDate>
      <guid>https://community.nxp.com/t5/S32K/S32K312-to-get-random-numbers/m-p/2032238#M45374</guid>
      <dc:creator>joma</dc:creator>
      <dc:date>2025-01-22T09:47:58Z</dc:date>
    </item>
  </channel>
</rss>