<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>topic S32k146 SDK dual-edge input capture in S32K</title>
    <link>https://community.nxp.com/t5/S32K/S32k146-SDK-dual-edge-input-capture/m-p/2030057#M45229</link>
    <description>&lt;P&gt;Hi&amp;nbsp; NXP：&lt;/P&gt;&lt;P&gt;I am using the S32K146 for the first time and would like to set up a demo for dual-edge input detection. According to the manual, dual-edge detection requires configuring two channels. However, I would like to know if it's possible to detect the frequency and duty cycle of the input signal using just one channel. Could you please provide an SDK-driven demo for dual-edge detection and how to measure the input signal's frequency and duty cycle?&lt;/P&gt;&lt;P&gt;Thank you.&lt;/P&gt;&lt;P&gt;&lt;span class="lia-inline-image-display-wrapper lia-image-align-inline" image-alt="LaiBighead_0-1737180365035.png" style="width: 400px;"&gt;&lt;img src="https://community.nxp.com/t5/image/serverpage/image-id/320165i44BAB9DCD8128318/image-size/medium?v=v2&amp;amp;px=400" role="button" title="LaiBighead_0-1737180365035.png" alt="LaiBighead_0-1737180365035.png" /&gt;&lt;/span&gt;&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;</description>
    <pubDate>Sat, 18 Jan 2025 06:06:24 GMT</pubDate>
    <dc:creator>Chandler_L</dc:creator>
    <dc:date>2025-01-18T06:06:24Z</dc:date>
    <item>
      <title>S32k146 SDK dual-edge input capture</title>
      <link>https://community.nxp.com/t5/S32K/S32k146-SDK-dual-edge-input-capture/m-p/2030057#M45229</link>
      <description>&lt;P&gt;Hi&amp;nbsp; NXP：&lt;/P&gt;&lt;P&gt;I am using the S32K146 for the first time and would like to set up a demo for dual-edge input detection. According to the manual, dual-edge detection requires configuring two channels. However, I would like to know if it's possible to detect the frequency and duty cycle of the input signal using just one channel. Could you please provide an SDK-driven demo for dual-edge detection and how to measure the input signal's frequency and duty cycle?&lt;/P&gt;&lt;P&gt;Thank you.&lt;/P&gt;&lt;P&gt;&lt;span class="lia-inline-image-display-wrapper lia-image-align-inline" image-alt="LaiBighead_0-1737180365035.png" style="width: 400px;"&gt;&lt;img src="https://community.nxp.com/t5/image/serverpage/image-id/320165i44BAB9DCD8128318/image-size/medium?v=v2&amp;amp;px=400" role="button" title="LaiBighead_0-1737180365035.png" alt="LaiBighead_0-1737180365035.png" /&gt;&lt;/span&gt;&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;</description>
      <pubDate>Sat, 18 Jan 2025 06:06:24 GMT</pubDate>
      <guid>https://community.nxp.com/t5/S32K/S32k146-SDK-dual-edge-input-capture/m-p/2030057#M45229</guid>
      <dc:creator>Chandler_L</dc:creator>
      <dc:date>2025-01-18T06:06:24Z</dc:date>
    </item>
    <item>
      <title>Re: S32k146 SDK dual-edge input capture</title>
      <link>https://community.nxp.com/t5/S32K/S32k146-SDK-dual-edge-input-capture/m-p/2030214#M45243</link>
      <description>&lt;P&gt;&lt;A href="mailto:Hi@LaiBighead" target="_blank"&gt;Hi@LaiBighead&lt;/A&gt;&lt;/P&gt;
&lt;P&gt;This is a demo I post before, you can take a look at this.&lt;/P&gt;
&lt;P&gt;&lt;A href="https://community.nxp.com/t5/S32K-Knowledge-Base/S32K1-Calculate-the-motor-speed-based-on-the-FTM/ta-p/1515933" target="_blank"&gt;https://community.nxp.com/t5/S32K-Knowledge-Base/S32K1-Calculate-the-motor-speed-based-on-the-FTM/ta-p/1515933&lt;/A&gt;&lt;/P&gt;
&lt;P&gt;&amp;nbsp;&lt;/P&gt;</description>
      <pubDate>Mon, 20 Jan 2025 02:14:45 GMT</pubDate>
      <guid>https://community.nxp.com/t5/S32K/S32k146-SDK-dual-edge-input-capture/m-p/2030214#M45243</guid>
      <dc:creator>Senlent</dc:creator>
      <dc:date>2025-01-20T02:14:45Z</dc:date>
    </item>
    <item>
      <title>Re: S32k146 SDK dual-edge input capture</title>
      <link>https://community.nxp.com/t5/S32K/S32k146-SDK-dual-edge-input-capture/m-p/2030940#M45289</link>
      <description>I'm glad to receive your reply. I have made some attempts with this case, and it was somewhat enlightening. However, when trying the dual-edge detection, I’m unsure when to obtain the Cnv values of CHn and CHn+1.</description>
      <pubDate>Tue, 21 Jan 2025 01:14:36 GMT</pubDate>
      <guid>https://community.nxp.com/t5/S32K/S32k146-SDK-dual-edge-input-capture/m-p/2030940#M45289</guid>
      <dc:creator>Chandler_L</dc:creator>
      <dc:date>2025-01-21T01:14:36Z</dc:date>
    </item>
    <item>
      <title>Re: S32k146 SDK dual-edge input capture</title>
      <link>https://community.nxp.com/t5/S32K/S32k146-SDK-dual-edge-input-capture/m-p/2031027#M45296</link>
      <description>双边沿检测功能已实现，但很奇怪，会一致卡住FTM4_CH2_Input_Detect函数里面，捕获通道频率设置为375Khz，给通道输入250Khz的PWM波；</description>
      <pubDate>Tue, 21 Jan 2025 03:08:52 GMT</pubDate>
      <guid>https://community.nxp.com/t5/S32K/S32k146-SDK-dual-edge-input-capture/m-p/2031027#M45296</guid>
      <dc:creator>Chandler_L</dc:creator>
      <dc:date>2025-01-21T03:08:52Z</dc:date>
    </item>
    <item>
      <title>Re: S32k146 SDK dual-edge input capture</title>
      <link>https://community.nxp.com/t5/S32K/S32k146-SDK-dual-edge-input-capture/m-p/2031167#M45307</link>
      <description>&lt;P&gt;Hi@&lt;SPAN&gt;LaiBighead&lt;/SPAN&gt;&lt;/P&gt;
&lt;P&gt;双边沿输入捕获250KHz，一秒钟相当于中断差不多500K次，你说你这样用考虑过S32K146的性能吗？&lt;/P&gt;
&lt;P&gt;通常电机控制中也就个10K或者20K，你这么高的速率它能处理的了吗。&lt;/P&gt;</description>
      <pubDate>Tue, 21 Jan 2025 07:06:49 GMT</pubDate>
      <guid>https://community.nxp.com/t5/S32K/S32k146-SDK-dual-edge-input-capture/m-p/2031167#M45307</guid>
      <dc:creator>Senlent</dc:creator>
      <dc:date>2025-01-21T07:06:49Z</dc:date>
    </item>
    <item>
      <title>Re: S32k146 SDK dual-edge input capture</title>
      <link>https://community.nxp.com/t5/S32K/S32k146-SDK-dual-edge-input-capture/m-p/2032132#M45364</link>
      <description>谢谢，问题已解决，祝您生活愉快</description>
      <pubDate>Wed, 22 Jan 2025 08:07:33 GMT</pubDate>
      <guid>https://community.nxp.com/t5/S32K/S32k146-SDK-dual-edge-input-capture/m-p/2032132#M45364</guid>
      <dc:creator>Chandler_L</dc:creator>
      <dc:date>2025-01-22T08:07:33Z</dc:date>
    </item>
  </channel>
</rss>